Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Cannot get WiFi connected
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 52 subscribers
  • Views 1386 views
  • Users 0 members are here
  • azure sphere kit
  • wifi
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Cannot get WiFi connected

clem57
clem57 over 7 years ago

Today when I tried to connect to the contest page, I got "WiFi not configured". So I tied to enable/disable the definition. Also a restart as well. After all this I am left with the following:

 

SSID                       : ****************

Configuration state : temp-disabled

Connection state    : disconnected

Security state         : psk

 

So now I did another enable. After a bit, finally it connected.

My question is: Was this the correct approach?

 

 

  • Sign in to reply
  • Cancel

Top Replies

  • peterfenn
    peterfenn over 7 years ago +2 verified
    The difficulty to sometimes connect to a Wi-Fi A/P at a location with multiple Wi-Fi networks/devices is a known bug that you can expect to be fixed in the upcoming OS release.
  • mukulb
    mukulb over 7 years ago +1
    Some times there will be some internal issues. So we can use this, but it is not recommended.
Parents
  • clem57
    0 clem57 over 7 years ago

    Update:

    So I leave the Azure Sphere connected all day, but unused. When I get home it is in this temp-disabled state. The best solution is to unplug the device and re-power up. Then it will connect just fine to the WiFi.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago

    Update:

    So I leave the Azure Sphere connected all day, but unused. When I get home it is in this temp-disabled state. The best solution is to unplug the device and re-power up. Then it will connect just fine to the WiFi.

    Clem