Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum I2C data reading
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 53 subscribers
  • Views 860 views
  • Users 0 members are here
  • azurespherech
  • i2c
  • azuresphkt
Related

I2C data reading

vassily98
vassily98 over 7 years ago

Hi, I am having issues with I2C data reading. The code stops at "Log_Debug(buf[i]);" with a "Segmentation fault occurred".

 

int main(void)
{
static int i2cFd = -1;
const uint8_t* buf[] = { 0, 0 };
    Log_Debug("Loading\n");
i2cFd = I2CMaster_Open(2);
I2CMaster_SetDefaultTargetAddress(i2cFd, 10);
I2CMaster_SetBusSpeed(i2cFd, 100000);
I2CMaster_SetTimeout(i2cFd, 100);
/*if (i2cFd < 0) {
Log_Debug("ERROR: I2CMaster_Open: errno=%d (%s)\n", errno, strerror(errno));
return -1;
}*/


    while (true) {
Log_Debug("Reading...\n");
I2CMaster_Read(i2cFd, 10, &buf, 2);
Log_Debug("Read returned: ");
for (int i = 0; i < 1; i++) {
Log_Debug(buf[i]);
}
Log_Debug("\n\n");
nanosleep(5000000000, NULL);
    }
}

 

This is the console output:

Remote debugging from host 192.168.35.1
Loading
Reading...
Read returned:

 

 

 

I am using an arduino slave with this code as onRequest:

void onI2CRequest(int bytes) {
  TinyWire.send(digitalRead(pin1));
  TinyWire.send(digitalRead(pin2));
}

 

With an Arduino master data is read correctly.

  • Sign in to reply
  • Cancel

Top Replies

  • wizio
    wizio over 7 years ago +3 suggested
    try: Log_Debug("%02X", (int)buf[i]); // hex value the first Log_Debug() parameter is pointer of formated string as printf - C++ Reference
Parents
  • wizio
    0 wizio over 7 years ago

    try:

    Log_Debug("%02X", (int)buf[i]); // hex value

    the first Log_Debug() parameter is pointer of formated string

    as printf - C++ Reference

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vassily98
    0 vassily98 over 7 years ago in reply to wizio

    Now code runs. But the console shows strange values...

     

    This is standard reading:

    Reading...
    Read returned: 101

     

    This when pin1 is low-level:

    Reading...
    Read returned: 100

     

    This when pin2 is low-level:

     

    Reading...
    Read returned: 01

     

    This when both low-level:

    Reading...
    Read returned: 00

     

    The problem is that 0 in the middle of the two..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vassily98
    0 vassily98 over 7 years ago in reply to wizio

    Now code runs. But the console shows strange values...

     

    This is standard reading:

    Reading...
    Read returned: 101

     

    This when pin1 is low-level:

    Reading...
    Read returned: 100

     

    This when pin2 is low-level:

     

    Reading...
    Read returned: 01

     

    This when both low-level:

    Reading...
    Read returned: 00

     

    The problem is that 0 in the middle of the two..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • wizio
    0 wizio over 7 years ago in reply to vassily98

    Log_Debug("Read returned: %d, %d\n", (int)buf[0], (int)buf[1]);

    not need for()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jgroman
    0 jgroman over 7 years ago in reply to wizio

    In the original code the for loop prints only buf[0] and since it is casted to int, it creates 16-bit value out of buf[0] and buf[1]. This causes the zero in the middle - 0xb1b2.