Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum UART Problems
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 53 subscribers
  • Views 1177 views
  • Users 0 members are here
Related

UART Problems

stephenmo
stephenmo over 7 years ago

Has anyone had any success getting UART working on the Azure Sphere?

 

I've taken a look at Microsofts documentation and the UART example that I could find. I can't seem to get a UART_OPEN that doesn't return an error (-1).

 

I think I'm getting Tripped up on UART ID. My guess is that this UART_ID is the ID defined in the application manifest eg "Uart": ["ISU0] would be 0.

image

I've done the usual rx->tx and tx_>rx, ensured my serial device is 3.3v and is outputting data so I'm a bit confused by this.

I've ensured that i've defined     "Uart": ["ISU0"] in my app_manifest.json.

 

Has anyone had any success and have any tips?

 

Minimal example for what I'm trying

 

 

```c

#include <applibs/log.h>

#include <applibs/gpio.h>

#define UART_STRUCTS_VERSION 1

#include <applibs/uart.h>

 

int uartFd = -2;

int main(int argc, char *argv[])

{

UART_Config uartConfig;

UART_InitConfig(&uartConfig);

uartConfig.baudRate = 9600;

uartFd = UART_Open(0, &uartConfig);

 

 

if (uartFd < 0)

{

Log_Debug(":( Couldn't open UART");

}

else

{

Log_Debug("YAY!");

}

    return 0;

}

```

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 7 years ago +3 verified
    Hi, Stephen, Use MT3620_UART_ISU0. MT3620_UART_ISU0 is defined as 4 . In the AVNET examples it is defined as MT3620_RDB_HEADER2_ISU0_UART. uartFd = UART_Open(MT3620_UART_ISU0 , &uartConfig); // MT3620_UART_ISU0…
  • stephenmo
    stephenmo over 7 years ago +3 suggested
    Thanks Clem and Enrique, both of your solutions work. Those constants Enrique mentioned are defined here for anyone else looking.
  • clem57
    clem57 over 7 years ago +2 suggested
    This is the example for the bare metal usage which I recommend to have deterministic usage. : "Uart" : [ "ISU0" ], https://github.com/Azure/azure-sphere-samples/blob/master/Samples/UART/UART_RTApp_MT3620_BareMetal…
Parents
  • javagoza
    0 javagoza over 7 years ago

    Hi, Stephen,

     

    Use MT3620_UART_ISU0.

     

    MT3620_UART_ISU0 is defined as 4.

     

    In the AVNET examples it is defined as MT3620_RDB_HEADER2_ISU0_UART.

     

     

    uartFd = UART_Open(MT3620_UART_ISU0 , &uartConfig); // MT3620_UART_ISU0  is 4

     

    In the manifest use "ISU0"

     

    "Uart": ["ISU0"]

     

    And don't forget to connect GND

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • javagoza
    0 javagoza over 7 years ago

    Hi, Stephen,

     

    Use MT3620_UART_ISU0.

     

    MT3620_UART_ISU0 is defined as 4.

     

    In the AVNET examples it is defined as MT3620_RDB_HEADER2_ISU0_UART.

     

     

    uartFd = UART_Open(MT3620_UART_ISU0 , &uartConfig); // MT3620_UART_ISU0  is 4

     

    In the manifest use "ISU0"

     

    "Uart": ["ISU0"]

     

    And don't forget to connect GND

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer