Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere device cannot connect
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 52 subscribers
  • Views 1721 views
  • Users 0 members are here
Related

Azure Sphere device cannot connect

lotekmachine
lotekmachine over 6 years ago

I have installed per the instructions and all goes well until I try to connect to the command prompt, it says it cannot connect to a device. I went thru the debug prompt , monitoring it with putty and this is what the console reports

 

[1BL] BOOT: 70900000/00000000/01000000

G=47144B5148CDA7AD067C823660D80F2B7303EC0D002894ABC13BB564A44BE3CB1A5BF8177ADB00A9DAAB8CC82251D91573CA3AF531D0018D5D7CB1B34F1B44B7

[1BL] !! ERROR: capability image is not for this device

D=05ba2acf0d2972322c51be54fc814287652f2816d7f8dad385acb59af99c8b182ddbd0824a09908c2f9264d4ee3f0113b4782f30ff62cfcf7ad25e9c30168be1,N=3a68479f1ec7e560b2a86f0ea7f8f456635707197cadb87cd7af279533e64847

[PLUTON] Logging initialized

[PLUTON] Booting application core

 

Anthony

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 6 years ago

    lotekmachine try this command looking for the following output...

     

    azsphere device capability download --type appdevelopment --output ./appdevcap

     

    Downloading device capability configuration for device ID <device ID>.

    Successfully downloaded device capability configuration.

    Successfully wrote device capability configuration file './appdevcap'.

    Command completed successfully in 00:00:07.7393213.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to clem57

    Is this your kit?

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lotekmachine
    0 lotekmachine over 6 years ago in reply to clem57

    Yes it is, Ill try the command a bit later and get back to you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • lotekmachine
    0 lotekmachine over 6 years ago in reply to clem57

    Yes it is, Ill try the command a bit later and get back to you