Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Problem of invalid Starter Kit MAC address
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 53 subscribers
  • Views 779 views
  • Users 0 members are here
Related

Problem of invalid Starter Kit MAC address

vedvaru
vedvaru over 6 years ago

Hi

 

I was trying yesterday to post the data from my Azure sphere to the contest server for the first time.

However my submission was not accepted because of the error - ERROR: Invalid Wi-Fi MAC Address for an Avnet Starter Kit ....

Kindly advise how to solve this issue, my device has mac address beginning with the 00:02 as expected by the batch script- sk_check.bat

I have already added the timeout of 30 seconds to the script after the azsphere restarts so that it's picking up the ip address which is fine.

  • Sign in to reply
  • Cancel

Top Replies

  • vedvaru
    vedvaru over 6 years ago in reply to Gough Lui +2
    Hi Gough Liu Many thanks for the support. The solution provided by you worked fine.
  • clem57
    clem57 over 6 years ago in reply to Gough Lui +1
    Wow the second time this issue cropped up! Thanks Gough Lui for seeing it.
  • Gough Lui
    Gough Lui over 6 years ago in reply to clem57 +1 verified
    Actually clem57 , I think it is the third as I posted a comment to Wrong device name mentioned during the daily sensing where Chandan Jha had "dropped in" on the thread to ask: i am getting wrong mac address…
Parents
  • Gough Lui
    0 Gough Lui over 6 years ago

    I believe you might have a find.exe that is POSIX compatible in your PATH environment before the MS-DOS/Windows version of find.exe.

     

    Please read the comments that I've posted here: https://www.element14.com/community/docs/DOC-92683/l/sensing-the-world-challenge#start=175  starting on Page 8 in the comment thread addressing Kenneth Meyers who had this problem.

     

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to Gough Lui

    Wow the second time this issue cropped up! Thanks Gough Lui  for seeing it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to clem57

    Actually clem57, I think it is the third as I posted a comment to Wrong device name mentioned during the daily sensing where Chandan Jha had "dropped in" on the thread to ask:

    i am getting wrong mac address error while the bat file runs but after that right mac address is written in the box automatically. i checked it on the device mac is correct but still i get emails from Microsoft for wrong mac address......please help.

    It's perhaps something that the organisers should anticipate in the future - the possibility of POSIX-compatible command name clashes and differences in PATH variable ordering. I suppose we do get a similar issue in Linux from time-to-time where scripts are written expecting to use the GNU versions of certain tools, and break when migrated to embedded devices which use busybox versions of the tools which have less features instead.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 6 years ago in reply to clem57

    Actually clem57, I think it is the third as I posted a comment to Wrong device name mentioned during the daily sensing where Chandan Jha had "dropped in" on the thread to ask:

    i am getting wrong mac address error while the bat file runs but after that right mac address is written in the box automatically. i checked it on the device mac is correct but still i get emails from Microsoft for wrong mac address......please help.

    It's perhaps something that the organisers should anticipate in the future - the possibility of POSIX-compatible command name clashes and differences in PATH variable ordering. I suppose we do get a similar issue in Linux from time-to-time where scripts are written expecting to use the GNU versions of certain tools, and break when migrated to embedded devices which use busybox versions of the tools which have less features instead.

     

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • vedvaru
    0 vedvaru over 6 years ago in reply to Gough Lui

    Hi Gough Liu

     

    Many thanks for the support.

    The solution provided by you worked fine.