Avnet & Tria Boards Community
  • Products
  • Dev Tools
  • Avnet & Tria Boards Community
  • More
  • Cancel
Avnet & Tria Boards Community
Avnet Boards Blog PYNQ v2.6 on Ultra96v2
  • Avnet Boards Blog
  • Forums
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet & Tria Boards Community to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 3 Nov 2020 6:19 AM Date Created
  • Views 7698 views
  • Likes 3 likes
  • Comments 30 comments
  • ultra96-v2
  • pmbus
  • pynq v2.6
Related
Recommended

PYNQ v2.6 on Ultra96v2

ralphjy
ralphjy
3 Nov 2020

Last week I saw an announcement that PYNQ v2.6 is available for the Ultra96v1 and Ultra96v2 https://discuss.pynq.io/t/pynq-v2-6-is-avialable-for-ultra96-v1-and-v2/1951 .

 

PYNQ v2.6 is compatible with Xilinx tools version 2020.1.  DPU-PYNQ for v2.6 isn't available yet but because a pre-built image for the Ultra96v2 is available for PYNQ v2.6, I thought that I'd see what has changed from v2.5.

 

The first thing that I noticed is that there are 3 new notebooks in the Common directory

  1. display_port_introduction.ipynb
  2. programming_pybind11.ipynb
  3. ultra96_pmbus.ipynb

 

image

 

The pmbus notebook caught my eye because I had attended the PMBus webinar that Chris Ammann ctammann  had presented back in July PMBus and Power Supply Telemetry .

Chris had mentioned to me that the next BSP release will include the capability to update the PMICs on the Ultra96v2 and the UltraZed-EV and I expect will also include the sensors program that will display the PMIC settings.

 

I hoped that this pmbus notebook might provide the same information as that sensors program provided, i.e. the voltage and current measurements and settings for the all the PMICs.

 

The slide from the webinar shows the 3 PMICs and the 11 voltages that they control on the Ultra96v2 (I am not sure about the configuration of the Ultra96v1).

image

 

Running the pynq.get_rails() function almost works.  It provides the voltage, current and power information for the 2 IRPS5401 parts.  Unfortunately it lists the 10 voltages in alphabetical order by name rather than by IC position.  I can fix that easily enough but I don't understand why IR38060 (5V) isn't listed.  I also don't understand all the garbled stuff at the end.

 

image

 

I looked at the ultra96.conf file in /etc/sensors.d/ directory and the entry for the IR38060 at the end looks incorrect but I'm not quite sure what it should be.

I think it should be :

chip "*-i2c-6-45"

        label in1 "5V"

        label curr1 "5V"

        label power1 "5V"

 

I'll try that tomorrow.

 

ultra96.conf

bus "i2c-6" "i2c-0-mux (chan_id 4)"


chip "*-i2c-6-43"
        ignore in1
        ignore power1
        ignore curr1
        label in2 "AUX"
        label in3 "1V2"
        label in4 "PSDDR"
        label in5 "INT"
        label in6 "3V3_D"
        label power2 "AUX"
        label power3 "1V2"
        label power4 "PSDDR"
        label power5 "INT"
        label power6 "3V3_D"
        label curr2 "AUX"
        label curr3 "1V2"
        label curr4 "PSDDR"
        label curr5 "INT"
        label curr6 "3V3_D"

chip "*-i2c-6-44"
        ignore in1
        ignore power1
        ignore curr1
        label in2 "PSAUX"
        label in3 "PSINT_LP"
        label in4 "3V3"
        label in5 "PSINT_FP"
        label in6 "PSPLL"
        label power2 "PSAUX"
        label power3 "PSINT_LP"
        label power4 "3V3"
        label power5 "PSINT_FP"
        label power6 "PSPLL"
        label curr2 "PSAUX"
        label curr3 "PSINT_LP"
        label curr4 "3V3"
        label curr5 "PSINT_FP"
        label curr6 "PSPLL"

chip "*-i2c-6-45"
        #ignore power1
        label in1 "VIN"
        label curr1 "5V"
        label power1 "5V"
        label in2 "5V"
        compute in2 @/256,@*256

 

 

Anyway, I'll play with this some more.  The notebook also includes a DataRecorder class that allows you to record/plot the sensor measurements while running tests.  Here's a link to the PYNQ library documentation https://pynq.readthedocs.io/en/v2.6.1/pynq_libraries/pmbus.html .

 

Hope the updated DPU-PYNQ is available soon and also the new BSP release so I can update the current limit for running the DPU.

  • Sign in to reply

Top Comments

  • ctammann
    ctammann over 5 years ago +1
    Hey Ralph, Thanks for your interest in this functionality. Let me follow up with my team specifically about the 38060. Without knowing the code, what you say above makes sense if the called out address…
  • ctammann
    ctammann over 5 years ago in reply to ralphjy +1
    Hey Ralph, So the PS vs PL only matters for the reporting from the UltraScale device. The regulator info should still be accessible the same way. I don't know that there is a config file for that, but…
  • ctammann
    ctammann over 5 years ago in reply to ralphjy +1
    Hey Ralph, Check out this dtsi on the UltraZed platform - https://github.com/Avnet/meta-avnet/blob/master/recipes-bsp/device-tree/files/uz7ev-evcc/system-bsp.dtsi specifically lines 48 - 86 where the I2C…
  • albertabeef
    albertabeef over 5 years ago in reply to ralphjy

    Ralph,

    Oops, I did not see your latest post ... sorry about that ...

    The plot.show() function started working after installing packages with pip3.
    I think "pip3 install matplotlib" was the one, but there may have been another package.
    Sorry, I can't remember exactly.

    Hope this helps !

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 5 years ago in reply to blackz

    Yuxuan,

     

    I did not try this on PYNQ, but was able to install the lmsensors package on other 2020.2 (petalinux) design as follows:

       dnf install packagegroup-petalinux-lmsensors

      pip3 install pysensors

     

    I don't know if "dnf" is available on PYNQ.  If not, the following "may" work.
       apt install lm-sensors

      pip3 install pysensors

     

    Let me know if this works.

     

    Regards,

     

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • blackz
    blackz over 5 years ago in reply to ctammann

    Hi Chris,

     

    Thanks for your reply, the prebuilt image https://github.com/Avnet/Ultra96-PYNQ/releases I downloaded doesn't have the sensors command:

    image

    I used PySensors package to check the sensors, I think I maybe need to rebuild the image to make this functionality work.

     

    Yuxuan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • blackz
    blackz over 5 years ago in reply to ralphjy

    Hi Ralph,

     

    Thanks for your reply, it helps me a lot. I believe I need to rebuild the image with the patch you mentioned, I got the PYNQ V2.6 image from http://avnet.me/ultra96v2-pynq-image-v2.6.

    I had a try to solve the problem by using the method mentioned at https://github.com/jgoeders/dac_sdc_2021/tree/master/support/measure_power, it enabled me to measure the power at '5V',

    but they are based on PYNQ V2.5, it will impair the DPU + PYNQ, which won't work anymore.

    image

    I'll have a try to rebuild the image to see whether it will work, thanks a lot!

     

    Yuxuan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ctammann
    ctammann over 5 years ago

    Hey guys,

     

    So the sensors command is included in the 2020.1 bsp, however I'm not a software expert by any stretch so I need to clarify what changes if any need to be made to call these functions from PYNQ. Let me see if I can get you some more clarity

    Thanks
    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>