Avnet & Tria Boards Community
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • More
  • Cancel
Avnet & Tria Boards Community
Avnet Boards Blog PYNQ v2.6 on Ultra96v2
  • Avnet Boards Blog
  • Forums
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet & Tria Boards Community to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 3 Nov 2020 6:19 AM Date Created
  • Views 7863 views
  • Likes 3 likes
  • Comments 30 comments
  • ultra96-v2
  • pmbus
  • pynq v2.6
Related
Recommended

PYNQ v2.6 on Ultra96v2

ralphjy
ralphjy
3 Nov 2020

Last week I saw an announcement that PYNQ v2.6 is available for the Ultra96v1 and Ultra96v2 https://discuss.pynq.io/t/pynq-v2-6-is-avialable-for-ultra96-v1-and-v2/1951 .

 

PYNQ v2.6 is compatible with Xilinx tools version 2020.1.  DPU-PYNQ for v2.6 isn't available yet but because a pre-built image for the Ultra96v2 is available for PYNQ v2.6, I thought that I'd see what has changed from v2.5.

 

The first thing that I noticed is that there are 3 new notebooks in the Common directory

  1. display_port_introduction.ipynb
  2. programming_pybind11.ipynb
  3. ultra96_pmbus.ipynb

 

image

 

The pmbus notebook caught my eye because I had attended the PMBus webinar that Chris Ammann ctammann  had presented back in July PMBus and Power Supply Telemetry .

Chris had mentioned to me that the next BSP release will include the capability to update the PMICs on the Ultra96v2 and the UltraZed-EV and I expect will also include the sensors program that will display the PMIC settings.

 

I hoped that this pmbus notebook might provide the same information as that sensors program provided, i.e. the voltage and current measurements and settings for the all the PMICs.

 

The slide from the webinar shows the 3 PMICs and the 11 voltages that they control on the Ultra96v2 (I am not sure about the configuration of the Ultra96v1).

image

 

Running the pynq.get_rails() function almost works.  It provides the voltage, current and power information for the 2 IRPS5401 parts.  Unfortunately it lists the 10 voltages in alphabetical order by name rather than by IC position.  I can fix that easily enough but I don't understand why IR38060 (5V) isn't listed.  I also don't understand all the garbled stuff at the end.

 

image

 

I looked at the ultra96.conf file in /etc/sensors.d/ directory and the entry for the IR38060 at the end looks incorrect but I'm not quite sure what it should be.

I think it should be :

chip "*-i2c-6-45"

        label in1 "5V"

        label curr1 "5V"

        label power1 "5V"

 

I'll try that tomorrow.

 

ultra96.conf

bus "i2c-6" "i2c-0-mux (chan_id 4)"


chip "*-i2c-6-43"
        ignore in1
        ignore power1
        ignore curr1
        label in2 "AUX"
        label in3 "1V2"
        label in4 "PSDDR"
        label in5 "INT"
        label in6 "3V3_D"
        label power2 "AUX"
        label power3 "1V2"
        label power4 "PSDDR"
        label power5 "INT"
        label power6 "3V3_D"
        label curr2 "AUX"
        label curr3 "1V2"
        label curr4 "PSDDR"
        label curr5 "INT"
        label curr6 "3V3_D"

chip "*-i2c-6-44"
        ignore in1
        ignore power1
        ignore curr1
        label in2 "PSAUX"
        label in3 "PSINT_LP"
        label in4 "3V3"
        label in5 "PSINT_FP"
        label in6 "PSPLL"
        label power2 "PSAUX"
        label power3 "PSINT_LP"
        label power4 "3V3"
        label power5 "PSINT_FP"
        label power6 "PSPLL"
        label curr2 "PSAUX"
        label curr3 "PSINT_LP"
        label curr4 "3V3"
        label curr5 "PSINT_FP"
        label curr6 "PSPLL"

chip "*-i2c-6-45"
        #ignore power1
        label in1 "VIN"
        label curr1 "5V"
        label power1 "5V"
        label in2 "5V"
        compute in2 @/256,@*256

 

 

Anyway, I'll play with this some more.  The notebook also includes a DataRecorder class that allows you to record/plot the sensor measurements while running tests.  Here's a link to the PYNQ library documentation https://pynq.readthedocs.io/en/v2.6.1/pynq_libraries/pmbus.html .

 

Hope the updated DPU-PYNQ is available soon and also the new BSP release so I can update the current limit for running the DPU.

  • Sign in to reply

Top Comments

  • ctammann
    ctammann over 5 years ago +1
    Hey Ralph, Thanks for your interest in this functionality. Let me follow up with my team specifically about the 38060. Without knowing the code, what you say above makes sense if the called out address…
  • ctammann
    ctammann over 5 years ago in reply to ralphjy +1
    Hey Ralph, So the PS vs PL only matters for the reporting from the UltraScale device. The regulator info should still be accessible the same way. I don't know that there is a config file for that, but…
  • ctammann
    ctammann over 5 years ago in reply to ralphjy +1
    Hey Ralph, Check out this dtsi on the UltraZed platform - https://github.com/Avnet/meta-avnet/blob/master/recipes-bsp/device-tree/files/uz7ev-evcc/system-bsp.dtsi specifically lines 48 - 86 where the I2C…
  • ralphjy
    ralphjy over 5 years ago in reply to blackz

    Hi Yuxuan,

     

    If you look earlier in the comments at a response from Chris Ammann - You may also need to make sure this patch is being included in your BSP build - https://www.element14.com/community/external-link.jspa?url=https%3A%2F%2Fgithub.com%2FAvnet%2Fmeta-avnet%2Fblob%2Fmaster…

     

    The prebuilt PYNQ V2.6 image did not include this patch.  I have never tried DPU+PYNQ v 1.3.0, so you need to check whether the BSP used includes or requires this patch.  If it doesn't, you'll need to rebuild the image with the patch installed.   Maybe ctammann can comment on whether this functionality has been included in newer BSPs.

     

    Unfortunately, I don't currently have my Ultra96 setup running as I am working on other projects that needed the space and other resources - so I can't try this out for you.

     

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • blackz
    blackz over 5 years ago in reply to ralphjy

    Hi, Ralph,

     

    I'm a student trying to use DPU+PYNQ v 1.3.0 to deploy some models, when I'm trying to measure the power at [recorder = pynq.DataRecorder(rails["5V"].power)], it didn't work, which it is just like what you described here.

    I found it's because I couldn't get the sensor ir38060-i2c-6-45.

    image

    image

    I think you may know the solution to the problem. I would appreciate it very much, if you can write an answer to it when you are available.

    Thanks a lot!

     

    Yuxuan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to albertabeef

    Hi Mario,

    I wanted to ask you about what you did to get plt.show() to work (even once).   Did you find a GUI backend that would work?  I can't seem to figure out how to install any of them using pip3.  Did you have to rebuild your python installation?  Python3.7 is supposed to have tk included but maybe with petalinux that has to be enabled (not sure if that is a package option, I know qt is).

     

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to albertabeef

    Hi Mario,

    I got a chance to update the PMICs on my Ultra96v2 today.  I can now run the Vitis-AI 1.2 examples but am getting flickering in the display window.  Not sure what is going on - I don't have this problem on my UltraZed-EV with the same monitor but I also don't get the EDID and EGL errors.

     

    I also got a chance to try your pmbus-power-monitoring.  Looks like you changed the name of your scripts but have not updated your instructions to use the new name.

     

    Looks good.  I'll play around with it more when I get time.

     

    Thanks,

    Ralph

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • albertabeef
    albertabeef over 5 years ago in reply to ralphjy

    Ralph,

    I just updated the scripts, added a new argument to specify the maxlimit (allows to zoom in on those low values if needed).
    The plt.show() is now working, but I did not switch to using it, since it only displays once (ie. no animation).
    If you can figure out how to make use of matplotlib's animate functionnality, that would be awesome !I'm going to leave things as is, unless you have udpates or suggestions.
    Hope this helps your work !

    Mario.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>