Dev Tools
  • Products
  • More
Dev Tools
Forum Touch interface by detecting light levels in a single LED
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 81 subscribers
  • Views 1302 views
  • Users 0 members are here
  • technologies
  • lighting
  • led
  • led_lighting
  • leds
Related

Touch interface by detecting light levels in a single LED

Catwell
Catwell over 16 years ago

Using two digital i/o pins a microprocessor can be used to both emit and detect light through a LED. The concept is simple, switch the biasing of the diode for each condition depending on the circuit layout of the diode. Since the LED is a photodiode, sensitive to light that is above the spectrum at which it displays, it can be polled for the current light level it sees.

 

imageimage

Then you simulate the biasing of the LED in the microcontroller to emit and detect. Depending on the number of LEDs, even a low frequency uC could handle the job.
imageimage
The video attached to the post demonstrates how fast and accurate this interface can operate. Also attached is a document on building a touch LED interface, where the above Figure clips were taken from. My immediate idea is a fun interactive light wall for advertisement. But the versatility of this simple input has no bounds. Buttons for a device, a simple touch screen, a hand reconfigurable digital sign, to just name a few possibilities. But does it work in the dark?
 
See also "Engineer's Notebooks" 1977, By Forrest M. Mins. Mins describes how an LED can be used as a photodiode.
 
Cabe
Attachments:
TR2003-35.pdf

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Neat idea, that I hadn't come across before, thank you.

    Using an analogue input connected to the junction between the LED and the resistor, you might also measure temperature when the diode is forward biased....

     

    Andy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Dogmagnet,

     

    Can you post a temperature measuring schematic based on your idea?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Catwell
    Catwell over 15 years ago in reply to e14 Contributor

    Dogmagnet,

     

    Can you post a temperature measuring schematic based on your idea?

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Catwell

    The forward voltage of an LED (or any diode) is a function of its junction temperature, decreasing about 4mV per degree Celcius.  So when a calibration curve exists, Vf => Tj.