Dev Tools
  • Products
  • More
Dev Tools
Forum Decoupling capacitors behavior on power-off
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 84 subscribers
  • Views 1132 views
  • Users 0 members are here
Related

Decoupling capacitors behavior on power-off

modelrailwaycat
modelrailwaycat over 10 years ago

Hello,

 

I am designing a home control system which contains a 'net' of multiple PCBs. Each PCB has several decoupling capacitors, namely 1 large 100 uF capacitor near the power supply connector (5V), and several 100nF spread on the board close to the ICs Vcc pins (between 6 and 10 per board). The finished system will include about 60 boards like this, separated several centimeters or even meters one of each other, and all of them powered by the same power supply. So at the end all the capacitors will be paralelled to the power rails.

 

My question is about the behavior of the system when the power will be turned off. At this point, I realize I will have an equivalent +6000 uF capacitor. What should be considered regarding the design of the system or the power supply in order to guarantee a safe operation?

 

Thank you very much in advance!

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 10 years ago +1
    What should be considered regarding the design of the system or the power supply This is an excellent example of good engineering. The turn off shouldn't be much of an issue, as each board will draw…
Parents
  • D_Hersey
    D_Hersey over 10 years ago

    This was more of a concern in the tube era, 'cause lethal potentials.  Big bypass caps had bleeder resistors in shunt so they would drain before the chassis could be opened after powerdown.  Big stereo PAs initially fill their bp caps through a resistor then use a timed relay to shunt down the resistor.  Nowadays they have a thermistor type that can be used without control, it is called an inrush surge limiter.

     

    PIO resistors can have so much dielectric soakage that they can charge themselves back up!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 10 years ago

    This was more of a concern in the tube era, 'cause lethal potentials.  Big bypass caps had bleeder resistors in shunt so they would drain before the chassis could be opened after powerdown.  Big stereo PAs initially fill their bp caps through a resistor then use a timed relay to shunt down the resistor.  Nowadays they have a thermistor type that can be used without control, it is called an inrush surge limiter.

     

    PIO resistors can have so much dielectric soakage that they can charge themselves back up!