Dev Tools
  • Products
  • More
Dev Tools
Forum Impact generator
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 81 subscribers
  • Views 1003 views
  • Users 0 members are here
Related

Impact generator

e14 Contributor
e14 Contributor over 13 years ago

Hi there !

First post on Element14, I hope I'm not doing it wrong image

 

I use an arduino, and I want to create a device that can generate a small impact.

A little bit like a windows braker that are used on scene of accident, but my project has nothing to do with windows or car crash.

 

I tried to think about a simple way to allow the arduino to create a small impact on demand.

I don't think I need over 2 to 5 impacts per seconds, but I need the impact to be as constant as possible ( same velocity and same force everytime )

 

A vibration could also do the job...

 

Anyway, I'm open to lots of idea since so far, no "ready to go" solution seems to exist, so I was counting on some good idea to enlight me.

 

 

----------------

 

My whole idea is to create a device that can read the resonance of an object ( Ie.: a fuel tank ), so I need to "hit" ( the impact part ) something, then I will use a piezo sensor ( from electronic drums) to try to read the vibration that will come from the object that is being inspected.

 

The basic purpose, in that example, would be to determine, using the resonnance, if the thank is full of empty, or contain something else than fuel inside.

 

 

 

Thanks for taking the time to read image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 13 years ago +1
    Do you mean something like this ? http://www.dtic.mil/cgi-bin/GetTRDoc?AD=ADA560339 Bruel & Kjoer used to make some rather nice ones but this current one is more for sound than vibration: http://www.bksv…
  • michaelkellett
    michaelkellett over 13 years ago

    Do you mean something like this ?

     

    http://www.dtic.mil/cgi-bin/GetTRDoc?AD=ADA560339

     

    Bruel & Kjoer used to make some rather nice ones but this current one is more for sound than vibration:

     

    http://www.bksv.com/products/transducers/acoustic/sound-sources/tapping-machine-3207.aspx

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago

    Wouldn't some selenoid powered device help you here they should operate about the speed you are interested in

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to michaelkellett

    Yes, is look pretty much like what I want to do, except I'm aiming to do a handheld device, and I don't expect as close as the precision they achieve with they device.

     

    The point that bug me is the actuator, how to create the solenoid. I understand how to make the impact tip produce the hit, but I don't understand how to make it go back in ready mode after the impact was produced.

     

    I was hoping to find an "actuator + impact tip" all ready to go, but it looks like I'm gona have to build that myself image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    You can do that by reversing the current to the selenoid and the actuator will reverse direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    O yeah how about having some form of magnetic coupling  to hold your device on to the thing been sensed assuming it's steel of course!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    These are good ideas image

     

    Thanks for the help guys !