Dev Tools
  • Products
  • More
Dev Tools
Forum Impact generator
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 81 subscribers
  • Views 1004 views
  • Users 0 members are here
Related

Impact generator

e14 Contributor
e14 Contributor over 13 years ago

Hi there !

First post on Element14, I hope I'm not doing it wrong image

 

I use an arduino, and I want to create a device that can generate a small impact.

A little bit like a windows braker that are used on scene of accident, but my project has nothing to do with windows or car crash.

 

I tried to think about a simple way to allow the arduino to create a small impact on demand.

I don't think I need over 2 to 5 impacts per seconds, but I need the impact to be as constant as possible ( same velocity and same force everytime )

 

A vibration could also do the job...

 

Anyway, I'm open to lots of idea since so far, no "ready to go" solution seems to exist, so I was counting on some good idea to enlight me.

 

 

----------------

 

My whole idea is to create a device that can read the resonance of an object ( Ie.: a fuel tank ), so I need to "hit" ( the impact part ) something, then I will use a piezo sensor ( from electronic drums) to try to read the vibration that will come from the object that is being inspected.

 

The basic purpose, in that example, would be to determine, using the resonnance, if the thank is full of empty, or contain something else than fuel inside.

 

 

 

Thanks for taking the time to read image

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 13 years ago +1
    Do you mean something like this ? http://www.dtic.mil/cgi-bin/GetTRDoc?AD=ADA560339 Bruel & Kjoer used to make some rather nice ones but this current one is more for sound than vibration: http://www.bksv…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    These are good ideas image

     

    Thanks for the help guys !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    These are good ideas image

     

    Thanks for the help guys !