Dev Tools
  • Products
  • More
Dev Tools
Forum Free Developement tools from XMOS
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 84 subscribers
  • Views 5424 views
  • Users 0 members are here
Related

Free Developement tools from XMOS

xmos_support
xmos_support over 12 years ago

Download the latest development tools xTIMEcomposer and xSOFTip explorer for free. Check out the user forum - www.xcore.com . The Xcore community comprises experienced 3rd party users and XMOS engineering staff, and using this resource ensures that all XMOS technology users will benefit from the answer.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +2
    Hi, The XMOS toolchains is built around various open source tools such as gdb, LLVM, eclipse, and binutils, and standard intermediate formats such as ELF and dwarf. Source tarballs for the open source…
  • morgaine
    morgaine over 12 years ago in reply to xmos_support +1
    XMOS Support wrote: We do have public documentation for enough stuff (architecture, ABI etc.) to create a toolchain. Have a look at the following projects for more details: http://www.xcore.com/projects…
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem +1
    Thanks for the improved description, John! I hope your experience helps XMOS Support to understand my reasons for asking. It's not an "information wants to be free" kind of thing at all, but a desire that…
  • Problemchild
    Problemchild over 12 years ago in reply to morgaine

    Morgane this is as a result of the core vs thread  thing  so a singe old core = 8 threads = 8 new cores.

     

    Their reasoning was that folk found the concept of a thread confusing.. might sound daft to you but I can asure you that explaining it to many so called hardware savy people that it is confusing to people, so I think they are right here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to xmos_support

    XMOS Support wrote:

     

    Are XMOS devices fully documented so that OSHW communities can develop around these devices and create their own complete toolchains to program them?

     

    We do have public documentation for enough stuff (architecture, ABI etc.) to create a toolchain. Have a look at the following projects for more details:

    http://www.xcore.com/projects/gcc-xs1
    http://www.xcore.com/projects/binutils-xs1

    This is certainly right I managed to re-build most of the tool chain  personally to  run on the original RPI ... as you can imagine the performance sucked rather image !!

    Not  tried it  recently but should work better on the BBB or Odroid.. They did use Eclipse as the IDE and that really needs 1GB or so to be effective image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to xmos_support

    XMOS Support wrote:

     

    We do have public documentation for enough stuff (architecture, ABI etc.) to create a toolchain. Have a look at the following projects for more details:

    http://www.xcore.com/projects/gcc-xs1
    http://www.xcore.com/projects/binutils-xs1

     

    Thank you for replying, XMOS Support.  Would it be possible to define what is not documented please, just in outline or summary?  It's not inherently a problem, but it's important to know where the line is drawn so that it's clear that whatever is not documented does not actually matter for OSHW success.

     

    I'll try to explain why I'm being persistent.  One of our top contributors, John Beetem, has for many years been working on a toolchain to support the "well documented" Cypress PSoC4/5 architecture that embeds FPGA-like elements within an ARM-based host.  The project seemed to have no secrecy hurdles to overcome, but towards the end, very detailed analysis of the register specifications revealed that some of the bit definitions required for configuring PSoC's programmable logic elements had been held back, and so the project fell at the last hurdle.  (This is a second-hand description of events and may not be 100% accurate, but hopefully close enough to explain the danger of partial information.)

     

    This is why I'm trying to understand in advance the extent and limits of XMOS documentation.  There are many kinds of process, fabrication and marketing documentation that are of no interest to OSHW builders and programmers whatsoever, and so their absence would not matter.  But conversely, if information that allows official software to achieve something important (such as configuring logic elements or peripherals or tracing/debugging or any other programmable facility) is omitted from public documentation then it is likely that there will be problems ahead.

     

    I hope this explains what I'm after.  It's really about advance planning, trying to determine whether it is wise or not to begin a multi-year investment of one's time, and it influences purchasing choices.  Knowing the bounds of what is documented allows an informed decision to be made.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I'll try to explain why I'm being persistent.  One of our top contributors, John Beetem, has for many years been working on a toolchain to support the "well documented" Cypress PSoC4/5 architecture that embeds FPGA-like elements within an ARM-based host.  The project seemed to have no secrecy hurdles to overcome, but towards the end, very detailed analysis of the register specifications revealed that some of the bit definitions required for configuring PSoC's programmable logic routing elements had been held back, and so the project fell at the last hurdle is examining what can be done.  (This is a second-hand description of events and may not be 100% accurate, but hopefully close enough to explain the danger of partial information.)

    Thank you for referencing my work.  Just to clarify for other readers, I'm working on a system for hardware/software co-design where "hardware" in this case is primarily programmable logic.  I would like to make my system capable of going from design entry to bit-stream without needing any proprietary tools.  Unfortunately, most FPGA vendors do not provide the bit-level documentation needed to do this, and if you ask for an explanation they direct you to iamaweasel.com.   Cypress PSoC4/5 is a very promising target, because they do in fact provide bit-level documentation for everything except the routing.  I plan to explore Cypress routing very soon after completing a few other tasks first -- we'll see what I come up with and what I can release.

     

    My general philosophy towards ICs is that vendors should document everything that's needed to use the chip functions for which customers buy the chip.  It's fine to have hidden test modes not used by customers.  I'm willing to live with hidden bit-stream encryption provided that customers can choose not to encrypt and bypass that logic.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Thanks for the improved description, John!

     

    I hope your experience helps XMOS Support to understand my reasons for asking.  It's not an "information wants to be free" kind of thing at all, but a desire that helpful engineering by independent parties not be held back.  A multiplicity of independent tools is highly likely to increase device sales, so there is much to gain for the manufacturer by being fully open in this specific area.

     

    Your defining form of words is extremely well chosen: [highlighting is mine]

     

    John Beetem wrote:

     

    My general philosophy towards ICs is that vendors should document everything that's needed to use the chip functions for which customers buy the chip.  It's fine to have hidden test modes not used by customers.  I'm willing to live with hidden bit-stream encryption provided that customers can choose not to encrypt and bypass that logic.

     

    That's a perfect statement of the level of documentation needed, and it is also a very reasonable expectation to have because after all we buy chips so that we can use all their functions. Denying some of those functions to the open source community is not reasonable --- they too are paying full price for the chips after all.  Hopefully XMOS Support will understand that expectation and define the level of documentation using your terms.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to morgaine

    One advantage here is that at least one of their Toolchains was openly built around Open source tools.

    But as you described so well earlier it doesn't take a lot of "secret source" to ruin your project generally way way down the line after you have put in a whole load of effort.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to Problemchild

    Indeed.  After years of work, that is one surprise that an open source developer really does not need.

     

    Nobody is paying for the work, it's typically a labour of love and freely offered to the world, yet the existence of such additional toolchains is strongly to the commercial benefit of the company in numerous way.

     

    Education is an important issue for me owing to past involvement.  Among other benefits, open tools make a hardware platform more attractive to education through independence from commercial update cycles, they allows bugs discovered by students to be understood and fixed rapidly in-house without delaying courses (often fixed by the students themselves!), and they enable research students to extend the toolchains for specific project aims, a common desire and an easy way of starting graduates off in new directions.  (Highly relevant since parallelism is an important research area.)

     

    Outside of education the benefits of open systems are very widely known of course and in 2013 no longer even need stating.  Perhaps in light of recent highly public events though, it's worth noting that open software can be assigned a far higher degree of trust and security than any closed proprietary toolkit.  When you're designing control systems for a nuclear power plant involving cryptographic security, or you simply want to protect your family or property, that is not a matter to be taken lightly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to Problemchild

    Contact seems to have dried up, although of course XMOS Support  might be simply busy, or investigating the question with the intention of giving a well-informed answer.  I hope that's the case.

     

    Meanwhile ...

    John Alexander wrote:

     

    One advantage here is that at least one of their Toolchains was openly built around Open source tools.

     

    Which toolchain is that?  I've been looking at the Xcore github repos and haven't found any XMOS toolchain sources yet.  The two mentioned toolchain projects (gcc-xs1 and binutils-xs1) appear to be one-person efforts and no files have been posted for either of them.  There are tons of application modules in Github, but they're generally written in XC --- is that compiler maintained as open source?

     

    If not, then since XC has extensions not present in gcc, the point made by John applies to it.  Is all the functionality employed within the XC implementation documented, so that a fully-functional equivalent open source tool (assuming that XC is not) could be written from the documentation?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Hi,

     

    The XMOS toolchains is built around various open source tools such as gdb, LLVM, eclipse, and binutils, and standard intermediate formats such as ELF and dwarf.

     

    Source tarballs for the open source components are on <http://www.xmos.com/products/design-tools-source>.

     

    Hope this helps,

    Henk

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Thanks for that link Henk, the previous toolchain used Eclipse asthe front end what are they using now??

    Sorry haven't installed it yet thus the question!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>