Dev Tools
  • Products
  • More
Dev Tools
Forum 24 VDC Line 120 VAC Buttons?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 82 subscribers
  • Views 856 views
  • Users 0 members are here
Related

24 VDC Line 120 VAC Buttons?

MrMiz
MrMiz over 11 years ago

I just realized that the terminals are for 24 VDC and most buttons I'm finding on the web are for VAC... I'm having trouble find VDC buttons... and forget about searching for DC buttons. Anybody have any advice on either using VAC buttons on a VDC line or know where I can find VDC buttons?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 11 years ago in reply to MrMiz +1
    Hi MrMiz, It will not matter whether the button is rated for AC volts or DC volts in your circumstance. You can confidently buy which ever switch cosmetically fits your need. There is probably a convention…
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    Without data, I wouldn't use a switch rated at 110 V AC much above 24 V DC.  Typically, they are rated much lower in DC service than AC service.  Check the datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 11 years ago

    Without data, I wouldn't use a switch rated at 110 V AC much above 24 V DC.  Typically, they are rated much lower in DC service than AC service.  Check the datasheet.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jw0752
    jw0752 over 11 years ago in reply to D_Hersey

    Hi Don, As usual you have a very good point. However, this thread was carried over from a previous thread and so I had the knowledge that the application was an electronic garage door opener and all he needed was a push button to toggle the UP - STOP - DOWN function. As such I saw no need to be too concerned with switch ratings. For the sake of those who may not know the context it is important to emphasize that switches that are used in large power switching situations, unlike this one, need to be properly sized to minimize arcing and premature failure.

    John