Dev Tools
  • Products
  • More
Dev Tools
Forum live view magnifier for smd assembly
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 80 subscribers
  • Views 654 views
  • Users 0 members are here
Related

live view magnifier for smd assembly

e14 Contributor
e14 Contributor over 10 years ago

Thinking about using a video magnifier, in live view, suspended above a pcb for placing smd components to a board, you would look at your monitor rather than the board. any thoughts on this ?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to shabaz +1
    Hey shabaz, thanks for the reply, good points about stability, also about lighting, as a photographer, i use soft boxes to soften a photo and cut out glare, same technique could be applied here. I'm looking…
  • shabaz
    0 shabaz over 10 years ago

    Hi William,

     

    There is a prototype system documented here: Building a Digital PCB Inspection Microscope with the Gizmo 2 

    which offers some ideas perhaps.

    Here are some brief experiences from the whole project:

    1. Perhaps discuss directly with camera vendors which lenses they recommend for their cameras given your requirements. And discuss with lens manufacturers if you can too. I used a Computar lens, but I would strongly consider asking Fujitsu too, their lenses look great.

    2. When it comes to the camera stand, use very thick steel (about 25mm dia); with any less there is a risk of oscillations if you accidentally touch the camera. I used 12.5mm which is just-about acceptable (I just avoid touching the camera or stand) but I wish I'd gone with 25mm. For similar reasons make sure you clamp it to steel or aluminium. I used a short length of timber, and this too causes oscillations that travel to the camera.

    3. Lighting is super important, and it is not just about directing a strong beam of light from one direction otherwise you get glare. Sometimes even bouncing the light off walls is good, combined with some light aimed at the workpiece.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Hey shabaz, thanks for the reply, good points about stability, also about lighting, as a photographer, i use soft boxes to soften a photo and cut out glare, same technique could be applied here. I'm looking to prototype using low cost magnifier/camera, at the moment, it's just an idea, I'll look at the link you provided, Thanks again for the speedy response to my post.

     

    William.