Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum Doubt with I2C connector
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 79 subscribers
  • Views 1312 views
  • Users 0 members are here
  • board
  • but passthrough
  • i2c
  • layout
  • schematics
  • duplicate connector
  • prototype
  • Design
  • raspberry pi
  • psoc 4200
  • cypress psoc 4200
Related

Doubt with I2C connector

balearicdynamics
balearicdynamics over 9 years ago

Some days ago I have assembled a first prototye of a PSoC 4200 series based on the CY8CKIT-049042xx board "implanted" over a custom board. The microcontroller can manage a couple of Stepper motors via a L298 controller board. Every unit will be controlled by a Raspberry PI via I2C protocol. Below the schematics and the first PCB.

imageimageimage

I tested the boards and worked well but I discovered a missing wire, the common ground signal between the PI and the controlled boards. The boards does not need a VCC as are powered by a different source. For prototype testing this is not a very serious problems, I wired an extra-cable to connect the two ground.

Then I have updated the schematics to a version 2 with a new PCB layout. For completeness I have added the following things:

  1. The GND pin for the I2C connector
  2. The VCC pin (not used in this particular project but useful in some other case(
  3. Replicated the connector to have the option to create an I2C bus chain from a Raspberry PI to multiple boards (with different I2C address

Below the new schematics and the new layout

imageimage

The two I2 connectors on the board can be shown in the layout in the bottom left corner.

My doubt is if it is sufficient to replicate the layout as shown in the images above or some extra circuitry is needed (e.g. to differentiate the I2C in and the out connectors). Any suggestion is welcome.

 

Thanks in advance.

Enrico

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 9 years ago +3 verified
    Hi Enrico, To me it looks good, no need for anything extra, and no need to do anything different for the I2C in/out. I think (I'm not knowledgeable on PSoC so I'm guessing) that the PSoC has the ability…
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz +2 suggested
    Hi Shabaz! Thank you for the good suggestion. With your detailed answer you got me anothrer further suggestion just based on the PSoC I2C atchitecture. The I2C component (that is one of the configurable…
  • balearicdynamics
    balearicdynamics over 9 years ago +1
    Accordingly with the suggestions of shabaz below the new schematics and layout. About the power line instead it was my mistake: PSoC support both power 3.3V and 5V so the jumper is not needed. Enrico
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Accordingly with the suggestions of shabaz below the new schematics and layout. About the power line instead it was my mistake: PSoC support both power 3.3V and 5V so the jumper is not needed.

     

    Enrico

    imageimage

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Accordingly with the suggestions of shabaz below the new schematics and layout. About the power line instead it was my mistake: PSoC support both power 3.3V and 5V so the jumper is not needed.

     

    Enrico

    imageimage