Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum How do I program a Cypress CYBLE-214009 chip?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 80 subscribers
  • Views 2245 views
  • Users 0 members are here
  • cyble-214009
  • frontpage
  • london
  • cypress
Related

How do I program a Cypress CYBLE-214009 chip?

dominik.kania
dominik.kania over 9 years ago

Hello and thanks for stopping by.

 

I'm new here, currently prototyping an air quality sensor, based on a Cypress CYBLE-214009 processor.

So far, I have used the CYBLE-214009-EVAL evaluation board as an interface enabling me to program the chip. Now, I'd like to miniaturise the design and use only the CYBLE-214009 bluetooth processor (it's super small and has a buit-in BLE) on a customised board. However, I could not see a programming board from Cypress that would allow me to simply drop the processor on a socket in order to program it. Sure enough, Cypress advertises a development kit, but it looks like it does not have a socket that would allow me to simply drop in and program the processor itself.

 

Your advice would be much appreciated.

 

Regards,

Dominik

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago +2
    Normally your custom card would be designed to include a programming connector. As mentioned direct programming adapters can be expensive because it is hard to make robust connectors at the small pitch…
  • koudelad
    koudelad over 9 years ago +1 suggested
    Hello, the PSoC4 BLE device can be programmed using MiniProg3, http://www.cypress.com/documentation/development-kitsboards/cy8ckit-002-psoc-miniprog3-program-and-debug-kit If you plan to design your own…
  • dominik.kania
    dominik.kania over 9 years ago in reply to koudelad +1 suggested
    Thanks David. I'm aware of MiniProg3 and should have better specified the question. What I would like to know specifically is whether the following programming kit ( http://www.cypress.com/file/304411…
  • koudelad
    0 koudelad over 9 years ago

    Hello,

    the PSoC4 BLE device can be programmed using MiniProg3, http://www.cypress.com/documentation/development-kitsboards/cy8ckit-002-psoc-miniprog3-program-and-debug-kit

    If you plan to design your own board, you can place the 10 pin JTAG connector there.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dominik.kania
    0 dominik.kania over 9 years ago in reply to koudelad

    Thanks David. I'm aware of MiniProg3 and should have better specified the question.

     

    What I would like to know specifically is whether the following programming kit (http://www.cypress.com/file/304411/download) allows to program CYBLE-214009 or if not, what would be a suitable altetnative. I have reached out to Cypress but no news from them so far.

     

    Dominik

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • koudelad
    0 koudelad over 9 years ago in reply to dominik.kania

    Oh, OK.

    According to CYBLE-022001-00, EZ-BLE PROC Module page, the mentioned kit CYBLE-022001-PROG EZ-BLETm Module Programming Kit is listed in Development Kits / Boards. So I would say it is supported, but let a Cypress employee / someone who actually owns the device to confirm.

     

    However, the module programming kit still requires a programmer:

     

    Programming Procedure

    1. Connect the kit with one of the following three programming devices:
      1. BLE Pioneer kit (CY8CKIT-042-BLE)
      2. MiniProg3 (CY8CKIT-002)
      3. Third-party programming tool, such as MPQ-PSoC
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koudelad
    0 koudelad over 9 years ago in reply to dominik.kania

    And it is also listed in the document, you referenced. So I guess no more confirmation is required.

    The EZ-BLE Module Programming Kit (CYBLE-022001-PROG) enables you to easily program the following EZ-BLE PRoC modules prior to manufacturing: CYBLE-022001-00CYBLE-022001-00, CYBLE-222005-00 and CYBLE-222014-01

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dominik.kania
    0 dominik.kania over 9 years ago in reply to koudelad

    Thanks again David, very helpful. The question is whether this programming kit also allows to program CYBLE-214009 which I think belongs to the same "family" but is not explicitly referenced in the support guide..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • koudelad
    0 koudelad over 9 years ago in reply to dominik.kania

    I am sorry, I was confused. You are right and I was wrong.

    You are using CYBLE-214009-00 (size 11 x 11 x 1.8 mm) which is drop-in compatible with CYBLE-014008-00CYBLE-014008-00No information about compatibility with  CYBLE-022001-00CYBLE-022001-00 CYBLE-222005-00 and CYBLE-222014-01 found on the website these are 10 x 10x 1.8 mm So wait for the response from Cypress and if there is no programming module kit available / planned, you would have to go with the JTAG connector, as mention above.

    If you plan to use a larger batch, they could help you with programming them in the factory.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dominik.kania
    0 dominik.kania over 9 years ago in reply to koudelad

    David, just as an update - there is a bespoke programming kit that Cypress recommended for this specific chip. Not cheap at ~$250 but will last 10,000+ manual programming cycles. Thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 9 years ago

    Normally your custom card would be designed to include a programming connector.

    As mentioned direct programming adapters can be expensive because it is hard to make robust connectors at the small pitch needed.

    I have not seen a socket or adapter connector for this module.

    You could try to build a programming fixture with a small clamp and some needle probes but it will be very fiddly.