Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum I need an OLED display, but I can't find it
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 80 subscribers
  • Views 981 views
  • Users 0 members are here
  • oled
  • pic18f
  • stm32f407
  • amoled
Related

I need an OLED display, but I can't find it

ltomi91
ltomi91 over 9 years ago

Hi Everybody!

 

I want to use in my project an OLED display with following parameters:

- the module (or viewing area) height is ~ 60mm

- color (RGB), graphic

- with touch

- if possible, with simple interface

 

I want to show some figure, text and simple animation on this display, but these should look really nice. So I think the resolution min. 480*800, but I have no experience in this topic. And the type is PMOLED or AMOLED.. I think the AMOLED version is better.

I've been surfing the web, but I did not find this display at all, so I was thinking of using a mobile phone display. But the result is same, no technical documents to any OLED mobile phone display (... and distributor).

I can use PIC and STM32F407 microcontrollers, but I am also interested to other solutions.

 

So my question is: where can I found an OLED displays refer to this topic?

 

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • ltomi91
    ltomi91 over 9 years ago in reply to koudelad +1
    Thank you the answer! Unfortunately, I need just a few displays. I found a potential display, but without any info: http://www.diytrade.com/china/pd/15957415/PA480272A_480xRGBx272_AMOLED_Graphic_Display_Module…
  • koudelad
    0 koudelad over 9 years ago

    Hello,

     

    I am afraid that there are only small OLED displays ( < 2 " ) available in small quantities, mainly the cyan (+ yellow) variant. I tried to google the biggest size just out of curiosity and it seems it is not easy to manufacture larger displays: https://en.wikipedia.org/wiki/OLED (see the Fabrication chapter).

     

    If you plan to sell your device in big volumes, send a quote to some display manufacturers and see what kind of response you get. It is usual that some components for cell phones are made only in large volumes for big customers with contracts (and a lot of money), the specifications and other documents are not public.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ltomi91
    0 ltomi91 over 9 years ago in reply to koudelad

    Thank you the answer!

     

    Unfortunately, I need just a few displays.

    I found a potential display, but without any info: http://www.diytrade.com/china/pd/15957415/PA480272A_480xRGBx272_AMOLED_Graphic_Display_Module.html

    ... so I hope that find a description of mobile phone oled display, or I stay at the TFT.

     

    Edit: if I will find an (RGB) OLED display in portrait position (so 720x1280 resolution), can I use in landscape position?

     

    Thanks.