Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum PIC18LF67K40: Debug mode
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 3 answers
  • Subscribers 81 subscribers
  • Views 1515 views
  • Users 0 members are here
Related

PIC18LF67K40: Debug mode

angelj
angelj over 7 years ago

Does the PIC18LF67K40 work only in onchip integrated debug mode or can also in incircuit serial programming via two pins?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 7 years ago +1
    I hate fanciness where technical writing should be done Good job koudelad
Parents
  • angelj
    0 angelj over 7 years ago

    @David Koudela and BB-Sphere (Clem),

    In the datasheet of PIC18LF67K40(page 4), three features are listed under the section "Programming/Debug Features"

    1.In-Circuit Serial ProgrammingTm (ICSPTm) via Two Pins

    2. In-Circuit Debug (ICD) with Three Breakpoints via Two Pins

    3. Debug Integrated On-Chip

    But in the next page(5), it is mentioned as "I" under the column "Debug" of Table 1.The legend corresponding to I says "Debugging Methods: (I) – Integrated on Chip"

     

    So my question is whether this particular PIC has only ' Debug Integrated On-Chip" feature. Orelse, we can do debug using debugger like PICit3.

     

    Link for datasheet: http://ww1.microchip.com/downloads/en/DeviceDoc/PIC18(L)F67K40%20Data%20Sheet%2040001841D.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • koudelad
    0 koudelad over 7 years ago in reply to angelj

    The datasheet list the points you mentioned, but I am afraid it is just "marketing".

     

    In order to support debugging, the PIC has an on chip circuitry.  Have a look at page 811 of the datasheet, it lists the possible compilers, simulators, programmers and debugger. PICkit3 or newer (please note there is a PICkit4) will work just fine. Or ICD3 (there is also ICD4 which should be OK). You will need to connect the five pins mentioned in my previous post.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • koudelad
    0 koudelad over 7 years ago in reply to angelj

    The datasheet list the points you mentioned, but I am afraid it is just "marketing".

     

    In order to support debugging, the PIC has an on chip circuitry.  Have a look at page 811 of the datasheet, it lists the possible compilers, simulators, programmers and debugger. PICkit3 or newer (please note there is a PICkit4) will work just fine. Or ICD3 (there is also ICD4 which should be OK). You will need to connect the five pins mentioned in my previous post.

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer