Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum 96Boards Dual Camera Mezz Out of Box image - failed to find mode "1920x1080" for connector 42
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 80 subscribers
  • Views 3635 views
  • Users 0 members are here
  • imaging
  • mezzanine
  • ultra96
  • 96boards
  • modules
Related

96Boards Dual Camera Mezz Out of Box image - failed to find mode "1920x1080" for connector 42

jomoenginer
jomoenginer over 5 years ago

I have been attempting to run the Out of Box image as per the 96Boards Dual Camera Mezz Getting Started Guide, but I keep getting an error and no image is displayed on the screen. I have rebooted the board while connected to a monitor and still no luck.

 

Any suggestions on how to resolve this?

 

Ref:

Getting Started Guide

96Boards_Dual_Camera_Mezz_GSG.pdf

 

96Board Dual Camer Mezz page with Out of Box Image

96Boards ON Semiconductor Dual Camera Mezzanine | element14 | Design Center

 

I've tried this with multiple Monitors as well as connecting to a TV, but I get the same error:

 

root@ultra96v2-2020-1:~# run_1920_1080
725
failed to find mode "1920x1080" for connector 42
failed to create dumb buffer: Invalid argument
testing 1920x1080@YUYV overlay plane 38
Setting pipeline to PAUSED ...
ERROR: Pipeline doesn't want to pause.
ERROR: from element /GstPipeline:pipeline0/GstKMSSink:kmssink0: Could not get allowed GstCaps of device
Additional debug info:
../../../git/sys/kms/gstkmssink.c(1102): gst_kms_sink_start (): /GstPipeline:pipeline0/GstKMSSink:kmssink0:
driver does not provide mode settings configuration
Setting pipeline to NULL ...
Freeing pipeline ...
/usr/bin/run_1920_1080: line 20: kill: (725) - No such process
root@ultra96v2-2020-1:~# t

 

 

Boot message:

 

A Couple of message to note:

  xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0020000.mipi_csi2_rx_subsystem was not initialized!

 

  xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0080000.v_proc_ss was not initialized

 

96Boards Dual Camera Mezz Out of Box image error


[    2.990368] rtc_zynqmp ffa60000.rtc: registered as rtc0
[    2.995093] i2c /dev entries driver
[    2.999107] xilinx-video amba_pl@0:vcap_csi: device registered
[    3.004837] xilinx-csi2rxss a0020000.mipi_csi2_rx_subsystem: Xilinx CSI2 Rx Subsystem device found!
[    3.013283] xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0020000.mipi_csi2_rx_subsystem was not initialized!
[    3.025050] xilinx-tpg a0050000.v_tpg: invalid number of ports 0
[    3.030062] xilinx-tpg: probe of a0050000.v_tpg failed with error -22
[    3.036692] xilinx-vpss-scaler a0080000.v_proc_ss: xlnx,v-vpss-scaler-2.2 - compatible string is getting deprecated!
[    3.046994] xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0080000.v_proc_ss was not initialized!
[    3.056618] xilinx-vpss-scaler a0080000.v_proc_ss: Num Hori Taps 8
[    3.062754] xilinx-vpss-scaler a0080000.v_proc_ss: Num Vert Taps 8
[    3.068895] xilinx-vpss-scaler a0080000.v_proc_ss: VPSS Scaler Probe Successful
[    3.076300] xilinx-vtc a0060000.v_tc: device found, version 6.020
[    3.082283] usbcore: registered new interface driver uvcvideo

 

Full Boot Message

 

Xilinx Zynq MP First Stage Boot Loader 

Release 2020.1   Aug 14 2020  -  22:53:13
NOTICE:  ATF running on XCZU3EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE:  BL31: v2.2(release):v1.1-5588-g5918e656e
NOTICE:  BL31: Built : 22:34:55, Aug 14 2020


U-Boot 2020.01 (Aug 18 2020 - 17:33:39 +0000)

Model: Avnet Ultra96 Rev1
Board: Xilinx ZynqMP
DRAM:  2 GiB
PMUFW:    v1.1
EL Level:    EL2
Chip ID:    zu3eg
NAND:  0 MiB
MMC:   mmc@ff160000: 0, mmc@ff170000: 1
In:    serial@ff010000
Out:   serial@ff010000
Err:   serial@ff010000
Bootmode: SD_MODE
Reset reason:    EXTERNAL 
Net:   No ethernet found.
Hit any key to stop autoboot:  2     1     0 
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
Found U-Boot script /boot.scr
2007 bytes read in 20 ms (97.7 KiB/s)
## Executing script at 20000000
8313964 bytes read in 623 ms (12.7 MiB/s)
## Loading kernel from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'kernel@1' kernel subimage
     Description:  Linux kernel
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x100000f4
     Data Size:    8251525 Bytes = 7.9 MiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x00080000
     Entry Point:  0x00080000
     Hash algo:    sha256
     Hash value:   22ed1c58ad614712b771a0e27ff96d52d6b3269321ee423885176b4c41550f32
   Verifying Hash Integrity ... sha256+ OK
## Loading fdt from FIT Image at 10000000 ...
   Using 'conf@system-top.dtb' configuration
   Trying 'fdt@system-top.dtb' fdt subimage
     Description:  Flattened Device Tree blob
     Type:         Flat Device Tree
     Compression:  uncompressed
     Data Start:   0x107dea8c
     Data Size:    60535 Bytes = 59.1 KiB
     Architecture: AArch64
     Hash algo:    sha256
     Hash value:   239f2beeb0c26cfc03521c3c00c8931a234b07770ea13e7fa072f91e0669b391
   Verifying Hash Integrity ... sha256+ OK
   Booting using the fdt blob at 0x107dea8c
   Uncompressing Kernel Image
   Loading Device Tree to 000000000ffee000, end 000000000ffffc76 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.4.0-xilinx-v2020.1 (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP Tue Aug 18 16:15:52 UTC 2020
[    0.000000] Machine model: Avnet Ultra96 Rev1
[    0.000000] earlycon: cdns0 at MMIO 0x00000000ff010000 (options '115200n8')
[    0.000000] printk: bootconsole [cdns0] enabled
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x000000003ed40000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node rproc@3ed400000, compatible id shared-dma-pool
[    0.000000] cma: Reserved 512 MiB at 0x000000005fc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] psci: SMC Calling Convention v1.1
[    0.000000] percpu: Embedded 22 pages/cpu s49944 r8192 d31976 u90112
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] Speculative Store Bypass Disable mitigation not required
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 515524
[    0.000000] Kernel command line: earlycon console=ttyPS0,115200 clk_ignore_unused root=/dev/mmcblk0p2 rw rootwait cma=512M
[    0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 1512432K/2094848K available (11836K kernel code, 690K rwdata, 3684K rodata, 704K init, 516K bss, 58128K reserved, 524288K cma-reserved)
[    0.000000] rcu: Hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] random: get_random_bytes called from start_kernel+0x2a8/0x42c with crng_init=0
[    0.000000] arch_timer: cp15 timer(s) running at 100.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171024e7e0, max_idle_ns: 440795205315 ns
[    0.000004] sched_clock: 56 bits at 100MHz, resolution 10ns, wraps every 4398046511100ns
[    0.008479] Console: colour dummy device 80x25
[    0.012487] Calibrating delay loop (skipped), value calculated using timer frequency.. 200.00 BogoMIPS (lpj=400000)
[    0.022840] pid_max: default: 32768 minimum: 301
[    0.027602] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.034788] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[    0.043875] ASID allocator initialised with 32768 entries
[    0.047999] rcu: Hierarchical SRCU implementation.
[    0.052944] EFI services will not be available.
[    0.057350] smp: Bringing up secondary CPUs ...
[    0.062090] Detected VIPT I-cache on CPU1
[    0.062137] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.062536] Detected VIPT I-cache on CPU2
[    0.062556] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[    0.062915] Detected VIPT I-cache on CPU3
[    0.062934] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[    0.062984] smp: Brought up 1 node, 4 CPUs
[    0.097142] SMP: Total of 4 processors activated.
[    0.101814] CPU features: detected: 32-bit EL0 Support
[    0.106918] CPU features: detected: CRC32 instructions
[    0.112057] CPU: All CPU(s) started at EL2
[    0.116100] alternatives: patching kernel code
[    0.121618] devtmpfs: initialized
[    0.130505] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.134606] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.156620] xor: measuring software checksum speed
[    0.193587]    8regs     :  2375.000 MB/sec
[    0.233614]    32regs    :  2725.000 MB/sec
[    0.273645]    arm64_neon:  2365.000 MB/sec
[    0.273686] xor: using function: 32regs (2725.000 MB/sec)
[    0.277562] pinctrl core: initialized pinctrl subsystem
[    0.283681] NET: Registered protocol family 16
[    0.288702] DMA: preallocated 256 KiB pool for atomic allocations
[    0.293240] audit: initializing netlink subsys (disabled)
[    0.298660] audit: type=2000 audit(0.240:1): state=initialized audit_enabled=0 res=1
[    0.306304] cpuidle: using governor menu
[    0.310343] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.331356] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[    0.332410] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[    0.339080] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.345739] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[    1.426755] DRBG: Continuing without Jitter RNG
[    1.503595] raid6: neonx8   gen()  1546 MB/s
[    1.571612] raid6: neonx8   xor()  1466 MB/s
[    1.639665] raid6: neonx4   gen()  1489 MB/s
[    1.707724] raid6: neonx4   xor()  1430 MB/s
[    1.775803] raid6: neonx2   gen()  1135 MB/s
[    1.843810] raid6: neonx2   xor()  1189 MB/s
[    1.911900] raid6: neonx1   gen()   741 MB/s
[    1.979896] raid6: neonx1   xor()   895 MB/s
[    2.047943] raid6: int64x8  gen()  1166 MB/s
[    2.116021] raid6: int64x8  xor()   763 MB/s
[    2.184086] raid6: int64x4  gen()   984 MB/s
[    2.252113] raid6: int64x4  xor()   740 MB/s
[    2.320199] raid6: int64x2  gen()   684 MB/s
[    2.388220] raid6: int64x2  xor()   600 MB/s
[    2.456265] raid6: int64x1  gen()   453 MB/s
[    2.524301] raid6: int64x1  xor()   460 MB/s
[    2.524343] raid6: using algorithm neonx8 gen() 1546 MB/s
[    2.528293] raid6: .... xor() 1466 MB/s, rmw enabled
[    2.533223] raid6: using neon recovery algorithm
[    2.538631] iommu: Default domain type: Translated 
[    2.542919] SCSI subsystem initialized
[    2.546541] usbcore: registered new interface driver usbfs
[    2.551851] usbcore: registered new interface driver hub
[    2.557124] usbcore: registered new device driver usb
[    2.562169] mc: Linux media interface: v0.10
[    2.566372] videodev: Linux video capture interface: v2.00
[    2.571820] pps_core: LinuxPPS API ver. 1 registered
[    2.576733] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    2.585828] PTP clock support registered
[    2.589723] EDAC MC: Ver: 3.0.0
[    2.593289] zynqmp-ipi-mbox mailbox@ff990400: Registered ZynqMP IPI mbox with TX/RX channels.
[    2.601551] zynqmp-ipi-mbox mailbox@ff90000: Registered ZynqMP IPI mbox with TX/RX channels.
[    2.609801] FPGA manager framework
[    2.613207] Advanced Linux Sound Architecture Driver Initialized.
[    2.619455] Bluetooth: Core ver 2.22
[    2.622680] NET: Registered protocol family 31
[    2.627077] Bluetooth: HCI device and connection manager initialized
[    2.633395] Bluetooth: HCI socket layer initialized
[    2.638237] Bluetooth: L2CAP socket layer initialized
[    2.643259] Bluetooth: SCO socket layer initialized
[    2.648524] clocksource: Switched to clocksource arch_sys_counter
[    2.654281] VFS: Disk quotas dquot_6.6.0
[    2.658095] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    2.669202] NET: Registered protocol family 2
[    2.669672] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[    2.677725] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    2.685657] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[    2.693156] TCP: Hash tables configured (established 16384 bind 16384)
[    2.699418] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    2.706006] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    2.713193] NET: Registered protocol family 1
[    2.717709] RPC: Registered named UNIX socket transport module.
[    2.723273] RPC: Registered udp transport module.
[    2.727940] RPC: Registered tcp transport module.
[    2.732608] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    2.739281] PCI: CLS 0 bytes, default 64
[    2.743477] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    2.750174] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    2.758684] Initialise system trusted keyrings
[    2.762218] workingset: timestamp_bits=46 max_order=19 bucket_order=0
[    2.769344] NFS: Registering the id_resolver key type
[    2.773539] Key type id_resolver registered
[    2.777675] Key type id_legacy registered
[    2.781659] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    2.788331] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    2.807735] NET: Registered protocol family 38
[    2.807782] Key type asymmetric registered
[    2.810608] Asymmetric key parser 'x509' registered
[    2.815472] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[    2.822804] io scheduler mq-deadline registered
[    2.827301] io scheduler kyber registered
[    2.832010] GPIO IRQ not connected
[    2.834665] XGpio: gpio@a0040000: registered, base is 504
[    2.841779] xilinx-frmbuf a0000000.v_frmbuf_wr: Xilinx AXI frmbuf DMA_DEV_TO_MEM
[    2.847433] xilinx-frmbuf a0000000.v_frmbuf_wr: Xilinx AXI FrameBuffer Engine Driver Probed!!
[    2.855954] xilinx-frmbuf a00c0000.v_frmbuf_rd: Xilinx AXI frmbuf DMA_MEM_TO_DEV
[    2.863252] xilinx-frmbuf a00c0000.v_frmbuf_rd: Xilinx AXI FrameBuffer Engine Driver Probed!!
[    2.898012] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    2.902948] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    2.909710] brd: module loaded
[    2.915394] loop: module loaded
[    2.916359] mtdoops: mtd device (mtddev=name/number) must be supplied
[    2.920671] libphy: Fixed MDIO Bus: probed
[    2.924372] tun: Universal TUN/TAP device driver, 1.6
[    2.928502] CAN device driver interface
[    2.933150] usbcore: registered new interface driver asix
[    2.937624] usbcore: registered new interface driver ax88179_178a
[    2.943636] usbcore: registered new interface driver cdc_ether
[    2.949430] usbcore: registered new interface driver net1080
[    2.955056] usbcore: registered new interface driver cdc_subset
[    2.960936] usbcore: registered new interface driver zaurus
[    2.966484] usbcore: registered new interface driver cdc_ncm
[    2.973017] usbcore: registered new interface driver uas
[    2.977385] usbcore: registered new interface driver usb-storage
[    2.983509] gadgetfs: USB Gadget filesystem, version 24 Aug 2004
[    2.989815] rtc_zynqmp ffa60000.rtc: registered as rtc0
[    2.994550] i2c /dev entries driver
[    2.998569] xilinx-video amba_pl@0:vcap_csi: device registered
[    3.004283] xilinx-csi2rxss a0020000.mipi_csi2_rx_subsystem: Xilinx CSI2 Rx Subsystem device found!
[    3.012740] xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0020000.mipi_csi2_rx_subsystem was not initialized!
[    3.024495] xilinx-tpg a0050000.v_tpg: invalid number of ports 0
[    3.029518] xilinx-tpg: probe of a0050000.v_tpg failed with error -22
[    3.036142] xilinx-vpss-scaler a0080000.v_proc_ss: xlnx,v-vpss-scaler-2.2 - compatible string is getting deprecated!
[    3.046449] xilinx-video amba_pl@0:vcap_csi: Entity type for entity a0080000.v_proc_ss was not initialized!
[    3.056072] xilinx-vpss-scaler a0080000.v_proc_ss: Num Hori Taps 8
[    3.062211] xilinx-vpss-scaler a0080000.v_proc_ss: Num Vert Taps 8
[    3.068351] xilinx-vpss-scaler a0080000.v_proc_ss: VPSS Scaler Probe Successful
[    3.075752] xilinx-vtc a0060000.v_tc: device found, version 6.020
[    3.081738] usbcore: registered new interface driver uvcvideo
[    3.087379] USB Video Class driver (1.1.1)
[    3.092132] Bluetooth: HCI UART driver ver 2.3
[    3.095861] Bluetooth: HCI UART protocol H4 registered
[    3.100960] Bluetooth: HCI UART protocol BCSP registered
[    3.106252] Bluetooth: HCI UART protocol LL registered
[    3.111340] Bluetooth: HCI UART protocol ATH3K registered
[    3.116715] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    3.122967] Bluetooth: HCI UART protocol Intel registered
[    3.128307] Bluetooth: HCI UART protocol QCA registered
[    3.133513] usbcore: registered new interface driver bcm203x
[    3.139154] usbcore: registered new interface driver bpa10x
[    3.144668] usbcore: registered new interface driver bfusb
[    3.150116] usbcore: registered new interface driver btusb
[    3.155581] usbcore: registered new interface driver ath3k
[    3.161108] EDAC MC: ECC not enabled
[    3.164706] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    3.177173] sdhci: Secure Digital Host Controller Interface driver
[    3.182789] sdhci: Copyright(c) Pierre Ossman
[    3.187113] sdhci-pltfm: SDHCI platform and OF driver helper
[    3.193184] ledtrig-cpu: registered to indicate activity on CPUs
[    3.198758] zynqmp_firmware_probe Platform Management API v1.1
[    3.204503] zynqmp_firmware_probe Trustzone version v1.0
[    3.213383] zynqmp-pinctrl firmware:zynqmp-firmware:pinctrl: zynqmp pinctrl initialized
[    3.242139] alg: No test for xilinx-zynqmp-aes (zynqmp-aes)
[    3.242397] zynqmp_aes zynqmp_aes: AES Successfully Registered
[    3.242397] 

[    3.249637] alg: No test for xilinx-keccak-384 (zynqmp-keccak-384)
[    3.255846] alg: No test for xilinx-zynqmp-rsa (zynqmp-rsa)
[    3.261416] usbcore: registered new interface driver usbhid
[    3.266637] usbhid: USB HID core driver
[    3.270676] xlnk xlnk: Major 243
[    3.273759] xlnk xlnk: xlnk driver loaded
[    3.277624] xlnk xlnk: xlnk_pdev is not null
[    3.284350] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    3.288627] usbcore: registered new interface driver snd-usb-audio
[    3.295404] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    3.302632] Initializing XFRM netlink socket
[    3.306266] NET: Registered protocol family 10
[    3.311070] Segment Routing with IPv6
[    3.314348] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.320491] NET: Registered protocol family 17
[    3.324520] NET: Registered protocol family 15
[    3.328933] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    3.341802] can: controller area network core (rev 20170425 abi 9)
[    3.347980] NET: Registered protocol family 29
[    3.352356] can: raw protocol (rev 20170425)
[    3.356593] can: broadcast manager protocol (rev 20170425 t)
[    3.362219] can: netlink gateway (rev 20190810) max_hops=1
[    3.367778] Bluetooth: RFCOMM TTY layer initialized
[    3.372521] Bluetooth: RFCOMM socket layer initialized
[    3.377628] Bluetooth: RFCOMM ver 1.11
[    3.381346] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.386608] Bluetooth: BNEP filters: protocol multicast
[    3.391800] Bluetooth: BNEP socket layer initialized
[    3.396728] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.402613] Bluetooth: HIDP socket layer initialized
[    3.407715] 9pnet: Installing 9P2000 support
[    3.411807] Key type dns_resolver registered
[    3.416396] registered taskstats version 1
[    3.420090] Loading compiled-in X.509 certificates
[    3.425316] Btrfs loaded, crc32c=crc32c-generic
[    3.440452] ff000000.serial: ttyPS1 at MMIO 0xff000000 (irq = 40, base_baud = 6249999) is a xuartps
[    3.444433] ff010000.serial: ttyPS0 at MMIO 0xff010000 (irq = 41, base_baud = 6249999) is a xuartps
[    3.458556] printk: console [ttyPS0] enabled
[    3.458556] printk: console [ttyPS0] enabled
[    3.462864] printk: bootconsole [cdns0] disabled
[    3.462864] printk: bootconsole [cdns0] disabled
[    3.472012] of-fpga-region fpga-full: FPGA Region probed
[    3.482959] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    3.489571] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    3.496694] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    3.503809] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    3.510926] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    3.518050] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    3.525168] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    3.532286] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    3.539406] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    3.546606] xilinx-zynqmp-dma ffa80000.dma: ZynqMP DMA driver Probe success
[    3.553721] xilinx-zynqmp-dma ffa90000.dma: ZynqMP DMA driver Probe success
[    3.560834] xilinx-zynqmp-dma ffaa0000.dma: ZynqMP DMA driver Probe success
[    3.567952] xilinx-zynqmp-dma ffab0000.dma: ZynqMP DMA driver Probe success
[    3.575070] xilinx-zynqmp-dma ffac0000.dma: ZynqMP DMA driver Probe success
[    3.582190] xilinx-zynqmp-dma ffad0000.dma: ZynqMP DMA driver Probe success
[    3.589307] xilinx-zynqmp-dma ffae0000.dma: ZynqMP DMA driver Probe success
[    3.596424] xilinx-zynqmp-dma ffaf0000.dma: ZynqMP DMA driver Probe success
[    3.603795] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
[    3.615655] zynqmp_clk_divider_set_rate() set divider failed for spi1_ref_div1, ret = -13
[    3.624478] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    3.635213] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    3.643275] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    3.651859] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.664408] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.677133] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    3.687320] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.694346] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.700954] [drm] No driver support for vblank timestamp query.
[    3.706966] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffffc010cd78f0)
[    3.846935] random: fast init done
[    7.831159] [drm] Cannot find any crtc or sizes
[    7.835991] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    7.844097] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    7.854387] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    7.860943] xilinx-axipmon fd0b0000.perf-monitor: Probed Xilinx APM
[    7.867450] xilinx-axipmon fd490000.perf-monitor: Probed Xilinx APM
[    7.873964] xilinx-axipmon ffa10000.perf-monitor: Probed Xilinx APM
[    7.880980] dwc3 fe200000.dwc3: Failed to get clk 'ref': -2
[    7.886777] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[    7.898324] dwc3 fe300000.dwc3: Failed to get clk 'ref': -2
[    7.904106] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:1 protocol:3 pll_locked:yes
[    7.914399] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    7.919892] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    7.927662] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x0000000202010010
[    7.937077] xhci-hcd xhci-hcd.0.auto: irq 55, io mem 0xfe300000
[    7.943387] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.04
[    7.951658] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    7.958875] usb usb1: Product: xHCI Host Controller
[    7.963744] usb usb1: Manufacturer: Linux 5.4.0-xilinx-v2020.1 xhci-hcd
[    7.970349] usb usb1: SerialNumber: xhci-hcd.0.auto
[    7.975541] hub 1-0:1.0: USB hub found
[    7.979329] hub 1-0:1.0: 1 port detected
[    7.983476] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    7.988974] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    7.996634] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed
[    8.003213] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    8.011383] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.04
[    8.019658] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    8.026878] usb usb2: Product: xHCI Host Controller
[    8.031752] usb usb2: Manufacturer: Linux 5.4.0-xilinx-v2020.1 xhci-hcd
[    8.038357] usb usb2: SerialNumber: xhci-hcd.0.auto
[    8.043480] hub 2-0:1.0: USB hub found
[    8.047251] hub 2-0:1.0: 1 port detected
[    8.053063] i2c i2c-0: Added multiplexed i2c bus 2
[    8.057991] i2c i2c-0: Added multiplexed i2c bus 3
[    8.063035] i2c i2c-0: Added multiplexed i2c bus 4
[    8.067977] i2c i2c-0: Added multiplexed i2c bus 5
[    8.073472] tps65086 6-005e: Failed to read revision register
[    8.316537] usb 1-1: new high-speed USB device number 2 using xhci-hcd
[    8.469012] usb 1-1: New USB device found, idVendor=0424, idProduct=2744, bcdDevice= 2.21
[    8.477202] usb 1-1: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    8.484329] usb 1-1: Product: USB2744
[    8.487982] usb 1-1: Manufacturer: Microchip Tech
[    8.547284] hub 1-1:1.0: USB hub found
[    8.551081] hub 1-1:1.0: 4 ports detected
[    8.611225] usb 2-1: new SuperSpeed Gen 1 USB device number 2 using xhci-hcd
[    8.636912] usb 2-1: New USB device found, idVendor=0424, idProduct=5744, bcdDevice= 2.21
[    8.645094] usb 2-1: New USB device strings: Mfr=2, Product=3, SerialNumber=0
[    8.652230] usb 2-1: Product: USB5744
[    8.655887] usb 2-1: Manufacturer: Microchip Tech
[    8.691279] hub 2-1:1.0: USB hub found
[    8.695079] hub 2-1:1.0: 3 ports detected
[    8.904531] usb 1-1.4: new high-speed USB device number 3 using xhci-hcd
[    8.922683] i2c i2c-0: Added multiplexed i2c bus 6
[    8.928154] ina2xx_adc 7-0040: error configuring the device
[    8.933829] i2c i2c-0: Added multiplexed i2c bus 7
[    8.938769] i2c i2c-0: Added multiplexed i2c bus 8
[    8.943710] i2c i2c-0: Added multiplexed i2c bus 9
[    8.948513] pca954x 0-0075: registered 8 multiplexed busses for I2C switch pca9548
[    8.956117] cdns-i2c ff030000.i2c: 100 kHz mmio ff030000 irq 30
[    8.963000] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer with timeout 60s
[    8.970506] cdns-wdt ff150000.watchdog: Xilinx Watchdog Timer with timeout 10s
[    9.007198] mmc0: SDHCI controller on ff160000.mmc [ff160000.mmc] using ADMA 64-bit
[    9.015660] sdhci-arasan ff170000.mmc: allocated mmc-pwrseq
[    9.022271] usb 1-1.4: New USB device found, idVendor=0424, idProduct=2740, bcdDevice= 2.00
[    9.030625] usb 1-1.4: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[    9.037930] usb 1-1.4: Product: Hub Controller
[    9.042364] usb 1-1.4: Manufacturer: Microchip Tech
[    9.067917] mmc1: SDHCI controller on ff170000.mmc [ff170000.mmc] using ADMA 64-bit
[    9.079546] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    9.086743] rtc_zynqmp ffa60000.rtc: setting system clock to 1970-01-01T00:00:12 UTC (12)
[    9.094923] of_cfs_init
[    9.097394] of_cfs_init: OK
[    9.100372] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[    9.116785] mmc0: new high speed SDXC card at address 0001
[    9.122796] mmcblk0: mmc0:0001 00000 59.6 GiB 
[    9.128638]  mmcblk0: p1 p2
[    9.138996] mmc1: new high speed SDIO card at address 0001
[    9.237401] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[    9.243932] clk: Not disabling unused clocks
[    9.248194] ALSA device list:
[    9.251151]   #0: DisplayPort monitor
[    9.255278] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[    9.263900] cfg80211: failed to load regulatory.db
[    9.304569] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    9.312694] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    9.332092] devtmpfs: mounted
[    9.335362] Freeing unused kernel memory: 704K
[    9.339882] Run /sbin/init as init process
[    9.426708] random: crng init done

INIT: version 2.88 booting

Starting udev
[    9.885600] udevd[165]: starting version 3.2.8
[    9.953910] udevd[166]: starting eudev-3.2.8
[   10.116090] mali: loading out-of-tree module taints kernel.
[   10.122654] AP1302 4-003c: Probe: AP1302
[   10.126772] debugfs: Directory '4-003c' with parent 'regmap' already present!
[   10.166396] zynqmp_r5_remoteproc zynqmp-rpu: RPU core_conf: split
[   10.172958] remoteproc remoteproc0: r5@0 is available
[   10.221737] AP1302 4-003c: AP1302 Chip ID is 0x265
[   10.237426] AP1302 4-003c: AP1302 Chip Rev is 0x206
[   10.242412] AP1302 4-003c: Start to load firmware.
[   10.761329] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
[   16.670244] [drm] Cannot find any crtc or sizes
[   16.762099] AP1302 4-003c: Load firmware successfully.
[   16.768932] AP1302 4-003c: AP1302 probe Success Done
[   16.843826] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
Wed Aug 19 04:06:10 UTC 2020

Starting Ultra96 AP setup daemon.

Turning Ultra96 WiFi & Bluetooth LEDs ON...done.



[   19.260157] wifi_pm : 0
[   19.262692] wifi_pm : 1
Starting Flask server deamon to serve Ultra96 startup page[   19.265752] wilc_sdio mmc1:0001:1: Driver Initializing success
[   19.279223] WILC POWER UP
[   19.281906] wilc_sdio mmc1:0001:1: SDIO speed: 50000000
[   19.287416] wilc_sdio mmc1:0001:1: chipid 003000d0
.


INIT: Entering runlevel: 5


Starting system message bus: dbus.

Configuring network interfaces... Successfully initialized wpa_supplicant

done.

Starting Connection Manager

Starting haveged: haveged: listening socket at 3

haveged: haveged starting up






Starting Dropbear SSH server: dropbear.

Starting rpcbind daemon...done.

starting statd: done

Starting bluetooth: bluetoothd.

Starting internet superserver: inetd.

exportfs: can't open /etc/exports for reading

NFS daemon support not enabled in kernel

Starting ntpd: done

Starting syslogd/klogd: haveged: haveged: ver: 1.9.5; arch: generic; vend: ; build: (gcc 9.2.0 CTV); collect: 128K




haveged: haveged: cpu: (VC); data: 16K (D); inst: 16K (D); idx: 11/40; sz: 15456/64452




haveged: haveged: tot tests(BA8): A:1/1 B:1/1 continuous tests(B):  last entropy estimate 7.99804




haveged: haveged: fills: 0, generated: 0 




done

Starting internet superserver: xinetd.

 * Starting Avahi mDNS/DNS-SD Daemon: avahi-daemon

 [A [74G[ ok ]

Starting Telephony daemon

Starting watchdog daemon...done

Starting Linux NFC daemon

Starting tcf-agent: OK


PetaLinux 2020.1 ultra96v2-2020-1 ttyPS0

  • Sign in to reply
  • Cancel
Parents
  • jomoenginer
    0 jomoenginer over 5 years ago

    Looking at the modetest output, it is showing DP-1 as disconnected, yet I know I have a monitor connected.

     

    root@ultra96v2-2020-1:~# modetest -M xlnx
    Encoders:
    id crtc type possible crtcs possible clones
    41 0 TMDS 0x00000001 0x00000000
    
    
    Connectors:
    id encoder status name size (mm) modes encoders
    42 0 disconnected DP-1            0x0 0 41

     

    I've tested the cable on another device and it works just fine, so I am not clear as to why the mDP port of the Ultra96-V2 is not picking up a monitor/

     

    any thoughts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 5 years ago in reply to jomoenginer

    I think I may have found my issue.  in the Ultra96-V2 Getting Started Guide v2.0 it states:

    HDMI Monitor
    o Requires Active miniDP-to-HDMI adapter or cable

     

    The cable I have appears to be a Passive miniDP to HDMI cable, so I've ordered an Active miniDP to HDMI cable. Hopefully that resolves the issue.

     

    The 96boards Dual Camera Mezz GSG does not state this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 5 years ago in reply to jomoenginer

    With the Active miniDP to HDMI cable, I can get info from the monitor. However, it appears I do not have a monitor that supports 1920x1080. 

    It looks like something else to purchase.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jomoenginer
    0 jomoenginer over 5 years ago in reply to jomoenginer

    Okay, after purchasing a cheap Acer 27" 1080p monitor, I finally have an image from the Dual Camera Mezz.

     

    However, this did take some effort in that I had to run the  "run_1920_1080" script and reboot the board multiple times.

     

    An error is seen when scanning the monitor at first:

    root@ultra96v2-2020-1:~# modetest -M xlnx
    [   63.592199] zynqmp-display fd4a0000.zynqmp-display: DP-1: EDID is invalid:
    [   63.599097]     [00] BAD  00 ff ff ff ff ff ff 00 ff ff ff ff ff ff ff ff
    [   63.605621]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.612140]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.618660]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.625179]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.631696]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.638219]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.644744]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    Encoders:
    id    crtc    type    possible crtcs    possible clones    
    41    40    TMDS    0x00000001    0x00000000
    
    Connectors:
    id    encoder    status        name        size (mm)    modes    encoders
    42    41    connected    DP-1               600x330        5    41
      modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
      1024x768 60.00 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
      800x600 60.32 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
      800x600 56.25 800 824 896 1024 600 601 603 625 36000 flags: phsync, pvsync; type: driver
      848x480 60.00 848 864 976 1088 480 486 494 517 33750 flags: phsync, pvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      props:
        1 EDID:
            flags: immutable blob
            blobs:
    
            value:
                00ffffffffffff0004727e085ea87003
                251e0103803c2178ea3135a5554ea126
                0c5054a54b00714f81809500b300a9c0
                810081c09040f14480c870381e403020
                350055502100001e000000fd00304b1e
                5515000a202020202020000000fc004b
                323732484c20480a20202020000000ff
                00544e304141303031335730310a01fa
                020325f449900403011412051f132309
                07078301000065030c002000681a0000
                0101304be6023a801871382d40582c45
                0055502100001a011d007251d01e206e
                28550055502100001e8c0ad08a20e02d
                10103e96005550210000180000000000
                00000000000000000000000000000000
                0000000000000000000000000000002d
        2 DPMS:
            flags: enum
            enums: On=0 Standby=1 Suspend=2 Off=3
            value: 0
        5 link-status:
            flags: enum
            enums: Good=0 Bad=1
            value: 0
        6 non-desktop:
            flags: immutable range
            values: 0 1
            value: 0
        4 TILE:
            flags: immutable blob
            blobs:
    
            value:
        20 CRTC_ID:
            flags: object
            value: 40
        43 sync:
            flags: range
            values: 0 1
            value: 0
        44 bpc:
            flags: enum
            enums: 6BPC=6 8BPC=8 10BPC=10 12BPC=12
            value: 8
    
    CRTCs:
    id    fb    pos    size
    40    46    (0,0)    (1920x1080)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      props:
        22 ACTIVE:
            flags: range
            values: 0 1
            value: 1
        23 MODE_ID:
            flags: blob
            blobs:
    
            value:
                6ab102008007b007d007480800003804
                3b044004560400004b00000005000000
                48000000313932307831303830000000
                00000000000000000000000000000000
                00000000
        19 OUT_FENCE_PTR:
            flags: range
            values: 0 18446744073709551615
            value: 0
        24 VRR_ENABLED:
            flags: range
            values: 0 1
            value: 0
        33 output_color:
            flags: enum
            enums: rgb=0 ycrcb444=1 ycrcb422=2 yonly=3
            value: 0
        34 bg_c0:
            flags: range
            values: 0 4095
            value: 0
        35 bg_c1:
            flags: range
            values: 0 4095
            value: 0
        36 bg_c2:
            flags: range
            values: 0 4095
            value: 0
    
    Planes:
    id    crtc    fb    CRTC x,y    x,y    gamma size    possible crtcs
    38    0    0    0,0        0,0    0           0x00000001
      formats: VYUY UYVY YUYV YVYU YU16 YV16 YU24 YV24 NV16 NV61 GREY Y10  BG24 RG24 XB24 XR24 XB30 XR30 YU12 YV12 NV12 NV21 XV15 XV20
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 0
        17 FB_ID:
            flags: object
            value: 0
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 0
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 0
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 0
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 0
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 0
        37 tpg:
            flags: range
            values: 0 1
            value: 0
    39    40    46    0,0        0,0    0           0x00000001
      formats: AB24 AR24 RA24 BA24 BG24 RG24 RA15 BA15 RA12 BA12 RG16 BG16
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 1
        17 FB_ID:
            flags: object
            value: 46
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 40
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 1920
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 1080
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 125829120
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 70778880
        31 alpha:
            flags: range
            values: 0 255
            value: 255
        32 g_alpha_en:
            flags: range
            values: 0 1
            value: 1
    
    Frame buffers:
    id    size    pitch

     

     

    After a few reboots and running the run script, the screen is identified properly.

    root@ultra96v2-2020-1:~# modetest -M xlnx
    Encoders:
    id    crtc    type    possible crtcs    possible clones    
    41    40    TMDS    0x00000001    0x00000000
    
    Connectors:
    id    encoder    status        name        size (mm)    modes    encoders
    42    41    connected    DP-1               600x330        31    41
      modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, nvsync; type: driver
      1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
      1920x1080 59.94 1920 2008 2052 2200 1080 1084 1089 1125 148352 flags: phsync, pvsync; type: driver
      1920x1080 50.00 1920 2448 2492 2640 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
      1680x1050 59.88 1680 1728 1760 1840 1050 1053 1059 1080 119000 flags: phsync, nvsync; type: driver
      1400x1050 59.95 1400 1448 1480 1560 1050 1053 1057 1080 101000 flags: phsync, nvsync; type: driver
      1600x900 60.00 1600 1624 1704 1800 900 901 904 1000 108000 flags: phsync, pvsync; type: driver
      1280x1024 75.02 1280 1296 1440 1688 1024 1025 1028 1066 135000 flags: phsync, pvsync; type: driver
      1280x1024 60.02 1280 1328 1440 1688 1024 1025 1028 1066 108000 flags: phsync, pvsync; type: driver
      1440x900 59.90 1440 1488 1520 1600 900 903 909 926 88750 flags: phsync, nvsync; type: driver
      1280x800 59.91 1280 1328 1360 1440 800 803 809 823 71000 flags: phsync, nvsync; type: driver
      1152x864 75.00 1152 1216 1344 1600 864 865 868 900 108000 flags: phsync, pvsync; type: driver
      1280x720 60.00 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1280x720 60.00 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1280x720 59.94 1280 1390 1430 1650 720 725 730 750 74176 flags: phsync, pvsync; type: driver
      1280x720 50.00 1280 1720 1760 1980 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1024x768 75.03 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; type: driver
      1024x768 60.00 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
      800x600 75.00 800 816 896 1056 600 601 604 625 49500 flags: phsync, pvsync; type: driver
      800x600 60.32 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
      720x576 50.00 720 732 796 864 576 581 586 625 27000 flags: nhsync, nvsync; type: driver
      720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
      720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
      720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
      720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
      640x480 75.00 640 656 720 840 480 481 484 500 31500 flags: nhsync, nvsync; type: driver
      640x480 60.00 640 656 752 800 480 490 492 525 25200 flags: nhsync, nvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      720x400 70.08 720 738 846 900 400 412 414 449 28320 flags: nhsync, pvsync; type: driver
      props:
        1 EDID:
            flags: immutable blob
            blobs:
    
            value:
                00ffffffffffff0004727e085ea87003
                251e0103803c2178ea3135a5554ea126
                0c5054a54b00714f81809500b300a9c0
                810081c09040f14480c870381e403020
                350055502100001e000000fd00304b1e
                5515000a202020202020000000fc004b
                323732484c20480a20202020000000ff
                00544e304141303031335730310a01fa
                020325f449900403011412051f132309
                07078301000065030c002000681a0000
                0101304be6023a801871382d40582c45
                0055502100001a011d007251d01e206e
                28550055502100001e8c0ad08a20e02d
                10103e96005550210000180000000000
                00000000000000000000000000000000
                0000000000000000000000000000002d
        2 DPMS:
            flags: enum
            enums: On=0 Standby=1 Suspend=2 Off=3
            value: 0
        5 link-status:
            flags: enum
            enums: Good=0 Bad=1
            value: 0
        6 non-desktop:
            flags: immutable range
            values: 0 1
            value: 0
        4 TILE:
            flags: immutable blob
            blobs:
    
            value:
        20 CRTC_ID:
            flags: object
            value: 40
        43 sync:
            flags: range
            values: 0 1
            value: 0
        44 bpc:
            flags: enum
            enums: 6BPC=6 8BPC=8 10BPC=10 12BPC=12
            value: 8
    
    CRTCs:
    id    fb    pos    size
    40    46    (0,0)    (1920x1080)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      props:
        22 ACTIVE:
            flags: range
            values: 0 1
            value: 1
        23 MODE_ID:
            flags: blob
            blobs:
    
            value:
                6ab102008007b007d007480800003804
                3b044004560400004b00000005000000
                48000000313932307831303830000000
                00000000000000000000000000000000
                00000000
        19 OUT_FENCE_PTR:
            flags: range
            values: 0 18446744073709551615
            value: 0
        24 VRR_ENABLED:
            flags: range
            values: 0 1
            value: 0
        33 output_color:
            flags: enum
            enums: rgb=0 ycrcb444=1 ycrcb422=2 yonly=3
            value: 0
        34 bg_c0:
            flags: range
            values: 0 4095
            value: 0
        35 bg_c1:
            flags: range
            values: 0 4095
            value: 0
        36 bg_c2:
            flags: range
            values: 0 4095
            value: 0
    
    Planes:
    id    crtc    fb    CRTC x,y    x,y    gamma size    possible crtcs
    38    0    0    0,0        0,0    0           0x00000001
      formats: VYUY UYVY YUYV YVYU YU16 YV16 YU24 YV24 NV16 NV61 GREY Y10  BG24 RG24 XB24 XR24 XB30 XR30 YU12 YV12 NV12 NV21 XV15 XV20
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 0
        17 FB_ID:
            flags: object
            value: 0
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 0
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 0
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 0
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 0
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 0
        37 tpg:
            flags: range
            values: 0 1
            value: 0
    39    40    46    0,0        0,0    0           0x00000001
      formats: AB24 AR24 RA24 BA24 BG24 RG24 RA15 BA15 RA12 BA12 RG16 BG16
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 1
        17 FB_ID:
            flags: object
            value: 46
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 40
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 1920
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 1080
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 125829120
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 70778880
        31 alpha:
            flags: range
            values: 0 255
            value: 0
        32 g_alpha_en:
            flags: range
            values: 0 1
            value: 1
    
    Frame buffers:
    id    size    pitch

     

    The Camera output finally shows up on the monitor.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jomoenginer
    0 jomoenginer over 5 years ago in reply to jomoenginer

    Okay, after purchasing a cheap Acer 27" 1080p monitor, I finally have an image from the Dual Camera Mezz.

     

    However, this did take some effort in that I had to run the  "run_1920_1080" script and reboot the board multiple times.

     

    An error is seen when scanning the monitor at first:

    root@ultra96v2-2020-1:~# modetest -M xlnx
    [   63.592199] zynqmp-display fd4a0000.zynqmp-display: DP-1: EDID is invalid:
    [   63.599097]     [00] BAD  00 ff ff ff ff ff ff 00 ff ff ff ff ff ff ff ff
    [   63.605621]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.612140]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.618660]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.625179]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.631696]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.638219]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    [   63.644744]     [00] BAD  ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff ff
    Encoders:
    id    crtc    type    possible crtcs    possible clones    
    41    40    TMDS    0x00000001    0x00000000
    
    Connectors:
    id    encoder    status        name        size (mm)    modes    encoders
    42    41    connected    DP-1               600x330        5    41
      modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
      1024x768 60.00 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
      800x600 60.32 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
      800x600 56.25 800 824 896 1024 600 601 603 625 36000 flags: phsync, pvsync; type: driver
      848x480 60.00 848 864 976 1088 480 486 494 517 33750 flags: phsync, pvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      props:
        1 EDID:
            flags: immutable blob
            blobs:
    
            value:
                00ffffffffffff0004727e085ea87003
                251e0103803c2178ea3135a5554ea126
                0c5054a54b00714f81809500b300a9c0
                810081c09040f14480c870381e403020
                350055502100001e000000fd00304b1e
                5515000a202020202020000000fc004b
                323732484c20480a20202020000000ff
                00544e304141303031335730310a01fa
                020325f449900403011412051f132309
                07078301000065030c002000681a0000
                0101304be6023a801871382d40582c45
                0055502100001a011d007251d01e206e
                28550055502100001e8c0ad08a20e02d
                10103e96005550210000180000000000
                00000000000000000000000000000000
                0000000000000000000000000000002d
        2 DPMS:
            flags: enum
            enums: On=0 Standby=1 Suspend=2 Off=3
            value: 0
        5 link-status:
            flags: enum
            enums: Good=0 Bad=1
            value: 0
        6 non-desktop:
            flags: immutable range
            values: 0 1
            value: 0
        4 TILE:
            flags: immutable blob
            blobs:
    
            value:
        20 CRTC_ID:
            flags: object
            value: 40
        43 sync:
            flags: range
            values: 0 1
            value: 0
        44 bpc:
            flags: enum
            enums: 6BPC=6 8BPC=8 10BPC=10 12BPC=12
            value: 8
    
    CRTCs:
    id    fb    pos    size
    40    46    (0,0)    (1920x1080)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      props:
        22 ACTIVE:
            flags: range
            values: 0 1
            value: 1
        23 MODE_ID:
            flags: blob
            blobs:
    
            value:
                6ab102008007b007d007480800003804
                3b044004560400004b00000005000000
                48000000313932307831303830000000
                00000000000000000000000000000000
                00000000
        19 OUT_FENCE_PTR:
            flags: range
            values: 0 18446744073709551615
            value: 0
        24 VRR_ENABLED:
            flags: range
            values: 0 1
            value: 0
        33 output_color:
            flags: enum
            enums: rgb=0 ycrcb444=1 ycrcb422=2 yonly=3
            value: 0
        34 bg_c0:
            flags: range
            values: 0 4095
            value: 0
        35 bg_c1:
            flags: range
            values: 0 4095
            value: 0
        36 bg_c2:
            flags: range
            values: 0 4095
            value: 0
    
    Planes:
    id    crtc    fb    CRTC x,y    x,y    gamma size    possible crtcs
    38    0    0    0,0        0,0    0           0x00000001
      formats: VYUY UYVY YUYV YVYU YU16 YV16 YU24 YV24 NV16 NV61 GREY Y10  BG24 RG24 XB24 XR24 XB30 XR30 YU12 YV12 NV12 NV21 XV15 XV20
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 0
        17 FB_ID:
            flags: object
            value: 0
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 0
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 0
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 0
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 0
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 0
        37 tpg:
            flags: range
            values: 0 1
            value: 0
    39    40    46    0,0        0,0    0           0x00000001
      formats: AB24 AR24 RA24 BA24 BG24 RG24 RA15 BA15 RA12 BA12 RG16 BG16
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 1
        17 FB_ID:
            flags: object
            value: 46
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 40
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 1920
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 1080
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 125829120
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 70778880
        31 alpha:
            flags: range
            values: 0 255
            value: 255
        32 g_alpha_en:
            flags: range
            values: 0 1
            value: 1
    
    Frame buffers:
    id    size    pitch

     

     

    After a few reboots and running the run script, the screen is identified properly.

    root@ultra96v2-2020-1:~# modetest -M xlnx
    Encoders:
    id    crtc    type    possible crtcs    possible clones    
    41    40    TMDS    0x00000001    0x00000000
    
    Connectors:
    id    encoder    status        name        size (mm)    modes    encoders
    42    41    connected    DP-1               600x330        31    41
      modes:
        name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, nvsync; type: driver
      1920x1080 60.00 1920 2008 2052 2200 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
      1920x1080 59.94 1920 2008 2052 2200 1080 1084 1089 1125 148352 flags: phsync, pvsync; type: driver
      1920x1080 50.00 1920 2448 2492 2640 1080 1084 1089 1125 148500 flags: phsync, pvsync; type: driver
      1680x1050 59.88 1680 1728 1760 1840 1050 1053 1059 1080 119000 flags: phsync, nvsync; type: driver
      1400x1050 59.95 1400 1448 1480 1560 1050 1053 1057 1080 101000 flags: phsync, nvsync; type: driver
      1600x900 60.00 1600 1624 1704 1800 900 901 904 1000 108000 flags: phsync, pvsync; type: driver
      1280x1024 75.02 1280 1296 1440 1688 1024 1025 1028 1066 135000 flags: phsync, pvsync; type: driver
      1280x1024 60.02 1280 1328 1440 1688 1024 1025 1028 1066 108000 flags: phsync, pvsync; type: driver
      1440x900 59.90 1440 1488 1520 1600 900 903 909 926 88750 flags: phsync, nvsync; type: driver
      1280x800 59.91 1280 1328 1360 1440 800 803 809 823 71000 flags: phsync, nvsync; type: driver
      1152x864 75.00 1152 1216 1344 1600 864 865 868 900 108000 flags: phsync, pvsync; type: driver
      1280x720 60.00 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1280x720 60.00 1280 1390 1430 1650 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1280x720 59.94 1280 1390 1430 1650 720 725 730 750 74176 flags: phsync, pvsync; type: driver
      1280x720 50.00 1280 1720 1760 1980 720 725 730 750 74250 flags: phsync, pvsync; type: driver
      1024x768 75.03 1024 1040 1136 1312 768 769 772 800 78750 flags: phsync, pvsync; type: driver
      1024x768 60.00 1024 1048 1184 1344 768 771 777 806 65000 flags: nhsync, nvsync; type: driver
      800x600 75.00 800 816 896 1056 600 601 604 625 49500 flags: phsync, pvsync; type: driver
      800x600 60.32 800 840 968 1056 600 601 605 628 40000 flags: phsync, pvsync; type: driver
      720x576 50.00 720 732 796 864 576 581 586 625 27000 flags: nhsync, nvsync; type: driver
      720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
      720x480 60.00 720 736 798 858 480 489 495 525 27027 flags: nhsync, nvsync; type: driver
      720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
      720x480 59.94 720 736 798 858 480 489 495 525 27000 flags: nhsync, nvsync; type: driver
      640x480 75.00 640 656 720 840 480 481 484 500 31500 flags: nhsync, nvsync; type: driver
      640x480 60.00 640 656 752 800 480 490 492 525 25200 flags: nhsync, nvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      640x480 59.94 640 656 752 800 480 490 492 525 25175 flags: nhsync, nvsync; type: driver
      720x400 70.08 720 738 846 900 400 412 414 449 28320 flags: nhsync, pvsync; type: driver
      props:
        1 EDID:
            flags: immutable blob
            blobs:
    
            value:
                00ffffffffffff0004727e085ea87003
                251e0103803c2178ea3135a5554ea126
                0c5054a54b00714f81809500b300a9c0
                810081c09040f14480c870381e403020
                350055502100001e000000fd00304b1e
                5515000a202020202020000000fc004b
                323732484c20480a20202020000000ff
                00544e304141303031335730310a01fa
                020325f449900403011412051f132309
                07078301000065030c002000681a0000
                0101304be6023a801871382d40582c45
                0055502100001a011d007251d01e206e
                28550055502100001e8c0ad08a20e02d
                10103e96005550210000180000000000
                00000000000000000000000000000000
                0000000000000000000000000000002d
        2 DPMS:
            flags: enum
            enums: On=0 Standby=1 Suspend=2 Off=3
            value: 0
        5 link-status:
            flags: enum
            enums: Good=0 Bad=1
            value: 0
        6 non-desktop:
            flags: immutable range
            values: 0 1
            value: 0
        4 TILE:
            flags: immutable blob
            blobs:
    
            value:
        20 CRTC_ID:
            flags: object
            value: 40
        43 sync:
            flags: range
            values: 0 1
            value: 0
        44 bpc:
            flags: enum
            enums: 6BPC=6 8BPC=8 10BPC=10 12BPC=12
            value: 8
    
    CRTCs:
    id    fb    pos    size
    40    46    (0,0)    (1920x1080)
      1920x1080 75.00 1920 1968 2000 2120 1080 1083 1088 1110 176490 flags: phsync, pvsync; type: preferred, driver
      props:
        22 ACTIVE:
            flags: range
            values: 0 1
            value: 1
        23 MODE_ID:
            flags: blob
            blobs:
    
            value:
                6ab102008007b007d007480800003804
                3b044004560400004b00000005000000
                48000000313932307831303830000000
                00000000000000000000000000000000
                00000000
        19 OUT_FENCE_PTR:
            flags: range
            values: 0 18446744073709551615
            value: 0
        24 VRR_ENABLED:
            flags: range
            values: 0 1
            value: 0
        33 output_color:
            flags: enum
            enums: rgb=0 ycrcb444=1 ycrcb422=2 yonly=3
            value: 0
        34 bg_c0:
            flags: range
            values: 0 4095
            value: 0
        35 bg_c1:
            flags: range
            values: 0 4095
            value: 0
        36 bg_c2:
            flags: range
            values: 0 4095
            value: 0
    
    Planes:
    id    crtc    fb    CRTC x,y    x,y    gamma size    possible crtcs
    38    0    0    0,0        0,0    0           0x00000001
      formats: VYUY UYVY YUYV YVYU YU16 YV16 YU24 YV24 NV16 NV61 GREY Y10  BG24 RG24 XB24 XR24 XB30 XR30 YU12 YV12 NV12 NV21 XV15 XV20
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 0
        17 FB_ID:
            flags: object
            value: 0
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 0
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 0
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 0
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 0
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 0
        37 tpg:
            flags: range
            values: 0 1
            value: 0
    39    40    46    0,0        0,0    0           0x00000001
      formats: AB24 AR24 RA24 BA24 BG24 RG24 RA15 BA15 RA12 BA12 RG16 BG16
      props:
        8 type:
            flags: immutable enum
            enums: Overlay=0 Primary=1 Cursor=2
            value: 1
        17 FB_ID:
            flags: object
            value: 46
        18 IN_FENCE_FD:
            flags: signed range
            values: -1 2147483647
            value: -1
        20 CRTC_ID:
            flags: object
            value: 40
        13 CRTC_X:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        14 CRTC_Y:
            flags: signed range
            values: -2147483648 2147483647
            value: 0
        15 CRTC_W:
            flags: range
            values: 0 2147483647
            value: 1920
        16 CRTC_H:
            flags: range
            values: 0 2147483647
            value: 1080
        9 SRC_X:
            flags: range
            values: 0 4294967295
            value: 0
        10 SRC_Y:
            flags: range
            values: 0 4294967295
            value: 0
        11 SRC_W:
            flags: range
            values: 0 4294967295
            value: 125829120
        12 SRC_H:
            flags: range
            values: 0 4294967295
            value: 70778880
        31 alpha:
            flags: range
            values: 0 255
            value: 0
        32 g_alpha_en:
            flags: range
            values: 0 1
            value: 1
    
    Frame buffers:
    id    size    pitch

     

    The Camera output finally shows up on the monitor.