Dev Tools
  • Products
  • More
Dev Tools
Forum Antenna range extension with amplifier?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 652 views
  • Users 0 members are here
  • dc-dc
  • controller
  • amplifier
  • knode
  • Design
  • antenna
Related

Antenna range extension with amplifier?

Latch
Latch over 14 years ago
I have an antenna that can deliver 1Mbps at 30 kilometers. Can the range be extended through the use of an amplifier?
 
Latch
  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    If the situation is such that longer range only means lower received signal to noise ratio, then the answer is generally yes but there are many variables undefined.  For example the range may be limited by frame length and turn around time.  If your radio is already waiting for a reply after sending a packet, data rate is limited by timing not signal level.  The amplifier needs to sense transmit / receive state without reducing packet rate.  If full duplex the amplifier must not introduce noise into the receiver. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • YT2095
    0 YT2095 over 14 years ago

    as a general rule, you will gain only a single `S` point for each doubling of power, so for instance you`re pushing 1W out, you`ll only get 3db gain (3`s` points) for pushing 4W, perhaps you may be better with a directional beam like a Yagi or Cantenna (depending on the frequency you`re thinking of of course).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 14 years ago in reply to YT2095

    The antenna gain solution is much better because you dont need to switch the amplifier from transmit to receive.  Being passive, antenna gain is more  like actually reducing the range.  If the link is line of sight (sometimes called R-squared propagation) you should get a doubling of range for each 6dB antenna gain you put  in there. 

     

    73 DE AA1LL  

    Mason, NH

    USA