Dev Tools
  • Products
  • More
Dev Tools
Forum Antenna range extension with amplifier?
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 654 views
  • Users 0 members are here
  • dc-dc
  • controller
  • amplifier
  • knode
  • Design
  • antenna
Related

Antenna range extension with amplifier?

Latch
Latch over 14 years ago
I have an antenna that can deliver 1Mbps at 30 kilometers. Can the range be extended through the use of an amplifier?
 
Latch
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    If the situation is such that longer range only means lower received signal to noise ratio, then the answer is generally yes but there are many variables undefined.  For example the range may be limited by frame length and turn around time.  If your radio is already waiting for a reply after sending a packet, data rate is limited by timing not signal level.  The amplifier needs to sense transmit / receive state without reducing packet rate.  If full duplex the amplifier must not introduce noise into the receiver. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 14 years ago

    If the situation is such that longer range only means lower received signal to noise ratio, then the answer is generally yes but there are many variables undefined.  For example the range may be limited by frame length and turn around time.  If your radio is already waiting for a reply after sending a packet, data rate is limited by timing not signal level.  The amplifier needs to sense transmit / receive state without reducing packet rate.  If full duplex the amplifier must not introduce noise into the receiver.