Dev Tools
  • Products
  • More
Dev Tools
Forum Op-Amp virtual ground questions
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 81 subscribers
  • Views 761 views
  • Users 0 members are here
  • dc-dc
  • controller
  • knode
  • Design
  • dev_kit
  • op_amp
Related

Op-Amp virtual ground questions

Latch
Latch over 14 years ago
I have 6 op-amp active filter connected to four LM3886 amplifier ICs.
 
I am using a LM324 op-amp set up as a voltage follower (VCC/2 divider connected to the input.) When I connected this to the virtual ground of the op-amp series, the op-amp output (virtual ground) oscillated at 2MHz. I added a resistor+capacitor to the output of the follower, low pass filter, suppressing the oscillations.
 
Can I adjust the low pass filters capacitor for better regulation of the virtual ground, or will it overload the op-amp’s capacitive load? Or is it ok if the output is not swinging?
Is there another way to regulate/filter the virtual ground?
Also, will connecting some caps between the virtual ground and the VCC rail help any?
 
Latch
  • Sign in to reply
  • Cancel
  • RWM
    0 RWM over 14 years ago

    If you would send circuit diagram, it will be easier to help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Latch
    0 Latch over 14 years ago in reply to RWM

    image

     

    R1 = 2.7K

    R2 = 2.7K

    Vout = virtual ground

    Vin(max) = 4V if this is exceeded, the virtual ground ceases to be correct.

     

    Can I adjust C1 to regulate the virtual ground better?

     

    Latch

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to Latch

    Do you have bypass capacitor on Vcc/2  resistor divider? What is supply voltage?