Dev Tools
  • Products
  • More
Dev Tools
Forum Basic circuit with relay
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 2138 views
  • Users 0 members are here
  • circuit
  • with
  • relay
Related

Basic circuit with relay

e14 Contributor
e14 Contributor over 12 years ago

Hi.

First of all: I hope this is the place to post.

 

I am gonna make an easy circuit with a relay to control a pump.(see attachment)

I understand the principal, but I wonder if there is anything more I gotto think of, like resistors or something?

 

It is not to be used in a car.

 

I am thinking of using an car relay: 12V, Max 30 amp.

The pump use 12V and 4 amp.

The fuse need to be 4 amp?

 

Can the switch for example be wired directly to pluss and minus on the car battery or do I need a  resistor there?

Thanks!

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • dougw
    0 dougw over 12 years ago

    The circuit is good the way it is.

    The fuse could be a little higher current - 5 to 10 amps, as long as the wiring and connectors can survive whatever current the fuse allows.

    The switch/relay power could be connected at the output of the fuse to protect the relay and switch as well.

    You could use (large) snubber diodes across the relay coil and pump to minimize arcing on the switch and relay contacts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Thanks for your respond! image

     

    The switch will not be directly connected to the battery, but from another more convenient location (which allready have a fuse box).

    Could you explain this sentence:
    "You could use (large) snubber diodes across the relay coil and pump to minimize arcing on the switch and relay contacts."

    1. What is "snubber diodes"?

    2. What is "arcing"?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dougw

    Thanks for your respond! image

     

    The switch will not be directly connected to the battery, but from another more convenient location (which allready have a fuse box).

    Could you explain this sentence:
    "You could use (large) snubber diodes across the relay coil and pump to minimize arcing on the switch and relay contacts."

    1. What is "snubber diodes"?

    2. What is "arcing"?