Dev Tools
  • Products
  • More
Dev Tools
Forum Basic circuit with relay
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 2138 views
  • Users 0 members are here
  • circuit
  • with
  • relay
Related

Basic circuit with relay

e14 Contributor
e14 Contributor over 12 years ago

Hi.

First of all: I hope this is the place to post.

 

I am gonna make an easy circuit with a relay to control a pump.(see attachment)

I understand the principal, but I wonder if there is anything more I gotto think of, like resistors or something?

 

It is not to be used in a car.

 

I am thinking of using an car relay: 12V, Max 30 amp.

The pump use 12V and 4 amp.

The fuse need to be 4 amp?

 

Can the switch for example be wired directly to pluss and minus on the car battery or do I need a  resistor there?

Thanks!

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    Actually, if your relay capacity is marginal, welded contacts, which implies device destruction, is on the table.  In some instances, such as very large solenoid-operated valves, or stepper motors with mechanically reactive loads, we actually have to explore the dynamics of the anti-spike apparat.

     

    In your case, as in most, an anti-parallel diode across the load, rated for the operating current, is all you need or need to think about.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    Actually, if your relay capacity is marginal, welded contacts, which implies device destruction, is on the table.  In some instances, such as very large solenoid-operated valves, or stepper motors with mechanically reactive loads, we actually have to explore the dynamics of the anti-spike apparat.

     

    In your case, as in most, an anti-parallel diode across the load, rated for the operating current, is all you need or need to think about.