Dev Tools
  • Products
  • More
Dev Tools
Forum Basic circuit with relay
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 15 replies
  • Answers 1 answer
  • Subscribers 81 subscribers
  • Views 2146 views
  • Users 0 members are here
  • circuit
  • with
  • relay
Related

Basic circuit with relay

e14 Contributor
e14 Contributor over 12 years ago

Hi.

First of all: I hope this is the place to post.

 

I am gonna make an easy circuit with a relay to control a pump.(see attachment)

I understand the principal, but I wonder if there is anything more I gotto think of, like resistors or something?

 

It is not to be used in a car.

 

I am thinking of using an car relay: 12V, Max 30 amp.

The pump use 12V and 4 amp.

The fuse need to be 4 amp?

 

Can the switch for example be wired directly to pluss and minus on the car battery or do I need a  resistor there?

Thanks!

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    0 D_Hersey over 12 years ago

    1n4002 is a PS diode, its okay but not really manufactured for this application.  Early ones were quite slow, now they are average.  The 1n914  is gold-doped for minority carrier lifetime suppression and is much faster.  Because you are using a relay, you will be fine with it, only better than nothing protecting a transistor.  Say, why are you using a relay rather than a transistor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • D_Hersey
    0 D_Hersey over 12 years ago

    1n4002 is a PS diode, its okay but not really manufactured for this application.  Early ones were quite slow, now they are average.  The 1n914  is gold-doped for minority carrier lifetime suppression and is much faster.  Because you are using a relay, you will be fine with it, only better than nothing protecting a transistor.  Say, why are you using a relay rather than a transistor?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • dougw
    0 dougw over 12 years ago in reply to D_Hersey

    Good point Don, picking the best diode depends on the specific circuit and objectives. Even the choice of using a flyback diode may not be the ideal way to control flyback pulses in some applications since using a flyback diode can delay the relay turn off until the coil has discharged.

    The specific relay may also impact diode choice - for example some 12V relay coils have an impedance of 28 ohms. This would result in a coil current of over .4 amps. Since the current through the coil cannot change instantly, the flyback diode would see the same current, which is above the rated current for a 1N914 - so its life would be shortened if it were used with this relay.

    Conversely the 1N4000 series diodes can take higher current, but may allow a short spike up to 500 ns as they turn on.

    You can of course get high speed, high current diodes - if the application justifies the price.

     

    For those who haven't seen these flyback voltages, here is a video...

    (Note he calls it back EMF which is not an accurate term for flyback voltage or inductive spike)

    https://www.youtube.com/watch?v=43HFng0CVKg