Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Blog [FRDM-KL46Z + KDS + PE] Tutorial: UART communication with a console on the host through OpenSDA
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bheemarao
  • Date Created: 22 May 2015 11:16 AM Date Created
  • Views 2357 views
  • Likes 1 like
  • Comments 2 comments
  • kds
  • uart
  • kl46z
Related
Recommended

[FRDM-KL46Z + KDS + PE] Tutorial: UART communication with a console on the host through OpenSDA

bheemarao
bheemarao
22 May 2015

This project demonstrates UART through OpenSDA (character is printed back on console through the CDC port of the board) with the FRDM-KL46Z Board and Kinetis Design Studio.

 

I have created a demo project which communicates with a console on the host.

Before we start this project below are the pre-requisites:


  • KDS 2.0.0 software tool from Freescale

         (http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KDS_IDE)

  • FRDM-KL46Z Freedom development board

 

I have created a project by name “kl46-async uart” as shown below:

 

image

 

I am adding the component “AsynchroSerial” to our project which is the low-level driver used for this in Processor Expert is the ‘AsynchroSerial‘ component as shown

 

image

 

 

 

And i am adding the component “ Shell” as the Shell component offers a SendStr() method and other useful functionality.

  So add the Shell component for the project, and use the AsynchroSerial with the ‘Serial’ template.

 

image

 

The AsynchroSerial settings are been done as shown below:

The interrupt is enabled as shown below:


image

 

As the CDC port of KL46 is connected to UART0 port i.e

 

RX port is connected to PTA1 :UART0_RX

TX port is connected to PTA2 :UART0_TX

 

And the baud rate is set to standard 9600


image

 

Next select CLS1 shell and make the settings as shown below:

The default serial is connected to AsynchroSerial component AS1


image

 

Generate the processor expert code by clicking the button shown below:


image

image

 

 

Now its time to add our code:

We are just reading the character from console through RX pin of UART port and same character is printing back to the console from TX pin of UART port.

 

 

I have declared a variable ch[10] as a char and storing the typed character from console into it.

  Now build the project either by clicking on the small hammer button

image

or as shown below


image

 

You can see the compilation building the project


image

 

You can run this project either by going to Debug configuration and run by single step or by going to project properties > C/C++ Build > settings > Toolchains at the time of building the project opt for “create flash image”  click apply and ok

 

image

 

Next select Tool settings and select Motorola S-record to generate SREC format as shown below:


image

 

Click on ‘Apply’ and ‘ok’

Now build the project, after successfully build you can find the “kl46-async uart.srec” file inside the Debug folder as shown


image

 

You can check it at below location

 

image

 

To run your program plug on KL46 board to your computer and open the corresponding COM port (com port number can be noted from device manager after plugging the board) and settings as shown below.

 

image

 

Now just drag and drop the srec file to the KL46 folder detected

 

image

 

You can see the output as shown below: type a character it is printed back on console through the CDC port of the board.

 

image

 

I have enclosed the project folder and SREC file for quick reference and testing.

 

Happy Async uart testing image image

Attachments:
kl46-async uart.rar
kl46-async uart.srec.zip
  • Sign in to reply

Top Comments

  • clem57
    clem57 over 11 years ago +1
    Nice demo/tutorial. Keep up the informative work you do here. Clem
  • balearicdynamics
    balearicdynamics over 11 years ago

    Another good idea with full documentation to bookmark image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 11 years ago

    Nice demo/tutorial. Keep up the informative work you do here.

    Clem