• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Forum Freescale Processor Expert (Driver and RTOS tool for the Kinetis Freedom Boards) [video]
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 7 subscribers
  • Views 1458 views
  • Users 0 members are here
  • frdm-kl05
  • freescale
  • drivers
  • codewarrior
  • frdm-kl25z
  • kinetis-l
  • frdm-kl46z
  • processor-expert
Related

Freescale Processor Expert (Driver and RTOS tool for the Kinetis Freedom Boards) [video]

FreescaleTools_and_Software
FreescaleTools_and_Software over 14 years ago

Processor Expert is a very versatile GUI tool created by Freescale that lets you focus on what will make your next embedded design truly unique. Instead of having to re-invent the wheel by writing yet another peripheral driver, it generates customized C code for Kinetis MCU start-up initialization and peripheral drivers. It's not a compiler or linker, but instead generates the code that can then be pulled into your preferred build environment. It also eliminates the need for one-size-fits-all drivers, allowing you to customize peripheral drivers ideally suited to your project, and all without the need for extensive knowledge of the hardware modules and their registers.  It also flags any silicon conflicts as you configure your particular project (making peripheral module muxing easy), and makes migration to a new device straightforward since it encapsulates all the MCU information required.


Processor Expert can also provide the drivers for RTOSs such as MQX and MQX-Lite, allowing you to customize a BSP for your hardware. MQX-Lite is the very low-footprint subset of MQX (both are free) that lets you run an RTOS on the Kinetis L family. And PE also provides integration with the complimentary Freescale USB stack, letting you get connected quickly with USB projects.


Processor Expert supports the many types of processors found on the Freescale Freedom boards (Kinetis K and Kinetis L families, among others), so that no matter what your target MCU is, Processor Expert has you covered.


Processor Expert is available in two ways, though both provide the same rich features and functionality:

1) A stand-alone version which is named "Processor Expert Driver Suite" (and which can also be optionally installed as a plugin for Eclipse 3.7 for Linux)

2) Integrated into the Freescale CodeWarrior IDE


The stand-alone version can create the C source which can then pulled into many of the most popular ARM IDEs:

  • CodeWarrior ARM C Compiler 5.1 and higher (CodeWarrior for MCU, 10.1 and higher).
  • IAR ARM C Compiler 6.3 and higher
  • GNU C Compiler for ARM architecture
  • Keil C/C++ ARM Compiler 5.4 and higher

 

This post is divided into two types of video "tutorials" based on if you're using the stand-alone Processor Expert Driver Suite, or Processor Expert Embedded in CodeWarrior.

 

 

PROCESSOR EXPERT DRIVER SUITE

 

The stand-alone Processor Expert Microcontroller Driver Suite v10.2 can be downloaded for FREE, without limitations, from here :

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=PE_DRIVER_SUITE&tid=PEH


 

 

Processor Expert - Introduction (Driver Suite)

 

This video is unavailable.
You don't have permission to edit metadata of this video.


 

Processor Expert: Exporting and Importing Templates (Driver Suite)


This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert - Working with Components (Driver Suite)


This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: Creating an MQX Lite Project (Driver Suite)


This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: An MQX Lite Example (Driver Suite)

 

This video is unavailable.
You don't have permission to edit metadata of this video.


 

 

Processor Expert: Integrating with IAR Embedded

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: Integrating with Keil Microvision

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: The Code Model (Driver Suite)

 

This video is unavailable.
You don't have permission to edit metadata of this video.


 

PROCESSOR EXPERT EMBEDDED INTO CODEWARRIOR

 

CodeWarrior 10.5 includes Processor Expert built into the IDE. It can be downloaded for FREE at this link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-MCU10&tid=CWH


Note that there are several different versions to choose from (from the free Special Edition to a free 30-day evaluation version of the Professional edition) but all versions include Processor Expert.

 

Processor Expert - Introduction (CodeWarrior)

 

This video is unavailable.
You don't have permission to edit metadata of this video.


 

Processor Expert - Exporting and Importing Templates (CodeWarrior)


This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert - Working with Components (CodeWarrior)

 

This video is unavailable.
You don't have permission to edit metadata of this video.


 

 

Processor Expert: Creating an MQX Lite Project (CodeWarrior)


This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: An MQX Lite Example (CodeWarrior)

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 


 

Processor Expert: The Code Model (CodeWarrior)

 

This video is unavailable.
You don't have permission to edit metadata of this video.

 


  • Sign in to reply
  • Cancel
  • gordonmx
    gordonmx over 14 years ago

    Where are the download links?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 14 years ago in reply to gordonmx

    Sorry for the delay, Processor Expert Microcontroller Driver Suite 10.0 and Codewarrior 10.3beta were just uploaded today on Freescale website

    Link have been added to my initial post

     

    www.freescale.com/FRDM-KL25Z is now active with many additional documentation and code example, enjoy image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gordonmx
    gordonmx over 14 years ago in reply to FreescaleTools_and_Software

    The CodeWarrior v10.3 beta link is available on the Freescale site, but I'm having trouble download the file at work.  I'll try it from home later.