• Products and Partners
    Products and Partners
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
Freedom development platform
  • Products and Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Documents Tutorial for FRDM-KL25Z: Completing the Freescale Freedom Board
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: FreescaleTools_and_Software
  • Date Created: 8 Nov 2012 1:25 PM Date Created
  • Last Updated Last Updated: 27 Oct 2013 5:48 AM
  • Views 876 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Tutorial for FRDM-KL25Z: Completing the Freescale Freedom Board

This tutorial was extracted from Erich Styger blog http://mcuoneclipse.wordpress.com with his agreement.

 

imageimage

 

 

I had pre-ordered some FRDM-KL25Z boards, and they came with the extra headers in plastic bags:

 

image

Pre-ordered Freedom board with headers

 

 

 

 

I have received as well a batch of the production boards, and for these I need to order the missing parts. So for everyone else, here are the Farnell part numbers:

 


Here is a table of all the parts which are on the pre-production ‘white’ board, but not populated on the ‘black’ production board, with reference to the board schematics:

 

 

SchematicsFarnell Part##DescriptionComment
J1016683511SAMTEC – SSW-106-01-G-DSSW-106-01-G-D‘Arduino’ header 2×6, 2.54 mm
J1, J916683642SAMTEC – SSW-108-02-G-D‘Arduino’ header 2×8, 2.54 mm
J216683731SAMTEC – SSW-110-01-G-DSSW-110-01-G-D‘Arduino’ header 2×10, 2.54 mm
J3, J4, J1117049103MOLEX – 22-28-402222-28-4022 – BOARD-BOARD CONNECTOR HEADER, 2WAY, 1ROWJumper header, 2.54 mm
J6, J816677282SAMTEC – FTS-105-01-L-DDebug Connector 2×5 1.27 mm, (FYI, mating cable is 1667659)
U521366701ATMEL – AT45DB161E-SHD-B – DATAFLASH, 16MBIT, SPI, 8WSOICSerial flash (connected to OpenSDA K20, *not* to the KL25Z!)
BT19086541KEYSTONE – 3003 – BATTERYHOLDER 20mmBattery holder for CR2032 battery
(BT1)18234791CR 2032 Coin Li Battery, 3VCR2032 battery

 


I assume that things like the jumper headers are readily available, and are only required if I cut the trace between the jumpers on the board.

One or two debug connectors are only needed if I want to bypass OpenSDA, or to recover a CPU directly with a P&E Universal Multilink.

The Serial Flash chip is only connected to the K20 OpenSDA device, and currently not used.

 

 

 

 

:!:  Note: On some(!!!!) of the black production boards, R25 (near the 8 MHz crystal) is not populated, while it is on the white boards. Having the 1 MOhm resistor requires the PEE (USB) clock to run in ‘high gain’ main, while without R25 it has to run in ‘low power’ mode. See Tutorial: USB CDC with the KL25Z Freedom Board.

 

 

 

 

Happy upgrading :-)

  • header
  • connector
  • freescale
  • frdm-kl25z
  • arduino
  • freedom