Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#01 - Blinking LED
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 22 replies
  • Subscribers 28 subscribers
  • Views 4868 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#01 - Blinking LED

cy.gul
cy.gul over 13 years ago

To kick-start our 100 Projects in 100 Days community effort around the PSoC 4 Pioneer Kit, today I'm posting a simple "Blinking LED" project.

 

This is a very simple project that will help you get started with your first design for the PSoC 4 Pioneer Kit.

 

Project Schematic:


                    Actual screenshot from PSoC Creator schematic (TopDesign.cysch)image

 

 

In this design, a PWM Component drives the Pin Component which is connected to the Blue LED on the Pioneer Kit. The PWM modulates to make the blue LED blink at regular intervals

 

Hardware connections on the Kit:

  • Blue LED - P0[3] (this is internally wired, no extra connections required)

 

Software Setup:

  • See steps #1 - #6 from the main post here

 

Project Files:

  • Blinking LED.cywrk.Archive01.zip

     

Attachments:
Blinking LED.cywrk.Archive01.zip
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to shabaz +2
    The IDE installed fine, and I was able to compile a demo program. Just in case anyone tries it with Windows 7 64-bit: For me, when I tried to compile, it said a license had expired (although I've not installed…
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +1
    I see! It sounds straightforward and not so scary any more :-)
Parents
  • shabaz
    shabaz over 13 years ago

    Hi,

    The 'Software Setup' steps 1-6 link is broken. I looked at the zip file, but the main.c just contains essentially this:

    #include <device.h>

    void main()

    {

        Clock_Start();

        PWM_Start();


        for(;;)

        {


        }

    }

     

    Where would you have  defined what connects to the count, start and clock pins on your schematic that you've shown? (I don't have a PSoC board, I'm just curious). The other files in the zip didn't seem text-readable, but I may have missed it, or is it done on the IDE somewhere?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cy.gul
    cy.gul over 13 years ago in reply to shabaz

    Hi Shabaz,

    Good question!

     

    The main.c contains only the 2 lines needed to 'start' the 2 Components - PWM and Clock, that are placed, wired, and configured on the project schematic ("TopDesign.cysch").

    That's all the CPU needs to do! The rest of the design runs entirely in hardware with no CPU intervention required.

    To see how the 2 Components are setup, simply double-click them to open the Component configuration window.

     

    You can setup your global chip resources like Clocks, Pins-outs, Interrupts, DMA,etc. in their respective tabs. Here is a quick tutorial video that shows the workflow with the Pin Component as an example. http://video.cypress.com/video-library/video/PSoC-Software_PSoC-Creator/PSoC-Creator-Tutorial-Working-with-Pins/1768525420001

     

    To get started, you will need to install the free IDE - PSoC Creator.

     

    EDIT - thanks for noting the broken link, fixed now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cy.gul
    cy.gul over 13 years ago in reply to shabaz

    Hi Shabaz,

    Good question!

     

    The main.c contains only the 2 lines needed to 'start' the 2 Components - PWM and Clock, that are placed, wired, and configured on the project schematic ("TopDesign.cysch").

    That's all the CPU needs to do! The rest of the design runs entirely in hardware with no CPU intervention required.

    To see how the 2 Components are setup, simply double-click them to open the Component configuration window.

     

    You can setup your global chip resources like Clocks, Pins-outs, Interrupts, DMA,etc. in their respective tabs. Here is a quick tutorial video that shows the workflow with the Pin Component as an example. http://video.cypress.com/video-library/video/PSoC-Software_PSoC-Creator/PSoC-Creator-Tutorial-Working-with-Pins/1768525420001

     

    To get started, you will need to install the free IDE - PSoC Creator.

     

    EDIT - thanks for noting the broken link, fixed now!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • shabaz
    shabaz over 13 years ago in reply to cy.gul

    Hi Gagan, Thanks for the information! It sounds great. I'll try out the free IDE to experiment, downloading it now.