Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum 100 Projects in 100 Days
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 67 replies
  • Subscribers 41 subscribers
  • Views 55545 views
  • Users 0 members are here
  • pioneer
  • psoc4
  • capsense
  • psoc_creator
  • cypress
  • psoc
Related

100 Projects in 100 Days

vandana
vandana over 13 years ago

Cypress and element14 are excited to start a new community initiative around the PSoC 4 Pioneer Kit - 100 Projects in 100 Days.

image

 

Over the next several weeks, we will post a new PSoC Creator project everyday, designed specifically for the PSoC 4 Pioneer KitPSoC 4 Pioneer Kit (CY8CKIT-042).

These projects will be posted daily (Monday though Friday) to the element14 community along with simple instructions on how to use them, what expansion boards are needed, and a few notes on the project design itself.

For the community, these projects are as simple as program-and-play, and will turn into an extensive library of PSoC 4 Pioneer Kit design examples that work with many 3rd party exapansion boards including Arduino shields and Digilent Pmod daughter cards - allowing you to create the design you need, and interface with the hardware you want.

 

For a list of all projects released click here

 

To get started with these PSoC 4 Pioneer Kit community example projects -

 

Step 1     Buy the $25 PSoC 4 Pioneer Kit PSoC 4 Pioneer Kit 

 

Step 2     Download the latest version of PSoC Creator and the required kit software files from www.cypress.com/cy8ckit-042 

 

    • Existing PSoC Creator users - download only the Kit-042 files (you can update to PSoC Creator 2.2 SP1 using the built-in Cypress Update Manager)
        • CY8CKIT-042 Kit Only (~17MB)

 

    • New PSoC Creator users - download the full PSoC Creator + Kit-042 files
      • CY8CKIT-042 Kit Setup (~631MB) (available on the web archive at https://web.archive.org/web/20211205143146/https://download.cypress.com/downloadmanager/software/CY8CKIT042Setup_1.exe)

         

image

Step 3  A. Download the community projects posted here (each project is an individual .zip file)    

             B. Extract the contents of project .zip file to your computer

 


image

 

Projects Released

 

S No Date Project Title
1 01-May-2013 Simple Blinking LED
2 02-May-2013 CapSense Slider Example
3 03-May-2013 PSoC 4 Pioneer Kit Annotation Library
4 06-May-2013 USB-UART utility
5 07-May-2013 USB-I2C Utility
6 08-May-2013 Danger Shield with Light Sensor Control
7 09-May-2013 Danger Shield with 7-segment display
8 10-May-2013 Danger Shield Buzzer of Doom
9 13-May-2013 Graphics LCD Display
10 14-May-2013 LCD - Rotating Cube Demo
11 15-May-2013 GLCD Paddle Game
12 16-May-2013 Pioneer Board Oscilloscope
13 17-May-2013 CapSense Button & LED Control with Bridge Control Panel
14 20-May-2013 What was the value? - LED Memory Example
15 21-May-2013 CapSense Proximity Detection
16 22-May-2013 Proximity Theremin
17 23-May-2013 2-Channel OScope with GraphicsLCD
18 24-May-2013 'Catch the Shells' Game with ColorLCD Shield
19 28-May-2013 LED Memory! Part Deux. Just Deux it!
20 29-May-2013 Starter Designs
21 30-May-2013 Fractional Frequency Synthesizer
22 31-May-2013 “Kill The Ghost” Game
23 03-Jun-2013 tinyprintf Example
24 04-Jun-2013 XBee Router Loopback Example
25 05-Jun-2013 XBee Direct IO
26 06-Jun-2013 XBee API RxTx Example
27 07-Jun-2013 XBee RGB CapSense Control
28 10-Jun-2013 “WiFi? Why Not!” Arduino WiFi Shield Example
29 11-Jun-2013 Bluetooth Home Automation System
30 12-Jun-2013 Bluetooth with GLCD
31 13-Jun-2013 Ethernet Shield
32 14-Jun-2013 More Relay!
33 17-Jun-2013 Sweet Music Everywhere! MIDI Shield
34 18-Jun-2013 Resistive Touch Example
35 19-Jun-2013 UART, I2C, and SPI Joystick Example
36 20-Jun-2013 What? I can use the PSoC 5LP too?
37 21-Jun-2013 PSoC With Friends! Word Scramble Game
38 24-Jun-2013 Ultrasonic Distance Measurement
39 25-Jun-2013 Two PWMs for the price of one
40 26-Jun-2013 Pioneer PnP Sensors
41 27-Jun-2013 Thermistor Example
42 28-Jun-2013 Hangman Game
43 01-Jul-2013 Rise of the Machines (Rolling Robot)
44 02-Jul-2013 Run Away Run Away! (Proximity Robot)
45 03-Jul-2013 Stepper Motor Example
46 05-Jul-2013 “Paint The Night” Accelerometer Example
47 08-Jul-2013 Obstacle Avoider Robot
48 09-Jul-2013 Walk The Line! Robot Example
49 11-Jul-2013 Android Device Controlled Robot
50 12-Jul-2013 SD Card Example

S No

Date Project Title
51 15-Jul-2013 Music Player
52 16-Jul-2013 Strike A Pose! Digital Camera
53 17-Jul-2013 PSoC Eye
54 18-Jul-2013 Custom Component 4x4 Keypad
55 19-Jul-2013 Parallel to Serial UDB Component
56 22-Jul-2013 Accelerometer Level
57 23-Jul-2013 Digital Audio From A Single Pin
58 24-Jul-2013 An Introduction to Processing
59 25-Jul-2013 But Wait There’s More! Single PWM with 3 Outputs
60 26-Jul-2013 PSoC 4 Mini-Billboard
61 29-Jul-2013 Nokia 5110 LCD Interface
62 30-Jul-2013 Ready…Set…GO! PSoC Stopwatch
63 31-Jul-2013 Some Like it Hot! PSoC Thermostat
64 01-Aug-2013 Workspace Organization using PSoC Theromostat
65 02-Aug-2013 New to PSoC or the Pioneer Kit? START HERE!
66 05-Aug-2013 LED Blinky Revisited
67 06-Aug-2013 PSoC 4 Getting Started Lab 1 (LED Blinky)
68 07-Aug-2013 PSoC 4 Getting Started Lab 2 (PWM LED)
69 08-Aug-2013 PSoC 4 Getting Started Lab 3 (CapSense UART)
70 09-Aug-2013 PSoC 4 Getting Started Lab 4 (ADC)
71 12-Aug-2013 Get Your Motor Runnin’!
72 13-Aug-2013 TFT Touchscreen Shield
73 14-Aug-2013 TFT Touchscreen Tic-Tac-Toe Game
74 15-Aug-2013 PSoC Creator Training 110
75 16-Aug-2013 PSoC Creator Training 111                                          
76 19-Aug-2013 PSoC Creator Training 112
77 20-Aug-2013 PSoC Creator Training 113
78 21-Aug-2013 PSoC Creator Training 210
79 22-Aug-2013 PSoC Creator Training 211
80 23-Aug-2013 PSoC Creator Training 212/213/214
81 26-Aug-2013 NFC/RFID Shield
82 27-Aug-2013 RFID Reader and Writer Project #2
83 28-Aug-2013 Raspberry Pi Integration
84 29-Aug-2013 State Machines in PSoC 4
85 30-Aug-2013 UART Bootloader in PSoC 4
86 03-Sep-2013 GPS Algorithm
87 04-Sep-2013 Gas Sensor Example
88 05-Sep-2013 Simulation of Gas Sensor Example
89 06-Sep-2013 GPS Example
90 09-Sep-2013 Comparator Example
91 10-Sep-2013 Infrared Remote Control
92 11-Sep-2013 Serial Communications Examples
93 12-Sep-2013 4 Channel Multiplexed Comparator
94 13-Sep-2013 Opamp Dynamic Gain
95 16-Sep-2013 Hibernate and Stop Power Modes
96 17-Sep-2013 P4 Light Sensor Project Design
97 18-Sep-2013 Rice Cooker
98 19-Sep-2013 Thermal Printer
99 20-Sep-2013 I2C Pass Though 'Smart Wire'
100 23-Sep-2013 PSoC 4 Time Square Billboard
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago +4
    Hi Vandana, Can we request some from Cypress if they've not thought up all 100 yet? :-) I can think of some ones that require a good mix of analog and digital and software, but I'm not experienced with…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +4
    It wasn't done out of spite for other operating systems or anything so diabolical : ) We want to go cross platform, We know its important, but we have man-decades (maybe even man-centuries) of effort in…
  • DAB
    DAB over 13 years ago in reply to e14 Contributor +4
    Hi Chris, No need to appologize for being windows only. When you build tools you look at your market potential While there may be 2-3 million loyal Linux/Unix users there are 300-500 300-500 million Windows…
  • shabaz
    shabaz over 13 years ago

    Hi Vandana,

     

    Can we request some from Cypress if they've not thought up all 100 yet? :-) I can think of some ones that require a good mix of analog and digital and software, but I'm not experienced with PSoC platform to know if these are feasible.

    For example:

    1.metal detector

    2. PC-controlled curve tracer with current source and with voltage source, for BJT and FET

    3. inductance meter with adjustable choice of freq

    4. Some charge measurement device (maybe somehow using capsense?)

    5. logging device to capture analog readings via serial port to the PC and ability to set gain via PC, and a current source (so we can optionally log temperature with an RTD).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • vandana
    vandana over 13 years ago in reply to shabaz

    Thanks, Shabaz. We definitely are looking for project ideas that would help enable application development!

     

    If you havent ordered a kit yet, I would recommend you to buy the PSoC 4 Pioneer KitPSoC 4 Pioneer Kit (these should be in stock by next week) and test these projects and contribute your own too

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to vandana

    Oh!; ) I'll try to experiment virtually, and maybe pick #1 from the list for now .

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    Hey Shabaz, its not specifically for the Pioneer kit (it uses PSoC 3 or PSoC 5LP) but # 3 has been addressed: http://www.cypress.com/?app=forum&id=2492&rID=76890

     

    Its a full on LCR meter with adjustable frequency.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 13 years ago

    I really like this approach.

    The easiest way to get people to use your product is to provide them with ideas and tested solutions so that they can see the power of your device.

     

    I will keep an eye on the posts.  Who knows, I might even be talked into buy one an playing with it.

     

    Great idea,

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago

    It looks like a very nice board.  Pity that those of us who run Linux can't play.

     

    It seems so bizarre to me that a company whose main product is semiconductor devices (not software) deliberately reduces its customer base by playing favorites on operating systems.  It's just sheer blinkeredness and incompetence to not write development software in a portable manner so that people can use their chips regardless of which operating system they happen to use.

     

    Vandana, if you're in contact with Cypress, you might like to pass this comment along to them.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    It wasn't done out of spite for other operating systems or anything so diabolical : )  We want to go cross platform, We know its important, but we have man-decades (maybe even man-centuries) of effort in our existing tools, built on a windows platform.  Is it perfect?  Of course not.  Its going to take a lot of work to redo the tools to make them cross platform like they should be.

     

    I guess I just want you to know, we do hear you, and we are working to address it.  Or at least, I hear you : )

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • fustini
    fustini over 13 years ago in reply to e14 Contributor

    Thanks, as a full-time Linux user, that's to good to hear.  I'll second Morgaine's comment that the board does look very interesting but I'm unlikely to try it out until it's compatible with Linux.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    Thanks Chris, it's good to know that someone is listening. image

     

    In case additional ammunition is needed to convince beancounters, it's worth pointing out that among the many millions of Linux desktop users, the proportion with technical backgrounds or interests is enormously higher than for Windows or Mac.  The Linux/Unix world grew largely through word of mouth within communities devoted to science, technology and higher education, and this has given it a very different demographic to operating systems with a user base in office and media consumption and/or general use.

     

    This bias towards technical pursuits greatly offsets Linux's lower numbers for official "market share" in desktop operating systems, and makes catering to the needs of this community very much in the interest of SoC and board suppliers.  It really is strategic.

     

    Morgaine.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 13 years ago in reply to morgaine

    While I agree that it's nice if tools support Linux as well as Windows I can't believe that its (currently) a show stopper for anyone seriously interested in PSOCs - it's not that expensive to buy a Windows license and dual boot if you only have one computer and there are so many occasions when you just have to use Windows to interact with third parties (customers, suppliers whatever) that running both OSes is just a fact of life.

     

    Having said that it looks to me as if Microsoft is becoming less and less interested in what I call "Technical computing"  - so much so that I guess by the time we reach Windows 10 by far the majority of technical tools will run first on Linux with Windows as the poor relation - so it's definitely time for Cypress and others in the same boat to start work on that mountain of legacy code image

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
>