Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#02 - CapSense Slider
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 28 subscribers
  • Views 5170 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#02 - CapSense Slider

cy.gul
cy.gul over 13 years ago

On the 2nd day of our 100 Projects in 100 Days community effort, I am posting one of the PSoC 4 Pioneer Kit's bundled example projects.

 

This is a very simple yet effective CapSenseRegistered demo that implements a 5-segment slider, like the one available on the Pioneer kit.

Moving your finger across the capacative touch slider on the board, you will observe the multicolor LEDs gradually changing color from red to green. These LEDs are driven by the PWM Component.

 

 

Project Schematic:

image

                            (Actual PSoC Creator project schematic "TopDesign.cysch")

 

image

    (CapSense Component Customizer - Implementing a Capacitive Touch Slider)



Hardware Connections (all internal to the board, no external connections required):

  • 5-segment Slider - P1[1] - P1[5]
  • Green LED - P0[2]
  • Red LED - P1[6]

 

Software Setup:

  • See steps #1 - #6 from the main post here
  • Main.C - This example project implement simple firmware in the project's main.c as shown below (already completed in the example project). The code implmented scans the CapSense slider, then updates the PWM's PulseWidth with the slider value.

image

                                      ( Project firmware - main.c )


Demo Video

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Project Files:

  • CapSense.cywrk.Archive01.zip

 

 


Attachments:
CapSense.cywrk.Archive01.zip
CapSense_Configuration.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    good~!
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi,

    Following the example,I write the code to build a CapSense project in PSOC Creat 2.2 SP1,but find there are some errors,such as undefined reference to "PWMWriteCompae";

    Could you tell me the possible cause of these errors and help me to solve it?

    Thank you very much.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Attach the .ZIP-file here and upload the project

    Attachments:
    p4-capsense-1.cywrk.Archive02.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Now I can build it succesfully.I need to write the right API function name,pay attention to the big or small letter.

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Good to hear, Gui.

    Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Thank you very much!

    Could you explain,in more detail,why the multicolor LEDs will gradually change color from red to green?

    After use PWM_WriteCompare() function to update the PWM pulse width with the new slider position,how does the waveform of the PWM's output(line&line_n changes)?

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cy.gul
    cy.gul over 13 years ago in reply to e14 Contributor

    Hi Gui Zhao,

    By using the PWM_WriteCompare() API, you are effectively re-configuring the PWM Component's properties during run-time.

    By writing a new compare value each time with the slider position, the duty cycle of the PWM changes, which in-turn modifies the LED outputs.

    In our project, the PWM Component has 2 outputs, "line" and "line_n" - which are nothing but the inverse of each other (the sum total of these 2 outputs is thereby 100% duty cycle).

    "line" is connected to the Red LED while "line_n" (inverse) is connected to the Green LED.

    As you adjust the duty cycle of one of PWM outputs by writing a new compare value, the other one inversely changes. Thus, you are going from 0-100% duty cycle on one LED, and the opposite on the 2nd LED. The result to the naked eye is a gradual change between the LED output between Red and Green colors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cy.gul
    cy.gul over 13 years ago in reply to e14 Contributor

    Hi Gui Zhao,

    By using the PWM_WriteCompare() API, you are effectively re-configuring the PWM Component's properties during run-time.

    By writing a new compare value each time with the slider position, the duty cycle of the PWM changes, which in-turn modifies the LED outputs.

    In our project, the PWM Component has 2 outputs, "line" and "line_n" - which are nothing but the inverse of each other (the sum total of these 2 outputs is thereby 100% duty cycle).

    "line" is connected to the Red LED while "line_n" (inverse) is connected to the Green LED.

    As you adjust the duty cycle of one of PWM outputs by writing a new compare value, the other one inversely changes. Thus, you are going from 0-100% duty cycle on one LED, and the opposite on the 2nd LED. The result to the naked eye is a gradual change between the LED output between Red and Green colors.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to cy.gul

    Hi Gagan,

    By using the PWM_WriteCompare() API,the compare value has changed, I think it should be less than period value(The period value don't change).

    But I found you didn't care about that in the program.It seems that compare value is large than period value.Would you tell me the reason?

    Thanks