Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#17 - 2-Channel OScope with GraphicsLCD
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 31 subscribers
  • Views 5557 views
  • Users 0 members are here
  • graphics
  • sar
  • lcd
  • 100projects
  • oscilloscope
  • adc
  • arduino
  • 4
  • psoc
Related

PSoC 4 Pioneer Kit Community Project#17 - 2-Channel OScope with GraphicsLCD

cy.gul
cy.gul over 13 years ago

Hello folks!

 

Today we're posting another Oscilloscope project that uses the Color Graphics LCD Shield. This project is a little dual channel scope using the PSoC 4 Pioneer board and the SparkFun Arduino color graphics shield or equivalent.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The user input is via SW2 on the Pioneer board (none of the switches on the display are used). Tap the button to cycle through the options highlighted with a white box drawn around it. Hold the button for a second or more until the box moves to another parameter.

 

*      Trigger Channel:  "TRG 1" or "TRG 2"

*      Trigger Level:    From 100mV to 5000mV

*      Input Range:      5000mV, 2500mV, 1250mV, 625mV, 312mV

*      Samples per Second:  SPS  10k, 20k, 50k, 100k, 200k, 400k

 

image

 

Components used:

* Graphics LCD Component (over SPI)

* SAR ADC Component

* a few instances of the Pin Component

 

Software:

Inside the PSoC Creator project, you'll notice 2 Sources Files -

* main.c - this implements the main firmware for the project's user interface

* scope.c - this implements all of the oscilloscope functions

 

Hardware Required:

* PSoC 4 Pioneer Kit

* Sparkfun or equivalent Nokia 6100 based Color Graphics LCD Arduino Shield

 

Attachments:

PSoC Creator Project .zip file

Attachments:
P4Scope2.zip
  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 13 years ago +1
    Another fun project. I am curious about the way the two signals walked through each other. Is that due to the sampling or due to them being generated by different generators/time base? Keep up the fun…
  • mhastings
    mhastings over 13 years ago in reply to DAB +1
    DAB, I purposely made the two waveforms at a slightly different frequency so I could tell if I could sync to one or the other. The project lets you select the channel and the voltage level that you trigger…
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to cy.gul +1
    Hello Gagan. I debug the psoc creator project and compiled zero errors. thanks. Jesus Antonio.
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hi,

    I need help with project #17.  I have the psoc 4 pioneer kit and an LCD shield (ElecFreaks V1.2).  I can't find a datasheet for this project describing the required pin connections.  I built the project and programmed the device but I don't see anything on the display after pressing the reset.

     

    Thanks,

    AB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to e14 Contributor

    Hello AB.

    i have been working with this lcd, please dont forget  drive P3[4] high. please look at:

    http://www.element14.com/community/message/76334#76334/l/psoc-4-pioneer-kit-community-project09-graphics-lcd-display project 3009.

     

    regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Jesus,

    Thank you for your help.  The voltage on P3.4 is about 3.11V.  I may have to try project#9 first.

     

    AB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Jesus,

    Again, thanks for your help.  The LCD shield is working now.

     

    AB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Jesus,

    Again, thanks for your help.  The LCD shield is working now.

     

    AB