Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#041 – Thermistor Example
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 31 subscribers
  • Views 3558 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#041 – Thermistor Example

cy.wbz
cy.wbz over 13 years ago

Hello!

 

In today’s example we are creating a simple thermistor project that reports data up to the Bridge Control Panel using the PSoC 5LP device as a USB-UART bridge.

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • UART
  • Thermistor
  • ADC SAR
  • AMux

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

The Thermistor example was built using a custom Breadboard shield developed by Cypress, you can use the sparkfun breadboard to build this example. In this example we use a GE measurement and control sensorGE measurement and control sensor.

 

The project firmware pulls the value from the Thermistor using the ADC SAR and reports that value over the UART. We will then use the Bridge Control Panel to display that value in a chart format. This will allow us to plot the temperature over time.

 

Please refer to example #015 that uses the Bridge Control Panel and the USB-UART functionality. This example will instruct the user on how to setup the Bridge Control Panel for this example. When you’ve set up your design please use the following Bridge Control Panel commands and settings:

 

rx8 [h = 55] @1Temp @0Temp [t = aa]

 

Hardware Connections:

 

Connect a breadboard kit to the Pioneer Kit, the suggestion is to use the Sparkfun breadboard kit. Take the Thermistor and connect it to the Pioneer Kit using the following schematic:

 


image

 

Test Your Project:

 

Program the kit and then launch the Bridge Control Panel to read out the Thermistor values. The user can pinch the Thermistor with their fingers to drive up temperature on the Thermistor.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
4048.Project Images.zip
PSoC4_Thermistor.cyprj.Archive03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to cy.gul +1
    Hello Matt. Thanks for this project. Gagan you have reason extremely cheap! project in cost . I am waiting for components to build and test this project in my house. best regards, Jesus Antonio.
  • greatunclebulgaria
    greatunclebulgaria over 13 years ago +1
    Hi Matt, Great series of examples, looking forward to the robots! Could you supply the pins used on the PSoC4 board for the 3 (plus Vss) pins? This way we could use any breadboard. I assume the 10k reference…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello Matt!

    First of all, I wish to thank you for the example and the materials that you provided.

    I am rather new to all of this.

    Second of all, I wish to extend your example in order to measure temperature not with one, but with three thermistors.

    Do you think that would be possible?

    I must mention that I have the same board a PSoC 4 Pioneer KIT and I tried and succeeded to follow your example.

    Thank you, in advance for the help:-)!


    Alex

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello Matt!

    First of all, I wish to thank you for the example and the materials that you provided.

    I am rather new to all of this.

    Second of all, I wish to extend your example in order to measure temperature not with one, but with three thermistors.

    Do you think that would be possible?

    I must mention that I have the same board a PSoC 4 Pioneer KIT and I tried and succeeded to follow your example.

    Thank you, in advance for the help:-)!


    Alex