Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#055 – Parallel to Serial UDB Component
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 29 subscribers
  • Views 2885 views
  • Users 0 members are here
  • 100projects
Related

PSoC 4 Pioneer Kit Community Project#055 – Parallel to Serial UDB Component

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example is the release of a community component for a parallel to serial UDB component. At the bottom of this post we have included the example project for the component and the custom component datasheet. The key point of this component is that it’s applicable to PSoC 3/4/5LP device families.

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

image

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Parallel to Serial

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

The parallel to serial component contains a set of datapaths that allow conversion of any parallel data, given to the component, to be transmitted in a serial data output. The required baud rate can be set using the clock input.

 

In this example we are outputing some parallel values to the serial port. Feel free to test out this example using and Oscope to verify the serial output content.

 

Hardware Connections:

 

There are no connections for this example. This is a custom component released to the community that enables some type of set functionality. Please refer to yesterday’s post for information on how to import or export your custom component.

 

Test Your Project:

 

Program the Pioneer kit with your example that utilizes the parallel to serial component and connect the kit to your custom hardware.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
image
Parallel to Serial v1_0.zip
3823.Project Images.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB +1
    This project uses one Datapath instance for implementing Parallel to Serial conversion. Every UDB block contains one Datapath instance. So, you can use 4 such instances of this component in a 42xx family…
  • DAB
    DAB over 13 years ago

    A very useful capability.

     

    How many instances does the Psoc 4 support?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago

    Hello Matt.

    thanks for design this very useful component.

     

     

    regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    This project uses one Datapath instance for implementing Parallel to Serial conversion. Every UDB block contains one Datapath instance. So, you can use 4 such instances of this component in a 42xx family of PSoC 4 which contains 4 UDB blocks. It is not possible to use this component in 41xx family as they don't have any UDBs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to e14 Contributor

    Hello Kishore Kumar S.

    Thanks for your explanation. i have to say too that  the UDB array also provides a switched Digital System Interconnect (DSI) fabric that allows signals from peripherals and ports to be routed to and through the UDBs for communication and control.

     

    image

    Regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • DAB
    DAB over 13 years ago in reply to e14 Contributor

    Hi Kishore,

     

    That's what I thought, but I wanted to make sure so that everyone could see how these programmable hardware blocks work.

     

    Thanks

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    Speaking of parallel to serial, today's project shows how to make sound-effects by using the same concept (used in PSoC Creator's SPI and Shift Register components).

     

    Oh - it may also be interesting to state that PSoC 4 also has 2 SCBs (serial communication blocks) that can do SPI. Effectively, these are additional 'Parallel to serial' blocks that 41xx as well as 42xx parts have.

     

    PSoC 4's UDBs (Universal Digital Blocks) are a pretty versatile Programmable Logic fabric, in that there are a number of small custom functions that you can perform with them.

    For instance, Matt is soon going to release a project that implements an RGB LED controller function (Component) implemented in a single UDB (single Datapath and 3 Macrocells, actually).

    So if you understand the UDB, you can get really creative and efficient with your designs.

     

    Matt, do we have a release date for the triple-compare PWM ?

     

    Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cy.wbz
    cy.wbz over 13 years ago in reply to e14 Contributor

    Antonio,

     

    The triple compare PWM will be posted Thursday. The serial audio will be posted today (likely in the next hour) image

     

    -Matt Buza