Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#056 – Accelerometer Level
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 26 subscribers
  • Views 1080 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#056 – Accelerometer Level

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example builds on our earlier accelerometer example. Here we are using a three axis accelerometer as a digital level. The level reads the X, Y, and Z acceleration to determine the orientation.

Hardware used:

  • CY8CKIT-042 Pioneer Kit
  • 3-Axis Accelerometer

 

image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • PWM
  • UART
  • I2C
  • CyClock
  • CyPin

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we are implementing a level using a three axis I2C accelerometer. The firmware reads X, Y, and Z acceleration, filters the values, and calculates orientation relative to horizontal and 45 degrees. The project then sets the color of the RGB LEDs based on how close the orientation is to ideal. The project also prints out a raw acceleration value to the UART which can be used to display on a hyperterminal software or the Bridge Control Panel.

 

In this example we use the interrupt output of the accelerometer to prompt communication. It also detects when the configuration of the sensor is lost, and reconfigures it. This can happen when the device is power cycled during operation.

 


image

 

Hardware Connections:

 

For this example plug the Sparkfun three axis accelerometer breakout board into the J3 header, pins 1-6. You may need to solder wires or a header to the accelerometer. In our example we connected the accelerometer to a six pin cable. This allowed us to move the accelerometer around while holding the pioneer kit in our other hand. Please be careful of the orientation of the ribbon cable, if you reverse the polarity on the accelerometer you may cause damage to the device.

 

Test Your Project:

 

Connect your hardware and program the kit. Take the accelerometer and set it on a flat surface. Notice the LED begin to change color and then glow a bright green when on a level surface.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
KIT042_Accelerometer_Level.cyprj.Archive01.zip
8551.Project Images.zip
  • Sign in to reply
  • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago

    Hello Matt.

    Another good project. Shows one of the many applications which use accelerometers. other applications can be:

     

    • eCompass applications

    • Static orientation detection (Portrait / Landscape, Up / Down, Left / Right, Back /

    Front position identification)

    • Notebook, eReader and Laptop Tumble and Freefall Detection

    • Real-time orientation detection (virtual reality and gaming 3D user position feedback)

    • Real-time activity analysis (pedometer step counting, freefall drop detection for HDD, dead-reckoning GPS backup)

    • Motion detection for portable product power saving (Auto-SLEEP and Auto-WAKE for cell phone, PDA, GPS, gaming)

    • Shock and vibration monitoring (mechatronic compensation, shipping and warranty usage logging)

    • User interface (menu scrolling by orientation change, tap detection for button replacement).

    Regards,

     

    Jesus Antonio.