Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#057 – Digital Audio From A Single Pin
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 28 subscribers
  • Views 2275 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#057 – Digital Audio From A Single Pin

cy.wbz
cy.wbz over 13 years ago

Hello!

 

In this example we will show you how to use a digital signal to generate analog sound effects using the PSoC 4 device. The example projects will encode a sound as a string of 1s and 0s which, when smoothed by an RC filter, creates an approximation of the original sound.

 

image

 

Please refer to the following web site that explains the concept and algorithm in detail. This example was adapted from this web page.

We have included an example of the 1-bit audio output at the bottom of this post.

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations
  • Audio Recording

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • SPI
  • CyClock
  • CyPin

 

The components are configured by right clicking on the component in your Top Design schematic view and selecting Configure. Please enable the following selections in the Configuration windows for the listed components above.

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

At a high level the following actions were taken with the example project:

  • Convert a sound effect .wav file to 1-bit sound format (encoding the data)
  • Convert the 1-bit format to an array of bytes (formatting the data)
  • Shift out the array to a pin connected to a speaker (playing the data)

 

Encoding the Data:

 

The sound effect .wav file was converted to 1-bit format byte array using the free BTc Sound Encoder 3.0 software developed by Roman Black.

 

image

 

There are some important features to this software:

  • Being able to resample the data at a different rate
  • Simulating what the 1-bit sound would sound like
  • Seeing how the 1-bit sound wave matches the actual sound wave
  • Exporting the 1-bit format data to a ‘PIC Mikro C file’.

 

image

 

Formatting the Data:

 

The generated code from the above application is not directly readable by the PSoC. It needs to be converted to an array of bytes to allow for the array to be initialized when declared. This step was done using a Python script (attached to this post).

 

image

 

Playing the Data:

 

Once the sound is ready to be initialized as an array in C, playing it out with the PSoC is simple. In the example we use the SPI component to output the values to the RC circuit. The array of data is shifted out MSB first using the SPIM Component.

  • Since the data was sampled at 11.025 kHz, the SPIM is clocked at 22.050 kHz to achieve a bit-rate of 11.025 kHz.
  • Playing around with the (external) passives did not have much of an effect on playback quality. Playback quality is primarily determined by the bit-rate and is a tradeoff with the flash footprint.
  • The flash footprint of the projectwith 5 sound effects (bark, bell, boing, quack, crowing) is ~9k.

 

Hardware Connections:

 

In this example the user will need to connect an external RC circuit to an external speaker. The SPIM component is then connected to Pin 0[4].

 


image

 

Test Your Project:

 

Program the Pioneer board and enjoy the sound effects.

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
Audio Example.m4a
Sounds.cydsn.zip
2625.Project Images.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Hey, A few things to note: 1. Thanks to Roman Black - the author of the BTc software. He has been around for a long time, and kudos to him for doing such a good job at this software: http://www.romanblack…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hey,

     

    A few things to note:

    1. Thanks to Roman Black - the author of the BTc software. He has been around for a long time, and kudos to him for doing such a good job at this software: http://www.romanblack.com/picsound.htm

    2. The first sound in the attachment is a robotic voice saying: "I sound like a 1980s movie computer"

    3. Don't let the SPI throw you off - it is being used as a shift register to shift out the sound. A 8-bit shifter register with a 3-bit counter (for shifting out 8 values) would have sufficed. The current implementation just was easier.

    4. To get better results, buffer the pin output using PSoC 4's opamp, before sending it to the speaker. You will notice that the resultant waveform at the speaker (seen on an oscilloscope) is much more like the screenshots above.

    5. The sound quality is in a large way determined by the bitrate and size of the audio samples.

     

    Listen to the audio file, try it out, and let me know what you think!

     

    With a little more effort, the sound quality can be made good enough for simple toys or such applications.

     

    Have fun!

    Antonio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago

    Hey,

     

    A few things to note:

    1. Thanks to Roman Black - the author of the BTc software. He has been around for a long time, and kudos to him for doing such a good job at this software: http://www.romanblack.com/picsound.htm

    2. The first sound in the attachment is a robotic voice saying: "I sound like a 1980s movie computer"

    3. Don't let the SPI throw you off - it is being used as a shift register to shift out the sound. A 8-bit shifter register with a 3-bit counter (for shifting out 8 values) would have sufficed. The current implementation just was easier.

    4. To get better results, buffer the pin output using PSoC 4's opamp, before sending it to the speaker. You will notice that the resultant waveform at the speaker (seen on an oscilloscope) is much more like the screenshots above.

    5. The sound quality is in a large way determined by the bitrate and size of the audio samples.

     

    Listen to the audio file, try it out, and let me know what you think!

     

    With a little more effort, the sound quality can be made good enough for simple toys or such applications.

     

    Have fun!

    Antonio

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • DAB
    DAB over 13 years ago in reply to e14 Contributor

    Hi Antonio,

     

    Thanks for the link and references.

    I agree, the idea is very simple.  You just control the charge on the capacitor using time spacing between the bits.

    I think you could improve both clarity and reduce artifacts if you used two or three shift registers in conjunction with an adjustable waveform mixing circuit.

     

    Definitately a neat idea for sound effects.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    Hey DAB,

    Thanks for the idea, and for the different way of thinking about the project.

    Such projects really help revisit fundamentals and understand every-day science in a slightly different way

    Best.

    Antonio

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hey,

    Well I download the project and got it working with the default sounds.  I tried running BTc.exe to create a different bit scream.  The problem is I am running window 7 and the download site is saying XP or maybe vista.  I cannot open a wav file. Has anyone tried to run this in Window 7 or even 8.1?  I tried several different wav files.  I get the following Msg:

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Ill try it out sometime soon and let you know, Brian