Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 32 subscribers
  • Views 4998 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example we are showcasing how to interface to the Nokia 5110 LCD screen with the PSoC 4 Pioneer Kit. This simple display provides a 84 x 48 Graphics LCD that was used in the Nokia 5110 model in 1998. This example provides a simple example to write text and an image on the LCD screen. This example uses a bit-banging method for sending the data & clock from the CPU to the LCD panel. The project does not require any UDB resources, therefore it can be used with the PSoC 4 (42xx and 41xx families).

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Annotated Component for Kit-042
  • CyPins

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we provide you with a couple of firmware based files named “Nokia5110LCD.c” and  “Nokia5110LCD.h”. These files are the source & header files required for using APIs. In this example we support the following APIs to control the Nokia 5110 LCD screen.

  • void LCD_Character(uint8)
  • void LCD_Clear(void)
  • void LCD_Init(void)
  • void LCD_String(char*)
  • void LCD_Write(uint8, uint8)
  • void Send_Data(int8)
  • void LCD_gotoXY(uint8, uint8)
  • void LCD_Bitmap(char*)

 

The main.c simply calls the APIs defined in the source file for initialization & for displaying the string on the LCD.

 

In this example, LCD initialization is done as specified in the datasheet of PCD8544 LCD driver which is used in the LCD panel. It is not necessary to use all 8 pins of PSoC 4 for interfacing this LCD. Reset, Chip Enable, Power, Backlight & Ground pins can be connected to fixed voltage levels on the board. Only Data/Command, Data & Clock pins are used for sending the data to LCD.

 

Hardware Connections:

 

In this example we are not using any specific headers or shields. Instead we are providing a firmware example to interface with the Nokia 5110 screen. We have connected the screen in the following connections:

 


image

 

Test Your Project:

 

Connect your screen and program the Pioneer kit. See the screen display the example text and images.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
5732.Project Images.zip
imagePCD8544 datasheet.pdf
Nokia5110 LCD Interface.cywrk.Archive03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • chr1sg75
    chr1sg75 over 6 years ago in reply to koudelad +1
    Hi David, Thanks for taking the time to reply. Glad to see the forum is still alive. I have dug out an old BitScope, so I am in the process of debugging the signal lines. For what it's worth, I can answer…
Parents
  • chr1sg75
    chr1sg75 over 6 years ago

    I know this is an old post, but hopefully someone is still listening :-)

    I have tried to get this to work on the Cypress PSoC 4 Bluetooth BLE module (CY8CKIT-143A) but am having no luck.

    Obviously, I have changed the device in the project to the correct one, but apart from that, should I worry about anything else?

    I used the following pins (and updated the project to reflect these changes)

    RST -> P3.7

    CE -> P3.5

    DC -> P3.3

    DIN -> P3.1

    CLK -> P5.1

    VCC -> P5.0

    GND -> P2.5

    (I didn't connect the BL pin because I don't need the backlight)

    Any suggestions why I'm getting nothing on screen?

    Cheers,

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • koudelad
    koudelad over 6 years ago in reply to chr1sg75

    Hello,

     

    I guess many of us won't have exactly the same HW setup, so I would recommend a few things:

    1) Double check wiring, both data and power: if you apply voltage to an LCD, it usually brightens or darkens - does this happen? (Did the LCD work in any other application?)

    2) Does your PSoC program really run? Do you have a debugger? Does the code execute or is stuck somewhere? If you don't have a debugger, can you create a demo to draw a pixel, light an LED (or toggle any other pin you have free) or similar to verify it is running?

    3) If someone has similar HW, it would help if you posted a buildable project archive from PSoC Creator.

     

    If you don't find help here, post your question to a Cypress Developer Community: https://community.cypress.com/welcome

     

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • chr1sg75
    chr1sg75 over 6 years ago in reply to koudelad

    Hi David,

    Thanks for taking the time to reply. Glad to see the forum is still alive.

    I have dug out an old BitScope, so I am in the process of debugging the signal lines.

    For what it's worth, I can answer some of your suggestions:

    - The backlight illuminates when the LCD is powered (although BL needs to be pulled low).

    - It's the first time I've used the LCD, so I haven't seen anything on the screen previously. I guess it could be dead.

    - The PSoC definitely runs

    - I will post my archive if I fail to diagnose with the 'scope

    And of course, if I figure out what is going wrong, I'll post an update.

    Cheers

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • chr1sg75
    chr1sg75 over 6 years ago in reply to chr1sg75

    Update:

    I have 'scoped the signal lines and things appear to behaving as I would expect.

    I did wonder why the CE line is not set high during initialisation, but I guess if it doesn't matter as long as the LCD is reset properly.

    I will upload the archive and perhaps someone can tell me what I might be doing wrong. Also, some photos to show the hardware setup.

    p.s. I added a Temp signal so that I could have a known line to trigger the 'scope.

     

    imageimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • chr1sg75
    chr1sg75 over 6 years ago in reply to chr1sg75

    Update:

    I have 'scoped the signal lines and things appear to behaving as I would expect.

    I did wonder why the CE line is not set high during initialisation, but I guess if it doesn't matter as long as the LCD is reset properly.

    I will upload the archive and perhaps someone can tell me what I might be doing wrong. Also, some photos to show the hardware setup.

    p.s. I added a Temp signal so that I could have a known line to trigger the 'scope.

     

    imageimage