Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 32 subscribers
  • Views 4998 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example we are showcasing how to interface to the Nokia 5110 LCD screen with the PSoC 4 Pioneer Kit. This simple display provides a 84 x 48 Graphics LCD that was used in the Nokia 5110 model in 1998. This example provides a simple example to write text and an image on the LCD screen. This example uses a bit-banging method for sending the data & clock from the CPU to the LCD panel. The project does not require any UDB resources, therefore it can be used with the PSoC 4 (42xx and 41xx families).

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Annotated Component for Kit-042
  • CyPins

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we provide you with a couple of firmware based files named “Nokia5110LCD.c” and  “Nokia5110LCD.h”. These files are the source & header files required for using APIs. In this example we support the following APIs to control the Nokia 5110 LCD screen.

  • void LCD_Character(uint8)
  • void LCD_Clear(void)
  • void LCD_Init(void)
  • void LCD_String(char*)
  • void LCD_Write(uint8, uint8)
  • void Send_Data(int8)
  • void LCD_gotoXY(uint8, uint8)
  • void LCD_Bitmap(char*)

 

The main.c simply calls the APIs defined in the source file for initialization & for displaying the string on the LCD.

 

In this example, LCD initialization is done as specified in the datasheet of PCD8544 LCD driver which is used in the LCD panel. It is not necessary to use all 8 pins of PSoC 4 for interfacing this LCD. Reset, Chip Enable, Power, Backlight & Ground pins can be connected to fixed voltage levels on the board. Only Data/Command, Data & Clock pins are used for sending the data to LCD.

 

Hardware Connections:

 

In this example we are not using any specific headers or shields. Instead we are providing a firmware example to interface with the Nokia 5110 screen. We have connected the screen in the following connections:

 


image

 

Test Your Project:

 

Connect your screen and program the Pioneer kit. See the screen display the example text and images.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
5732.Project Images.zip
imagePCD8544 datasheet.pdf
Nokia5110 LCD Interface.cywrk.Archive03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • chr1sg75
    chr1sg75 over 6 years ago in reply to koudelad +1
    Hi David, Thanks for taking the time to reply. Glad to see the forum is still alive. I have dug out an old BitScope, so I am in the process of debugging the signal lines. For what it's worth, I can answer…
Parents
  • charrua
    charrua over 12 years ago

    Can someone help me, The download links don't work! it occurs for all the files in this example, but also on other files form the 100 days 100 projects list

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 12 years ago in reply to charrua

    Hi Luis,

    I updated my response above to include the files.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • charrua
    charrua over 12 years ago in reply to dougw

    Thanks Doug!

     

    I'm trying them this afternoon.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 12 years ago in reply to charrua

    Hi Luis,

    Make sure the pin driving the back light is set as an input until you figure out if the back light on your display requires more current than the pin can supply. Some of these 5110 displays have a back light drive transistor built-in and some don't. The ones that don't can damage an output pin by drawing too much current. The LCD back light pin could be wired directly to the 3.3V power supply instead of an output pin if you are connecting with jumper wires.

    Doug

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • charrua
    charrua over 12 years ago in reply to dougw

    Done that.

     

    Besides the changing of the pinout (mine is different from the one in the project) it wokrs ok!

     

    Thank you for the files and the help.

     

    Luis

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • ronniejk
    ronniejk over 10 years ago in reply to dougw

    Hello Douglas,

    This is what CyPin datasheet says about current.

    Current – The drive current selection determines the maximum nominal logic level current

    required for a specific pin. Pins can supply more current at the cost of logic level

    compliance or can have a maximum value that is less than listed, based on system

    voltages. See the device datasheet for more details on drive currents.

      4mA source, 8mA sink – Default

      4mA source, 25mA sink – Requires SIO

     

    So in case of a PSOC4 Pioneer kit  CY8CKIT-042CY8CKIT-042 what is the maximum current I can source safely if I don't worry about voltage level is 10mA a possibility

    My LCD seems to be using around 10mA and 3.3V hence the question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ronniejk
    ronniejk over 10 years ago in reply to dougw

    Hello Douglas,

    This is what CyPin datasheet says about current.

    Current – The drive current selection determines the maximum nominal logic level current

    required for a specific pin. Pins can supply more current at the cost of logic level

    compliance or can have a maximum value that is less than listed, based on system

    voltages. See the device datasheet for more details on drive currents.

      4mA source, 8mA sink – Default

      4mA source, 25mA sink – Requires SIO

     

    So in case of a PSOC4 Pioneer kit  CY8CKIT-042CY8CKIT-042 what is the maximum current I can source safely if I don't worry about voltage level is 10mA a possibility

    My LCD seems to be using around 10mA and 3.3V hence the question.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • dougw
    dougw over 10 years ago in reply to ronniejk

    It may depend on what voltage you need, but 10 ma from an output rated at 4 ma is probably too much to hope for. If you really can't add an external FET you might consider using 3 pins tied together. Since the output voltage will sag if more than 4 ma are drawn, the 3 outputs will share current as long as they are switched at the same time.