Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 32 subscribers
  • Views 4989 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#061 – Nokia 5110 LCD Interface

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today’s example we are showcasing how to interface to the Nokia 5110 LCD screen with the PSoC 4 Pioneer Kit. This simple display provides a 84 x 48 Graphics LCD that was used in the Nokia 5110 model in 1998. This example provides a simple example to write text and an image on the LCD screen. This example uses a bit-banging method for sending the data & clock from the CPU to the LCD panel. The project does not require any UDB resources, therefore it can be used with the PSoC 4 (42xx and 41xx families).

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Zip File of Images
    • Project Schematic
    • Component Configurations

 

Components Used:

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Annotated Component for Kit-042
  • CyPins

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

In this example we provide you with a couple of firmware based files named “Nokia5110LCD.c” and  “Nokia5110LCD.h”. These files are the source & header files required for using APIs. In this example we support the following APIs to control the Nokia 5110 LCD screen.

  • void LCD_Character(uint8)
  • void LCD_Clear(void)
  • void LCD_Init(void)
  • void LCD_String(char*)
  • void LCD_Write(uint8, uint8)
  • void Send_Data(int8)
  • void LCD_gotoXY(uint8, uint8)
  • void LCD_Bitmap(char*)

 

The main.c simply calls the APIs defined in the source file for initialization & for displaying the string on the LCD.

 

In this example, LCD initialization is done as specified in the datasheet of PCD8544 LCD driver which is used in the LCD panel. It is not necessary to use all 8 pins of PSoC 4 for interfacing this LCD. Reset, Chip Enable, Power, Backlight & Ground pins can be connected to fixed voltage levels on the board. Only Data/Command, Data & Clock pins are used for sending the data to LCD.

 

Hardware Connections:

 

In this example we are not using any specific headers or shields. Instead we are providing a firmware example to interface with the Nokia 5110 screen. We have connected the screen in the following connections:

 


image

 

Test Your Project:

 

Connect your screen and program the Pioneer kit. See the screen display the example text and images.

 


image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
5732.Project Images.zip
imagePCD8544 datasheet.pdf
Nokia5110 LCD Interface.cywrk.Archive03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • chr1sg75
    chr1sg75 over 6 years ago in reply to koudelad +1
    Hi David, Thanks for taking the time to reply. Glad to see the forum is still alive. I have dug out an old BitScope, so I am in the process of debugging the signal lines. For what it's worth, I can answer…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks!