Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Gameduino shield interfacing help
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 27 subscribers
  • Views 616 views
  • Users 0 members are here
Related

Gameduino shield interfacing help

e14 Contributor
e14 Contributor over 13 years ago

Hi all

 

Is possible help me with interfacing Gameduino shield and Psoc4 kit ?

 

http://excamera.com/sphinx/gameduino/

 

https://www.sparkfun.com/products/10593

 

Many thanks Kamil

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Any idea ?

     

    Please help me

     

    Many thanks

     

    Kamil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jesusantoniocar
    jesusantoniocar over 13 years ago in reply to e14 Contributor

    Hello Kamil.

    I hope you are better.

    could you speak more about your project, i  have not the Gameduino  shield, but if is possible i would like to help you.

     

    best regards,

     

    Jesus Antonio.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Hi Kamil,

    If I know well, the gameduino is an independent graphic unit, connected to the arduino on standard SPI interface. It has its own small cpu with a forth instruction set, build all in a xilinx fpga. In point of view from programming, you can use basically 2 commands, one for write a memory byte, another to read it, with the arduino SPI lib support.

    I am very new in the Pioneer board, but it seems me, for a minimal demo you can use an SPI block to access the gameduino interface, and a program, which send a small piture,s data to the gameduino memory to display it.

    It has sound sythetisator too, it can be used as a tone generator, write the memory/registers started at 2A00 (VOICES) This is the base of the 64 voice registers.  Here are the details:

    http://excamera.com/sphinx/gameduino/hardware.html#low-level-spi-interface

    t.janos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to jesusantoniocar

    Hi Kamil,

    If I know well, the gameduino is an independent graphic unit, connected to the arduino on standard SPI interface. It has its own small cpu with a forth instruction set, build all in a xilinx fpga. In point of view from programming, you can use basically 2 commands, one for write a memory byte, another to read it, with the arduino SPI lib support.

    I am very new in the Pioneer board, but it seems me, for a minimal demo you can use an SPI block to access the gameduino interface, and a program, which send a small piture,s data to the gameduino memory to display it.

    It has sound sythetisator too, it can be used as a tone generator, write the memory/registers started at 2A00 (VOICES) This is the base of the 64 voice registers.  Here are the details:

    http://excamera.com/sphinx/gameduino/hardware.html#low-level-spi-interface

    t.janos

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Hi t.janos

     

    Thanks info about gameduino spi :-)

     

    Yes gameduino is great platform for Psoc4 Pionner Kit

     

    Synthesizer engine is my favorite :-)

     

    Kamil