Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#094 – Amplifier with Dynamic Gain Switching
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 31 subscribers
  • Views 4132 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#094 – Amplifier with Dynamic Gain Switching

cy.wbz
cy.wbz over 13 years ago

Hello!

 

In today’s example project we are continuing to explore more analog centric projects. In this example we are implementing a 3 channel amplifier with a dynamic gain switch. Based on your end design you may want to change the gain of your amplifier when reading in your analog signals. In this example we use a button selection to control the gain on the amplifier, but in your design you may change the gain by inputs from your system. The values are then sent over the UART port to be displayed on a Hyperterminal application.

 


image

 

Forum Post Attachments:

 

At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Project Images

 

Components Used: 

 

The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • Amux
  • OpAmp
  • ADC SAR Seq
  • UART
  • Debouncer
  • CyClock
  • CyPins

 

Firmware Description:

 

The main.c firmware is included in the example project. Please review the commented sections for more details.

 

The Opamp is used to amplify the input signal. Selection of input channel is done using Input_Amux and selection of the Gain is done using the Gain_Amux. The UART is used to send ADC results through the UART bridge on the PSoC 5LP.

 

The Debouncer component is used to remove glitches from the input switch. The SAR ADC converts the analog output of the OpAmp into digital values. The ADC also generates an interrupt when its input is outside the defined voltage window (250mV-750mV). The LED is turned on when the ADC generates this interrupt.

 

The data displayed over the UART includes the ADC output of the active channel along with the channel number to the HyperTerminal.

 

Hardware Connections:

 

The external hardware connections for this example are detailed in the schematic capture for this project. We include the external components and layout information using the annotated components. These annotated components detail the various resistor values needed to control the variable gain amplifier.

 

image

 

Test Your Project:

 

Program the Pioneer board and connect your three input signals. Then connect the UART to the PSoC 5LP and launch the hyperterminal software to view the UART output.

 

image

 

I hope this example can help you in your design.

 

Best,

Matt

Attachments:
5187.Project Images.zip
Opamp_Dynamic_Gain_Switching01.zip
  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 13 years ago +1
    Just as a note: PSoC3 and 5 contain an internal PGA, so they canswitch gain even without external components.
  • michaelkellett
    michaelkellett over 8 years ago in reply to eduardosilva +1
    No need to pay and no need to use Psoc or to panic. There are loads and loads of analogue switch chips on the market. I can help you choose if you post a schematic showing, or you can choose yourself.…
  • michaelkellett
    michaelkellett over 8 years ago in reply to eduardosilva

    You'll need a Psoc user to help with Psoc specific stuff, do you have to use a Psoc or can you use any micro and some external hardware ?.

     

    Looks to me as if you need a dual 4 way analogue multiplexer - lots around - no problem. You component choice is bad - good quality 10uF capacitors are very big and very expensive, for filters you should use film capacitors or COG/NPO type ceramics. High value ceramic capacitors are very voltage dependent so introduce distortion.

    If you made the capacitors 1uF 63V film types you could scale the resistors up by a factor of 10 and have the same filter frequencies, but with sensible size of capacitors.

    BTW, that integrator looks worrying - there is no DC feedback on the amplifier so it will sit with its output at one rail or the other - perhaps you haven't shown us the complete circuit.

     

    Let me know if you have to use Psoc and if not I'll try to sketch out how to use the multiplexers. Do you have a design spec for the whole thing, and what is it for ?

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • eduardosilva
    eduardosilva over 8 years ago in reply to michaelkellett

    Good afternoon MK,

    Yes the final project of the university, consists of the use of the PSOC to carry out this work.

    I just needed some help with this part of Psoc, someone who could sketch something for me in Psoc, who understands how multiplexers work and how to do their control.

    As for the values of the compenents this is adaptable, and is not the most relevant. The integrator circuit is just the same.

    If someone could help me please ..

    Best wishes, friends,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<