Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 5LP Programmer Firmware
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 34 subscribers
  • Views 9786 views
  • Users 0 members are here
Related

PSoC 5LP Programmer Firmware

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today I would like to post an extra project for you guys. Attached to this post is the firmware for the PSoC 5LP device on the Pioneer kit. If you are designing a board and need a programmer and debugger for the board feel free to copy the PSoC 5LP layout on the Pioneer board and use this firmware to enable programming and debugging. The layout files are on the Cypress Pioneer Kit web page:

 

www.cypress.com/cy8ckit-042

 

This will allow you interface your custom board with our PSoC Creator and PSoC Programmer development tools.

 

In the example attached we have two projects, the source code for the PSoC 5LP and a base bootloadable project. To build the project you will need to perform the following actions:

 

1. Make the project KitProg_Bootloader active and build it first.

2. Open the KitProg project TopDesign.

3. Doube click the bootloadable component to open the bootloadable configuration.

4. Select the tab 'dependencies' and select the browse button.

5. Browse to the folder where the KitProg Bootloader.hex file is generated and select this file. Click Ok.

 

Good Luck!

Matt

Attachments:
KitProg version 2_03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +2
    The other day I found a little SOIC 0.65 pitch board (schmartboard) so I used one of my 4200 SSOP 28 pin chips. I bought 10 SSOPs 10 QFPs and 20 QFN while they were (and still are) a dollar a pop. I had…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Wow~ That's cool~
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hi all, Posting the PSoC 5LP firmware updated for PSoC Creator 3.0 -Ranjith Attachments: community.element14.com/.../KitProg.zip
Parents
  • wire67
    wire67 over 9 years ago

    Hi, how to transfer the bootloadable to the PSoC 5 ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wire67
    wire67 over 9 years ago in reply to wire67

    according to the source code:

    - Press PSoC 4 reset switch for more than 100ms during power-up.

    => If yes, blink the LED slowly(ON Time = 1.5s, OFF Time = 1.5s) to indicate that the device is in bootloader

     

    Then I guess using "bootloader host", leaving the default settings

    08:51:51 PM - program Started

    08:51:52 PM - The operation has timed out.

    08:51:52 PM - Communication port reported error 'Unable to read data from the target device'.

    08:51:52 PM - program failed in 1193 ms.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • wire67
    wire67 over 9 years ago in reply to wire67

    according to the source code:

    - Press PSoC 4 reset switch for more than 100ms during power-up.

    => If yes, blink the LED slowly(ON Time = 1.5s, OFF Time = 1.5s) to indicate that the device is in bootloader

     

    Then I guess using "bootloader host", leaving the default settings

    08:51:51 PM - program Started

    08:51:52 PM - The operation has timed out.

    08:51:52 PM - Communication port reported error 'Unable to read data from the target device'.

    08:51:52 PM - program failed in 1193 ms.