Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 5LP Programmer Firmware
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 34 subscribers
  • Views 9791 views
  • Users 0 members are here
Related

PSoC 5LP Programmer Firmware

cy.wbz
cy.wbz over 13 years ago

Hello!

 

Today I would like to post an extra project for you guys. Attached to this post is the firmware for the PSoC 5LP device on the Pioneer kit. If you are designing a board and need a programmer and debugger for the board feel free to copy the PSoC 5LP layout on the Pioneer board and use this firmware to enable programming and debugging. The layout files are on the Cypress Pioneer Kit web page:

 

www.cypress.com/cy8ckit-042

 

This will allow you interface your custom board with our PSoC Creator and PSoC Programmer development tools.

 

In the example attached we have two projects, the source code for the PSoC 5LP and a base bootloadable project. To build the project you will need to perform the following actions:

 

1. Make the project KitProg_Bootloader active and build it first.

2. Open the KitProg project TopDesign.

3. Doube click the bootloadable component to open the bootloadable configuration.

4. Select the tab 'dependencies' and select the browse button.

5. Browse to the folder where the KitProg Bootloader.hex file is generated and select this file. Click Ok.

 

Good Luck!

Matt

Attachments:
KitProg version 2_03.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +2
    The other day I found a little SOIC 0.65 pitch board (schmartboard) so I used one of my 4200 SSOP 28 pin chips. I bought 10 SSOPs 10 QFPs and 20 QFN while they were (and still are) a dollar a pop. I had…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Wow~ That's cool~
  • e14 Contributor
    e14 Contributor over 12 years ago +1
    Hi all, Posting the PSoC 5LP firmware updated for PSoC Creator 3.0 -Ranjith Attachments: community.element14.com/.../KitProg.zip
Parents
  • ilmete
    ilmete over 6 years ago

    Hi,

     

    I would like to share how to use CY8CKIT-059CY8CKIT-059 target board (CY8C5888LTI_LP097) as a kitprog v2.21;

     

    Load the attached hex into the CY8CKIT-059CY8CKIT-059 target board (CY8C5888LTI_LP097) with a kitprog and Psoc Programmer.

    And do following HW modifications on target board (You can see the modifications on attached pictures).

     

    - Snap the kit into two pieces.

    - Short P0.5 and P3.2 to GND.

    - Short P2.2 to P12.4  ( for switch functionality )

    - Short P3.1 to P2.1  ( for led    functionality )

     

    - Add a R-2R resistor divider to P1.6 from the VBUS or any VDDD pin on board. (GND---20k---P1.7---10K---VBUS)

    - Add a R-2R resistor divider to P1.7 from the VTARGET (New kit pin - Not on board). (GND---20k---P1.6---10K---VTARGETnew)

     

    If you use 5V board always you can add only one divider instead of two seperate;

     

      P1.6---|      |---10K---VDDIO (or VDD or VBUS or VTARGET on board)

            |------|

    P1.7---|      |---20K---GND

     

    - Use these outputs: P12.4 as RST, P12.3 as SWDCLK, P12.2 as SWDIO, GND , high side of the P1.7 Resistor as VTARGET.

                                    If you use one resistor divider you can use any VDDD,VDDIO,VTARG as VTARGET output.

     

    How I get the hex file;

    I couldn't load original kitprog hex file to CY8C5888LTI_LP097 on CY8CKIT-059CY8CKIT-059 with the Psoc Programmer.

    So I tried these;

    - I loaded a compatible bootloader hex to the CY8C5888LTI_LP097 with kitprog and PSOC Programmer to load metadata sections.

    - I removed the sections start with 0x80000000 and 0x90000000 in the original kitprog hex files.

    - Then I loaded this modified hex to the CY8C5888LTI_LP097 with J-Link and J-Flash.

    - Connected the board to PC with a USB cable. Psoc Programmer see the kitprog and it said upgrade. Upgraded it and it works as version 2.21

    - I readback the working code as a hex file with Psoc Programmer and checked it by reload it to CY8C5888LTI_LP097.  Working hex file attached.

     

    Regards.

    Attachments:
    CY8C5888__as_kitprog.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ilmete
    ilmete over 6 years ago

    Hi,

     

    I would like to share how to use CY8CKIT-059CY8CKIT-059 target board (CY8C5888LTI_LP097) as a kitprog v2.21;

     

    Load the attached hex into the CY8CKIT-059CY8CKIT-059 target board (CY8C5888LTI_LP097) with a kitprog and Psoc Programmer.

    And do following HW modifications on target board (You can see the modifications on attached pictures).

     

    - Snap the kit into two pieces.

    - Short P0.5 and P3.2 to GND.

    - Short P2.2 to P12.4  ( for switch functionality )

    - Short P3.1 to P2.1  ( for led    functionality )

     

    - Add a R-2R resistor divider to P1.6 from the VBUS or any VDDD pin on board. (GND---20k---P1.7---10K---VBUS)

    - Add a R-2R resistor divider to P1.7 from the VTARGET (New kit pin - Not on board). (GND---20k---P1.6---10K---VTARGETnew)

     

    If you use 5V board always you can add only one divider instead of two seperate;

     

      P1.6---|      |---10K---VDDIO (or VDD or VBUS or VTARGET on board)

            |------|

    P1.7---|      |---20K---GND

     

    - Use these outputs: P12.4 as RST, P12.3 as SWDCLK, P12.2 as SWDIO, GND , high side of the P1.7 Resistor as VTARGET.

                                    If you use one resistor divider you can use any VDDD,VDDIO,VTARG as VTARGET output.

     

    How I get the hex file;

    I couldn't load original kitprog hex file to CY8C5888LTI_LP097 on CY8CKIT-059CY8CKIT-059 with the Psoc Programmer.

    So I tried these;

    - I loaded a compatible bootloader hex to the CY8C5888LTI_LP097 with kitprog and PSOC Programmer to load metadata sections.

    - I removed the sections start with 0x80000000 and 0x90000000 in the original kitprog hex files.

    - Then I loaded this modified hex to the CY8C5888LTI_LP097 with J-Link and J-Flash.

    - Connected the board to PC with a USB cable. Psoc Programmer see the kitprog and it said upgrade. Upgraded it and it works as version 2.21

    - I readback the working code as a hex file with Psoc Programmer and checked it by reload it to CY8C5888LTI_LP097.  Working hex file attached.

     

    Regards.

    Attachments:
    CY8C5888__as_kitprog.zip