Cypress Kits
  • Products
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 38 subscribers
  • Views 8061 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP

cy.wbz
cy.wbz over 12 years ago

Hello!


In today’s example we are including a demonstration project for supporting Audio playback and audio recording using USB digital audio. The PSoC 5LP communicates with any USB host, provides a high-quality recording interface to it, and extras high-quality digital audio from the USB host. In this example we show the PSoC 5LP device communicating to:

  • Windows
  • Mac
  • Linux
  • Android
  • Raspberry Pi
  • BeagleBone Black
  • Android
  • iOS



image


This example project utilizes the PSoC 5LP device on the PSoC 4 Pioneer Kit. This example has the following features:

  • Audio-out (I2S)
  • Audio-in (PDM Mic)
  • USB Host Interface
  • Volume Control
  • Watchdog


The firmware was designed and tested with PSoC Creator 2.2 SP1.


Forum Post Attachments:


At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Project Images
  • Example Documentation


Components Used:


The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • I2C
  • EZI2C
  • SPI
  • UART


Firmware Description:


The main.c firmware is included in the example project. Please review the commented sections for more details.


Attached to this example project is a detailed example description. In this file we include a detailed write up of the external hardware used in the example, the internal firmware architecture, and how to recreate the system on your own. Please feel free to review this document for a detailed understanding of how the example is designed and used.


We are also listing the custom components, hardware, and firmware files necessary to create this example. Please feel free to download the zip file for more information.


Hardware Connections:


The hardware connections are detailed in the attached zip project. We include the codec board schematics in the documentation folder.


Test Your Project:


Please see the below image of the example in action.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I hope this example can help you in your design.

Best,

Matt

Attachments:
imagePioneerKit_P5LP_USB_Audio_UserGuide.pdf
PioneerKit_P5LP_USB_Audio.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +3
    The PSoC 5LP USB Audio example project offers a great way to do a general USB Audio solution. Here, I would like to add that if somebody is looking particularly for native MFi USB audio solution for Apple…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    The PSoC Creator project attached to the original post doesn't work with PSoC Creator 3.0 SP1 (It was build with PSoC Creator 2.2 SP1). I have made minimal changes to the original project (updated Cy_boot…
  • greatunclebulgaria
    greatunclebulgaria over 12 years ago +1
    Matt, Thanks for this post, looks very interesting, BUT I'm having trouble with the hardware connections. POSC4 P5LP header Pin POSC4 P5LP header Name AK4556 J6 Header AK4556 Pin Number CS42L51 CS42L51…
Parents
  • 1s2d3d54f4
    1s2d3d54f4 over 8 years ago

    Is there a good reason why Cypress code always uses global variables for everything instead of using limited-scope variables, parameters and returns, etc.?   And contains unnecessary comparisons like if (codecInit == TRUE) instead of if (codecInit), uses function-like macros instead of inline functions, defines macros like TRUE instead of using stdbool.h types, etc.?

     

    To read through the code and understand how it works, I constantly have to do a project-wide search for each variable and try to remember every other function that modifies it, and it's frustrating.  Every source I've found says these practices should be avoided, but maybe the rules are different for embedded code?  I want to change them all to make them more readable, but I'm afraid there's some reason they were done this way.  Do these practices help with optimizing code size or preventing stack overflows or something?  Or are they just bad programming?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • 1s2d3d54f4
    1s2d3d54f4 over 8 years ago

    Is there a good reason why Cypress code always uses global variables for everything instead of using limited-scope variables, parameters and returns, etc.?   And contains unnecessary comparisons like if (codecInit == TRUE) instead of if (codecInit), uses function-like macros instead of inline functions, defines macros like TRUE instead of using stdbool.h types, etc.?

     

    To read through the code and understand how it works, I constantly have to do a project-wide search for each variable and try to remember every other function that modifies it, and it's frustrating.  Every source I've found says these practices should be avoided, but maybe the rules are different for embedded code?  I want to change them all to make them more readable, but I'm afraid there's some reason they were done this way.  Do these practices help with optimizing code size or preventing stack overflows or something?  Or are they just bad programming?