Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 27 replies
  • Subscribers 38 subscribers
  • Views 8179 views
  • Users 0 members are here
Related

PSoC 4 Pioneer Kit Community Project#102 – USB Audio using the PSoC 5LP

cy.wbz
cy.wbz over 12 years ago

Hello!


In today’s example we are including a demonstration project for supporting Audio playback and audio recording using USB digital audio. The PSoC 5LP communicates with any USB host, provides a high-quality recording interface to it, and extras high-quality digital audio from the USB host. In this example we show the PSoC 5LP device communicating to:

  • Windows
  • Mac
  • Linux
  • Android
  • Raspberry Pi
  • BeagleBone Black
  • Android
  • iOS



image


This example project utilizes the PSoC 5LP device on the PSoC 4 Pioneer Kit. This example has the following features:

  • Audio-out (I2S)
  • Audio-in (PDM Mic)
  • USB Host Interface
  • Volume Control
  • Watchdog


The firmware was designed and tested with PSoC Creator 2.2 SP1.


Forum Post Attachments:


At the bottom of this post we are including the following items:

  • Example Project Zip File
  • Project Images
  • Example Documentation


Components Used:


The user can download the example project at the bottom of this post. The project uses the following list of Creator Components:

  • I2C
  • EZI2C
  • SPI
  • UART


Firmware Description:


The main.c firmware is included in the example project. Please review the commented sections for more details.


Attached to this example project is a detailed example description. In this file we include a detailed write up of the external hardware used in the example, the internal firmware architecture, and how to recreate the system on your own. Please feel free to review this document for a detailed understanding of how the example is designed and used.


We are also listing the custom components, hardware, and firmware files necessary to create this example. Please feel free to download the zip file for more information.


Hardware Connections:


The hardware connections are detailed in the attached zip project. We include the codec board schematics in the documentation folder.


Test Your Project:


Please see the below image of the example in action.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

I hope this example can help you in your design.

Best,

Matt

Attachments:
imagePioneerKit_P5LP_USB_Audio_UserGuide.pdf
PioneerKit_P5LP_USB_Audio.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago +3
    The PSoC 5LP USB Audio example project offers a great way to do a general USB Audio solution. Here, I would like to add that if somebody is looking particularly for native MFi USB audio solution for Apple…
  • e14 Contributor
    e14 Contributor over 12 years ago +2
    The PSoC Creator project attached to the original post doesn't work with PSoC Creator 3.0 SP1 (It was build with PSoC Creator 2.2 SP1). I have made minimal changes to the original project (updated Cy_boot…
  • greatunclebulgaria
    greatunclebulgaria over 12 years ago +1
    Matt, Thanks for this post, looks very interesting, BUT I'm having trouble with the hardware connections. POSC4 P5LP header Pin POSC4 P5LP header Name AK4556 J6 Header AK4556 Pin Number CS42L51 CS42L51…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    The PSoC 5LP USB Audio example project offers a great way to do a general USB Audio solution.

     

    Here, I would like to add that if somebody is looking particularly for native MFi USB audio solution for Apple Devices (not through Camera Connection Kit), then Cypress provides full support through their kit CY8CKIT-033A. Any MFi Licensee can order this kit as well as the installer package (containing example projects, documents and schematics) through MFi Avnet website.

     

    -Rohit

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    For the interest of members who wants to understand the implementation of the PDM audio path, this solution provides a single chip audio path implementation for converting 1-bit PDM input signal to PCM signal (which includes PDM clock generation, PDM Data sampling, DMA data transfer, integrator, decimator and droop correction filtering) and transfer the resultant PCM samples over USB audio class interface to a USB host device.

     

    This audio path implementation uses PSoC's UDB and DMA engine to process and transfer the microphone data, minimizing the CPU overhead and providing a high quality low power PDM microphone interface.

     

    For more details on implementation, see this article: http://edn.com/design/consumer/4425878/High-quality-PDM-microphone-interfacing-using-off-the-shelf-SoCs

     

    -Rohit

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dandumit
    dandumit over 12 years ago in reply to e14 Contributor

    Hi,

    I have landed on this page searching for PSoC4 and DMA. Unfortunately (for me) it seems that you are using PSoC5.

    Could you please confirm that PSoC4 has no DMA?

    BR,

    DAniel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dandumit
    dandumit over 12 years ago in reply to e14 Contributor

    Hi,

    I have landed on this page searching for PSoC4 and DMA. Unfortunately (for me) it seems that you are using PSoC5.

    Could you please confirm that PSoC4 has no DMA?

    BR,

    DAniel