Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum FreeRTOS ported to the PSoC 4
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 28 subscribers
  • Views 5119 views
  • Users 0 members are here
  • psoc4
  • freertos
Related

FreeRTOS ported to the PSoC 4

e14 Contributor
e14 Contributor over 12 years ago

I've ported FreeRTOS to PSoC 4 - which really was extremely trivial. It's simply the Cortex M0 port with some configuration & glue from the PSoC 5 demo.

The attached demo app creates three tasks that toggle the red, green and blue LEDs on the PSoC 4 pioneer board at slightly different rates, resulting in a pleasing (if somewhat psychedelic) light show. Adapting this demo for your own purposes should be straightforward.

Note that because the PSoC Capsense component makes (undocumented) use of the systick timer, it's not currently possible to use FreeRTOS and the PSoC Capsense component together.

Attachments:
FreeRTOSDemo.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Hello! You are confusing exception and interrupt vectors. In the ARM architecture you have an internal SYSTICK exception that gets triggered by the M3. The handler for this has to be installed in slot…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thanks guy

    I figured it out got it working. now i am trying to figure what benefits this gives me? watched a couple rtos video and they said the task scheduling techniques and queues between task.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Yes, I like to use an RTOS with CapSense. I put the CapSense scanning code in one task and push the results into a queue or a mailbox. Then I can write "application code" that just uses the queue for instructions - it does not have to worry about all the scanning and reading and interpreting finger activity.

    One nice feature of FreeRTOS is the idea of co-routines - these can save you a lot of SRAM because, unlike tasks, they share a stack.

    -- Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Yes, I like to use an RTOS with CapSense. I put the CapSense scanning code in one task and push the results into a queue or a mailbox. Then I can write "application code" that just uses the queue for instructions - it does not have to worry about all the scanning and reading and interpreting finger activity.

    One nice feature of FreeRTOS is the idea of co-routines - these can save you a lot of SRAM because, unlike tasks, they share a stack.

    -- Mark.