Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Wave Dac usage on Pioneer kit
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 28 subscribers
  • Views 1388 views
  • Users 0 members are here
Related

Wave Dac usage on Pioneer kit

fixstuff
fixstuff over 13 years ago

Hello,

 

I would like to use the Waveform Dac component in PSOC Creator 3, and get this message when I go to build:

 

Component 'WaveDAC8_1' uses component 'cy_dma_v1_70' in its implementation. 'cy_dma_v1_70' has an error: The cy_dma_v1_70 component (WaveDAC8_1_Wave1_DMA) is an Obsolete component. It is no longer recommended for use and should be replaced with a production version of the component (or an alternative implementation).

 

Component 'WaveDAC8_1' uses component 'cy_dma_v1_70' in its implementation. 'cy_dma_v1_70' has an error: The cy_dma_v1_70 component (WaveDAC8_1_Wave2_DMA) is an Obsolete component. It is no longer recommended for use and should be replaced with a production version of the component (or an alternative implementation).

 

Component 'WaveDAC8_1' uses component 'VDAC8_v1_90' in its implementation. 'VDAC8_v1_90' has an error: The VDAC8_v1_90 component (WaveDAC8_1_VDAC8) is an Obsolete component. It is no longer recommended for use and should be replaced with a production version of the component (or an alternative implementation).

 

Is the Waveform Dac v2.0 component functional in PSOC Creator 3 for the PSOC 4 on the Pioneer?

 

thanks,

 

james

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 13 years ago in reply to cy.gul +1
    From what I can see from Project #70 - It shows how to load an alternative bootloader for the onboard PSoC 5LP and how to revert it back again to normal. It doesn't explicitly show how to configure the…
  • fixstuff
    fixstuff over 13 years ago in reply to cy.gul +1
    Yes, I did end up getting the Waveform Dac working with the PSOC 5 LP. I've actually beeen doing quite a bit with the 5LP on the Pioneer board, and am stunned at just how much can be done on this little…
Parents
  • cy.gul
    0 cy.gul over 13 years ago

    Hi James,

     

    The Wavdac Component requires the use of DMA, which the current families of PSoC 4 do not feature. DMA is however available on both PSoC 3 and PSoC 5LP.

    In project#70 we have an example of the Wavdac running on Pioneer Kit's the PSoC 5LP.

    http://www.element14.com/community/message/86076#86076/l/psoc-4-pioneer-kit-community-project070-psoc-4-getting-started-lab-4-adc,


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • COMPACT
    0 COMPACT over 13 years ago in reply to cy.gul

    From what I can see from Project #70 - It shows how to load an alternative bootloader for the onboard PSoC  5LP and how to revert it back again to normal. It doesn't explicitly show how to configure the PSoC 5LP with a Waveform DAC component.

    With a PSoC 4 you can use the iDAC component.

    This may suit your needs.

    It doesn't have DMA but it can be used successfully to generate a variable analog voltage.

    In fact you can even modulate the the intensity of the onboard RGB LED with it.

    You can convert it to a vDAC be feeding the output across a fixed value resistor.

    Remember that V = i x R.

    You can boost the output using an amp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • COMPACT
    0 COMPACT over 13 years ago in reply to cy.gul

    From what I can see from Project #70 - It shows how to load an alternative bootloader for the onboard PSoC  5LP and how to revert it back again to normal. It doesn't explicitly show how to configure the PSoC 5LP with a Waveform DAC component.

    With a PSoC 4 you can use the iDAC component.

    This may suit your needs.

    It doesn't have DMA but it can be used successfully to generate a variable analog voltage.

    In fact you can even modulate the the intensity of the onboard RGB LED with it.

    You can convert it to a vDAC be feeding the output across a fixed value resistor.

    Remember that V = i x R.

    You can boost the output using an amp.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • COMPACT
    0 COMPACT over 13 years ago in reply to COMPACT

    For details of writing a PSoC 5LP project for the Pioneer kit read the About the community project #36.