Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Has anyone got a single ended ADC going on the PSoC Pioneer 4 from 0V to 5V?
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 28 subscribers
  • Views 845 views
  • Users 0 members are here
  • psoc4
Related

Has anyone got a single ended ADC going on the PSoC Pioneer 4 from 0V to 5V?

e14 Contributor
e14 Contributor over 12 years ago

I cannot seem to get mine working..

I am after just some example code which will take any pin as a 0V-5V input and maybe send the value out of the UART..

if not that even just a breakpoint after the conversion so I can get the right data out..

  • Sign in to reply
  • Cancel
Parents
  • juanes.pazj
    0 juanes.pazj over 12 years ago

    Hi I did a conversion of the IDAC to Voltage  IDAC conversion to VDAC (enabling two IDACs) psoc4

    you need to isolate the current source and add an opamp to convert that signal to voltage...

    Juan Esteban

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to juanes.pazj

    Hi I am sorry but I am not sure what your project is doing, I can't see the ADC and there doesn't seem to be any attached code..

     

    I have an LDR going into the PSOC and it is outputting 3.78V into the pin.. the ADC is set up to sample between 0V and 5V but on the output I just have 2047 always which is 11 bits all on..

     

    If I bring the signal below about 2.5V then it changes but it seems to be giving me a maximum of 2.5V and 11 bits..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to juanes.pazj

    Hi I am sorry but I am not sure what your project is doing, I can't see the ADC and there doesn't seem to be any attached code..

     

    I have an LDR going into the PSOC and it is outputting 3.78V into the pin.. the ADC is set up to sample between 0V and 5V but on the output I just have 2047 always which is 11 bits all on..

     

    If I bring the signal below about 2.5V then it changes but it seems to be giving me a maximum of 2.5V and 11 bits..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • vsluiter
    0 vsluiter over 12 years ago in reply to e14 Contributor

    Hi Samuel,

     

    I'm away from home, so can't test right now. Do you have the option to change the reference voltage? Probably it is now set to an internal 2.5V bandgap reference, where you'd like it to be something else (5V).

     

    Greetings,

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to vsluiter

    Hi Victor, I am not with my PSoC until tomorrow but someone on the Cypress forums has said they think it is because I am using a current limiting resistor going into the PSoC ADC pin when I don't really need one.. they said there is a 2.2k internal resistor so with my resistor outside the board it is creating a voltage divider.

     

    I have set the Vref to be 0-5V so I don't think it is that.. I will report back on my findings tomorrow when I get my board.. thanks for the reply