Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Interfacing more than one accelerometer using PSoC 4
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 30 subscribers
  • Views 1765 views
  • Users 0 members are here
Related

Interfacing more than one accelerometer using PSoC 4

e14 Contributor
e14 Contributor over 12 years ago

Is anyone knows about how to interface two accelerometers using PSoC 4? I want to access two MMA7455L.Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 12 years ago in reply to cy.gul +1
    Since SPI is a bus, there is no need to use multiple masters. Multiple chip-select signals are enough (and save pins that way). Different masters are only needed when the SPI configuration (CPOL / CPHA…
  • DAB
    0 DAB over 12 years ago

    Hi Yakub,

     

    I have not heard of anyone needing more than one accelerometer, but I am assuming you are talking about a standard 3-axis chip.

     

    If you want to use more than one 3-axis chip, then I am very curious about your application/idea.

     

    Conceptually, all you need is enough A/D ports on your PSOC to do the basic interface.  As I recall, there are at least twelve on the board, so you should be able to make it work.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 12 years ago

    The MMA7455L has both I2C and SPI outputs. I would recommend using SPI. Connect MISO, MOSI and CLK lines together. Then use two different select signals, and control them manually (via a control register) in your code. With that setup, you can use a single SPI master component, and select manually which one to talk to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to DAB

    Hi DAB,

     

    in this design I connected 7 gyro's and 7 accelerometers to one microcontroller:)

     

    I used SPI for that, with chip selects.

    The reason for choosing SPI was that we needed to get the data within a certain time after a synchronisation trigger, and SPI is much faster than I2C. The MMA455L has an address pin, so you could easily connect two of these to one I2C bus.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 12 years ago in reply to vsluiter

    Hi Victor,

     

    Thanks for the update.

    I have to admit, this is an area that I only spent a limited time working on projects.  So in my mind, one accelerometer was plenty, but now I can see a much larger world where they could be employed.  Its always a good day to learn something new.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cy.gul
    0 cy.gul over 12 years ago

    Hi Yakub,

    The MMA7455L seems to be an I2C/SPI accelerometer.

     

    The PSoC 4 has a SCB (serial communication block) that can have 2 x I2C/SPI/UART on it. These alone can get you talking to 2 accelerometers.

     

    Additionally, you can run a UDB-based SPI or I2C for a 3rd one in case you need it.

     

    See this as an example: PSoC 4 Pioneer Kit Community Project#035 – UART, I2C, and SPI Joystick Example

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 12 years ago in reply to cy.gul

    Since SPI is a bus, there is no need to use multiple masters. Multiple chip-select signals are enough (and save pins that way). Different masters are only needed when the SPI configuration (CPOL / CPHA) are needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to DAB

    Hi DAB,

     

    Thank you for your answer. In this case, I want to show in PC about 8 direction movement (like direction of the wind, e.g: N, NE, E, SE, S, SW, W, NW) using two accelerometer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 12 years ago in reply to e14 Contributor

    I can't see why you'd need two accelerometers for that... Please look into 2- or 3-axis accelerometers, they can give you 2-axis information in a single package!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • DAB
    0 DAB over 12 years ago in reply to e14 Contributor

    Hi Yakub,

     

    I agree with Victor, you should only need to use one accellerometer to get a full 360 by 360 movement direction.

    If you have a good MCU, the trigonometry is pretty basic to work out the direction from which the force is being applied to the sensor.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to vsluiter

    Hi vsluiter,

     

    Could you introduce more about the project you mentioned with 7 gyro's and 7 accelerometers? Like what sensors and what microcontroller?

     

    I have a project which needs 3 gyro's and 3 accelerometers. This is my first project related to hardware thing. Could you help me through? Thanks,

     

    SoFun