Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Interfacing more than one accelerometer using PSoC 4
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 30 subscribers
  • Views 1760 views
  • Users 0 members are here
Related

Interfacing more than one accelerometer using PSoC 4

e14 Contributor
e14 Contributor over 12 years ago

Is anyone knows about how to interface two accelerometers using PSoC 4? I want to access two MMA7455L.Thank you

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 12 years ago in reply to cy.gul +1
    Since SPI is a bus, there is no need to use multiple masters. Multiple chip-select signals are enough (and save pins that way). Different masters are only needed when the SPI configuration (CPOL / CPHA…
Parents
  • cy.gul
    0 cy.gul over 12 years ago

    Hi Yakub,

    The MMA7455L seems to be an I2C/SPI accelerometer.

     

    The PSoC 4 has a SCB (serial communication block) that can have 2 x I2C/SPI/UART on it. These alone can get you talking to 2 accelerometers.

     

    Additionally, you can run a UDB-based SPI or I2C for a 3rd one in case you need it.

     

    See this as an example: PSoC 4 Pioneer Kit Community Project#035 – UART, I2C, and SPI Joystick Example

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • hlipka
    0 hlipka over 12 years ago in reply to cy.gul

    Since SPI is a bus, there is no need to use multiple masters. Multiple chip-select signals are enough (and save pins that way). Different masters are only needed when the SPI configuration (CPOL / CPHA) are needed.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hlipka
    0 hlipka over 12 years ago in reply to cy.gul

    Since SPI is a bus, there is no need to use multiple masters. Multiple chip-select signals are enough (and save pins that way). Different masters are only needed when the SPI configuration (CPOL / CPHA) are needed.